Other Parts Discussed in Thread: OMAP-L138, OMAPL138
I'm new to the OMAP-L138, although I have lots of experience with other TI DSP's and DSP/BIOS. I need to use the EDMA to move some data in my application, so I'm trying to come up to speed to the point where I can do that. Unfortunately, I'm finding that there is no good overview of the EDMA and the library for the L138. I've crawled through the EDMA3 user manual, the EDMA3 resource manager user manual and numerous other documents, but it seems I will have to become a complete expert on both the hardware and the software for the EDMA, when all I really need is a good example of how to configure and run a QDMA from an EMIF FIFO to DDR. I can't believe I'm the only OMAP user who could use this type of documentation. Maybe it's out there and I've missed it.
I also find that figuring out how to include the correct library and include file path is also very non-obvious. I'm sure I'll get there, but I'm wasting days of my short development schedule. If anyone has any suggestions or examples that I could refer to, I would certainly appreciate it.
Dave