Part Number: AM3354
Tool/software: Linux
Hello Sir,
I am using AM3354BZCZD80 processor . I am using yocto build uboot source . The generated MLO AND uboot.img is not booting my board ,although i can boot the beaglebone black (AM3358bzcz100) with that image. while configuring i had used am335x_evm_defconfig . Can you give me any idea where and all i do have to concentrate for AM3354BZCZD80
CONFIG_ARM=y
CONFIG_AM33XX=y
CONFIG_TARGET_AM335X_EVM=y
CONFIG_SPL_STACK_R_ADDR=0x82000000
CONFIG_DEFAULT_DEVICE_TREE="am335x-evm"
CONFIG_SPL=y
CONFIG_SPL_STACK_R=y
CONFIG_SYS_EXTRA_OPTIONS="NAND"
CONFIG_HUSH_PARSER=y
CONFIG_AUTOBOOT_KEYED=y
CONFIG_AUTOBOOT_PROMPT="Press SPACE to abort autoboot in %d seconds\n"
CONFIG_AUTOBOOT_DELAY_STR="d"
CONFIG_AUTOBOOT_STOP_STR=" "
CONFIG_CMD_BOOTZ=y
# CONFIG_CMD_IMLS is not set
CONFIG_CMD_ASKENV=y
# CONFIG_CMD_FLASH is not set
CONFIG_CMD_MMC=y
CONFIG_CMD_SF=y
CONFIG_CMD_SPI=y
CONFIG_CMD_I2C=y
CONFIG_CMD_USB=y
CONFIG_CMD_DFU=y
CONFIG_CMD_GPIO=y
# CONFIG_CMD_SETEXPR is not set
CONFIG_OF_CONTROL=y
CONFIG_DM_MMC=y
CONFIG_CMD_DHCP=y
CONFIG_CMD_MII=y
CONFIG_CMD_PING=y
CONFIG_CMD_EXT2=y
CONFIG_CMD_EXT4=y
CONFIG_CMD_EXT4_WRITE=y
CONFIG_CMD_FAT=y
CONFIG_CMD_FS_GENERIC=y
CONFIG_SPI_FLASH=y
CONFIG_SPI_FLASH_WINBOND=y
CONFIG_DM_ETH=y
CONFIG_SYS_NS16550=y
CONFIG_TIMER=y
CONFIG_OMAP_TIMER=y
CONFIG_USB=y
CONFIG_USB_MUSB_HOST=y
CONFIG_USB_MUSB_GADGET=y
CONFIG_USB_GADGET=y
CONFIG_RSA=y
CONFIG_FIT=y
CONFIG_SPL_OF_LIBFDT=y
CONFIG_SPL_LOAD_FIT=y
CONFIG_OF_LIST="am335x-evm am335x-bone am335x-boneblack am335x-evmsk am335x-bonegreen am335x-icev2"
CONFIG_DM_NAND=y
CONFIG_USB_GADGET_DOWNLOAD=y
CONFIG_G_DNL_MANUFACTURER="Texas Instruments"
CONFIG_G_DNL_VENDOR_NUM=0x0451
CONFIG_G_DNL_PRODUCT_NUM=0xd022
CONFIG_MISC=y
CONFIG_DM_USB=y
CONFIG_USB_MUSB_TI=y
CONFIG_OF_BOARD_SETUP=y
CONFIG_CMD_TIME=y
CONFIG_DM_I2C=y
CONFIG_SPL_YMODEM_SUPPORT=y
with regards
pranav