Other Parts Discussed in Thread: TLV320AIC3106, DRA742, PMP, DRA752, TVP5158
Tool/software: Linux
Hi Sir
we used TI J6 solution with Linux for development in our customized board and found it failed during booting.
there are two error message during booting and it seems it is about systemd issue.
case 1:
Starting Apply Kernel Variables...
Starting Create Static Device Nodes in /dev...
Starting Rebuild Hardware Database...
Starting Rebuild Dynamic Linker Cache...
Starting Flush Journal to Persistent Storage...
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create Static Device Nodes in /dev.
[ 5.493671] systemd-journald[145]: Received request to flush runtime journal from PID 1
[ 96.162419] systemd-journald[145]: Failed to send WATCHDOG=1 notification message: Connection refused
[ 216.162358] systemd-journald[145]: Failed to send WATCHDOG=1 notification message: Transport endpoint is not connected
[ 276.162357] systemd-journald[145]: Failed to send WATCHDOG=1 notification message: Transport endpoint is not connected
Case 2:
[ OK ] Started Remount Root and Kernel File Systems.
Starting Rebuild Hardware Database...
Starting Rebuild Dynamic Linker Cache...
Starting Apply Kernel Variables...
Starting Create Static Device Nodes in /dev...
Starting Flush Journal to Persistent Storage...
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create Static Device Nodes in /dev.
[ 26.164844] INFO: rcu_preempt detected stalls on CPUs/tasks:
[ 26.170542] 1-...: (1 GPs behind) idle=2d7/140000000000000/0 softirq=566/569 fqs=2101
[ 26.178577] (detected by 0, t=2102 jiffies, g=-109, c=-110, q=169)
[ 26.184877] Task dump for CPU 1:
[ 26.188115] systemd R running 0 1 0 0x00000002
[ 26.194508] Backtrace:
[ 26.196977] [<c067a5bc>] (__schedule) from [<c067ac78>] (schedule+0x54/0xc4)
[ 26.204052] r10:be863770 r9:ef072000 r8:00000000 r7:30c5387d r6:ef073fb0 r5:00000000
[ 26.211946] r4:ef072000
[ 26.214499] [<c067ac24>] (schedule) from [<c0012d38>] (do_work_pending+0x28/0xc0)
[ 26.222010] r5:00000000 r4:ef072000
[ 26.225614] [<c0012d10>] (do_work_pending) from [<c000fb2c>] (slow_work_pending+0xc/0x20)
[ 26.233821] r7:30c5387d r6:ffffffff r5:90010030 r4:7f66e948
Could you advise what is wrong or how to debug this issue ?
thanks for reply.
BR
Yimin