This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2G02: Configuring GPMC for accesses between ARM-core and external FPGA as a psuedo SRAM

Part Number: 66AK2G02


Hello

I have succesfully compiled and downloaded an example project based on:

\ti\pdk_k2g_1_0_7\packages\ti\csl\example\gpmc\nor_read_write

I am using the EVMK2G board (desoldered the NAND-device) and connected AD0-15, WEn, REn, CSn and CLK to the FPGA.

- How to configure the GPMC_CONFIG7_0 register properly for this case? I don't need much of memory space so the smallest 16MB is okay (1111 for the MASKADRESS field I guess).

- What should I put in BASEADRESS field? The memory map specifies that GPMC_0_DATA has physical 40-bit adress between 00 3000 0000h and 006FFF FFFF

I have read

"7.3.4.8 Address Decoder and Chip-Select Configuration", "7.3.4.8.1 Chip-Select Base Address and Region Size" and so on in the TRM.

- Does the GPMC_CLK works and been driven without a proper setup in GPMC_CONFIG7_0?

- In "66AK2G0x_pinmux_data.c" the region: static pinmuxPerCfg_t gGpmc0PinCfg[] =

does not include PIN_GPMC_CLK and I think that could be an error.

When testing there is now activity on CSn_0 or GPMC_CLK.

Hopefully someone could give me something to continue the troubleshooting.

Kind regards

Fredrik

  • I've forwarded your query to the software experts. Their feedback should be posted here.

    BR
    Tsvetolin Shulev
  • Hi Frederik,

    I will jump in until experts are back from vacation...

    >>- How to configure the GPMC_CONFIG7_0 register properly for this case? I don't need much of memory space so the smallest 16MB is okay (1111 for the MASKADRESS field I guess).

    Yes, that should be fine. If smaller memory is available and not fully decoded it will just appear mirrored several times in device mem map.

    >>- What should I put in BASEADRESS field? The memory map specifies that GPMC_0_DATA has physical 40-bit adress between 00 3000 0000h and 006FFF FFFF

    As long as you don't have other GPMC CSx in use it doesn't really matter. You can use any value that then defines the start of that CS region in your mem map. Table 7-565 defines the bit mapping.

    I am not sure on the CLK question but if you can measure a signal I assume it is active. The clock logic probably does not check for valid combinations of config settings. The effect may be an interface with weird timing... So you need to define the GPMC config according to interface timing implemented in FPGA. Something we don't know...

    What is actually not working here?

    Regards,

    Frank

  • Hello

    We have done a set up and then making an access but receiving:

    ERRORNOTSUPPADD in the GPMC_ERR_TYPE register. Our conclusion is that something in GPMC_CONFIG7 is not correct.

    I have another set of "GPMC_ConfigNorDefault" with my settings for FPGA-device but we got the same problems there so must be something internal in the SoC/ARM.

    I will attach the code here for you for you so that less missunderstanding occur.

    /Fredrik

    /*
     *  Copyright (C) 2013-2016 Texas Instruments Incorporated - http://www.ti.com/
     *
     *  Redistribution and use in source and binary forms, with or without
     *  modification, are permitted provided that the following conditions
     *  are met:
     *
     *    Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     *    Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the
     *    distribution.
     *
     *    Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
     *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
     *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
     *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
     *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
     *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
     *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
     *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
     *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
     *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
     *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *
     */
     /**
     *   \file    main.c
     *
     *   \brief   Test application for NOR read and write
     *
     */
    /* ========================================================================== */
    /*                             Include Files                                  */
    /* ========================================================================== */
    #include "stdio.h"
    #include "string.h"
    #include "stdint.h"
    #include <ti/csl/csl_types.h>
    #include "device.h"
    #include "nor.h"
    //#include <ti/csl/example/utils/uart_console/inc/uartConfig.h>
    #include <ti/csl/csl_gpmc.h>
    #include <ti/csl/soc.h>
    #include <ti/csl/hw_types.h>
    #include <66AK2G0x_pinmux.h>
    #include <board_internal.h>
    
    #define UARTConfigPuts(a,b,c)
    #define UARTConfigPutNum(a,b)
    
    /* ========================================================================== */
    /*                                 Macros                                     */
    /* ========================================================================== */
    #define BUF_SIZE (32 * 1024)
    #define GPMC_CS0 0
    #define FLASH_BLOCK_SIZE (128 * 1024)
    
    #if !defined (__ARM_ARCH_7A__) && !defined (BUILD_GCC)
    #ifdef __cplusplus
    #pragma DATA_SECTION(".my_sect_ddr");
    #else
    #pragma DATA_SECTION(_srcBuffm, ".my_sect_ddr");
    #endif  /* #ifdef __cplusplus */
    uint8_t       _srcBuffm[FLASH_BLOCK_SIZE];
    #else
    uint8_t __attribute__((section(".my_sect_ddr"))) _srcBuffm[FLASH_BLOCK_SIZE];
    #endif
    
    /*To use UARTConfigPuts function for prints*/
    #if (defined (SOC_AM572x)) || (defined (SOC_AM571x))
    uint32_t uartBaseAddr = CSL_MPU_UART1_REGS;
    #endif
    #if defined (SOC_TDA2EX) || defined (SOC_DRA72x) || defined (SOC_TDA2XX) || defined (SOC_TDA2PX) || defined (SOC_DRA75x)
    uint32_t uartBaseAddr = SOC_UART1_BASE;
    #endif
    #if defined (SOC_TDA3XX) || defined (SOC_DRA78x)
    uint32_t uartBaseAddr = SOC_UART3_BASE;
    #endif
    
    /* ========================================================================== */
    /*                            Global Variables                                */
    /* ========================================================================== */
    signed char  *srcBuffm;
    unsigned int  NORStart = NOR_BASE;
    
    /* ========================================================================== */
    /*                          Function Declarations                             */
    /* ========================================================================== */
    static void NorTest(void);
    static int32_t local_DEBUGprintString(const char *s);
    
    /* ========================================================================== */
    /*                          Function Definitions                              */
    /* ========================================================================== */
     void padConfig_prcmEnable()
    {
    #if defined (SOC_AM572x) || defined (SOC_AM571x)
        /*Pad configurations */
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_UART1_RXD,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_UART1_TXD,0x00000000);
        /*Pad configurations*/
        /*GPMC Data lines AD0-AD15*/
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD0,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD1,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD2,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD3,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD4,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD5,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD6,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD7,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD8,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD9,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD10,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD11,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD12,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD13,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD14,0x00050000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_AD15,0x00050000);
        /*GPMC Add lines A0-A27*/
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A0,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A1,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A2,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A3,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A4,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A5,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A6,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A7,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A8,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A9,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A10,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A11,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A12,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A13,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A14,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A15,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A16,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A17,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A18,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A19,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A20,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A21,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A22,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A23,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A24,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A25,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A26,0x00040000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_A27,0x00040000);
       /*GPMC chip select*/
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_CS0,0x00060000);
         /*GPMC control lines*/
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_ADVN_ALE,0x00060000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_OEN_REN,0x00070000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_WEN,0x00070000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_BEN0,0x00070000);
        HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_GPMC_WAIT0,0x000F0000);
    #endif
    #if defined (SOC_TDA2XX) || defined (SOC_TDA2PX) || defined (SOC_TDA2EX) || defined (SOC_DRA72x) || defined (SOC_DRA75x)
    /*Pad configurations */
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_UART1_RXD,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_UART1_TXD,0x00000000);
        /*Pad configurations*/
        /*GPMC Data lines AD0-AD15*/
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_AD0,0x00050000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_AD1,0x00050000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_AD2,0x00050000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_AD3,0x00050000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_AD4,0x00050000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_AD5,0x00050000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_AD6,0x00050000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_AD7,0x00050000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_AD8,0x00050000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_AD9,0x00050000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_AD10,0x00050000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_AD11,0x00050000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_AD12,0x00050000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_AD13,0x00050000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_AD14,0x00050000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_AD15,0x00050000);
        /*GPMC Add lines A0-A27*/
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A0,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A1,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A2,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A3,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A4,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A5,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A6,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A7,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A8,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A9,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A10,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A11,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A12,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A13,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A14,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A15,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A16,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A17,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A18,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A19,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A20,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A21,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A22,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A23,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A24,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A25,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A26,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_A27,0x00040000);
       /*GPMC chip select*/
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_CS0,0x00060000);
         /*GPMC control lines*/
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_ADVN_ALE,0x00060000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_OEN_REN,0x00070000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_WEN,0x00070000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_BEN0,0x00070000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_GPMC_WAIT0,0x000F0000);
    #endif
    #if defined (SOC_TDA3XX) || defined (SOC_DRA78x)
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_SPI1_SCLK,0x00040001);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_SPI1_CS0,0x00000001);
        /*Pad configurations*/
        /*GPMC Data lines AD0-AD15*/
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_GPMC_AD0,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_GPMC_AD1,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_GPMC_AD2,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_GPMC_AD3,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_GPMC_AD4,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_GPMC_AD5,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_GPMC_AD6,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_GPMC_AD7,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_GPMC_AD8,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_GPMC_AD9,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_GPMC_AD10,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_GPMC_AD11,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_GPMC_AD12,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_GPMC_AD13,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_GPMC_AD14,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_GPMC_AD15,0x00040000);
        /*GPMC Add lines A0-A27*/
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VOUT1_D16,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VOUT1_D17,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VOUT1_D18,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VOUT1_D19,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VOUT1_D20,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VOUT1_D21,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VOUT1_D22,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VOUT1_D23,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VIN1A_D8,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VIN1A_D9,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VIN1A_D10,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VIN1A_D11,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VIN1A_D12,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VIN1A_D13,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VIN1A_D14,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VIN1A_D15,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_UART1_CTSN,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_UART1_RTSN,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_UART2_CTSN,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_UART2_RTSN,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VOUT1_D8,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VOUT1_D9,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VOUT1_D10,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VOUT1_D11,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VOUT1_D12,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VOUT1_D13,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VOUT1_D14,0x00040003);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_VOUT1_D15,0x00040003);
       /*GPMC chip select*/
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_GPMC_CS0,0x00040000);
         /*GPMC control lines*/
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_GPMC_ADVN_ALE,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_GPMC_OEN_REN,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_GPMC_WEN,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_GPMC_BEN0,0x00040000);
        HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_GPMC_WAIT0,0x00040000);
    #endif
        uint32_t v;
        uint32_t a=0, b=0;
    
    /*    const uint32_t* BOOTCFG_MAIN_PLL_CTL0 = (uint32_t*)0x02620350;
        const uint32_t* SECCTL = (uint32_t*)0x02130108;
    
        v = *BOOTCFG_MAIN_PLL_CTL0;
    
    
        // Enable Power domain
    
        while (*(uint32_t*)0x02350128 != 0);
    
    //    v = *(uint32_t*)0x02350000;
        v = *(uint32_t*)0x02350314;
    
        if (v & 0x1 == 0)
        {
            *(uint32_t*)0x02350314 |= 1;
            *(uint32_t*)0x02350120 |= 0x20;
    
            while (*(uint32_t*)0x02350128 == 0)
                a++;
    
            while (*(uint32_t*)0x02350128 != 0)
                b++;
        }
    
        // Enable Power module
    
        while (*(uint32_t*)0x02350128 != 0);
    
        v = *(uint32_t*)0x02350824;
        v = *(uint32_t*)0x02350A24;
    
        if (v & 0x103 != 0x103)
        {
            *(uint32_t*)0x02350A24 |= 0x103;
            *(uint32_t*)0x02350120 |= 0x20;
    
            while (*(uint32_t*)0x02350128 == 0)
                a++;
    
            while (*(uint32_t*)0x02350128 != 0)
                b++;
        }
    
        // Test access to GPMC register
    
        v = HW_RD_REG32(GPMC_BASE+0x10);
    */
    
        /*Pad configurations*/
        /*GPMC Data lines AD0-AD15*/
        HW_WR_REG32(CSL_BOOT_CFG_REGS+PIN_GPMC_AD0,0x00010000);
    
    
        HW_WR_REG32(CSL_BOOT_CFG_REGS+PIN_GPMC_AD1,0x00010000);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+PIN_GPMC_AD2,0x00010000);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+PIN_GPMC_AD3,0x00010000);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+PIN_GPMC_AD4,0x00010000);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+PIN_GPMC_AD5,0x00010000);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+PIN_GPMC_AD6,0x00010000);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+PIN_GPMC_AD7,0x00010000);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+PIN_GPMC_AD8,0x00010000);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+PIN_GPMC_AD9,0x00010000);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+PIN_GPMC_AD10,0x00010000);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+PIN_GPMC_AD11,0x00010000);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+PIN_GPMC_AD12,0x00010000);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+PIN_GPMC_AD13,0x00010000);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+PIN_GPMC_AD14,0x00010000);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+PIN_GPMC_AD15,0x00010000);
        /*GPMC Add lines A0-A27*/
    /*    HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VOUT1_D16,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VOUT1_D17,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VOUT1_D18,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VOUT1_D19,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VOUT1_D20,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VOUT1_D21,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VOUT1_D22,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VOUT1_D23,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VIN1A_D8,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VIN1A_D9,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VIN1A_D10,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VIN1A_D11,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VIN1A_D12,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VIN1A_D13,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VIN1A_D14,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VIN1A_D15,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_UART1_CTSN,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_UART1_RTSN,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_UART2_CTSN,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_UART2_RTSN,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VOUT1_D8,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VOUT1_D9,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VOUT1_D10,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VOUT1_D11,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VOUT1_D12,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VOUT1_D13,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VOUT1_D14,0x00040003);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+CTRL_CORE_PAD_IO_VOUT1_D15,0x00040003);*/
       /*GPMC chip select*/
        HW_WR_REG32(CSL_BOOT_CFG_REGS+PIN_GPMC_CSN0,0x00010000);
         /*GPMC control lines*/
        HW_WR_REG32(CSL_BOOT_CFG_REGS+PIN_GPMC_ADVN_ALE,0x00010000);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+PIN_GPMC_OEN_REN,0x00010000);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+PIN_GPMC_WEN,0x00010000);
    //    HW_WR_REG32(CSL_BOOT_CFG_REGS+PIN_GPMC_BEN0,0x00040000);
        HW_WR_REG32(CSL_BOOT_CFG_REGS+PIN_GPMC_WAIT0,0x00010000);
    
        HW_WR_REG32(CSL_BOOT_CFG_REGS+PIN_GPMC_CLK,0x00160000);
    
    }
    
    static int32_t local_DEBUGprintString(const char *s)
    {
    #if !defined (__ARM_ARCH_7A__)
        printf(s);
    #else
    //    UARTConfigPuts(uartBaseAddr,(char *)s, -1);
    #endif
        return TRUE;
    }
    
    
    GPMC_Config_t GPMC_ConfigNorDefault = {
        /* SysConfig - ROM Code defaults */
        0x8,           /*0x0008,*/
        /* IRQEnable - ROM Code defaults */
        0x0000,
        /* TimeOutControl - ROM Code defaults */
        0xf01f0000,
        /* Config - ROM Code defaults */
        0x000a0000,
        {
            0x00001010,
            0x001e1e01,
            0x00090907,
            0xf071d0b,
            0x001c1f1f,
            0x8f070080,
            0x00000f40,
        },
    };
    
    #if 0
    GPMC_Config_t GPMC_ConfigPseudo_SRAM_FPGA_Default = {
    /* SysConfig */
    0x8,
    /* IRQEnable */
    0x0000,
    /* TimeOutControl */
    0x00000000,
    /* Config - */
    0x00000000,
    {
    //See external excel file for bit settings
    //Need to use macro for each bit field? look at evmc66x_gpmc.h and include or copy to device.h
    0x7d0f1100, /* Config 1 */
    0x00030401, /* Config 2 */
    0x00000000, /* Config 3 */
    0x02018022, /* Config 4 */
    0x00040400, /* Config 5 */
    0x00010184, /* Config 6 */
    0x00000f40, /* Config 7 */
    },
    };
    #endif
    
    #define GPMC_0_CFG 0x21818000
    #define GPMC_ERR_TYPE ((uint32_t*)0x21818048)
    
    int main(void)
    {
        uint32_t           baseAddr = GPMC_0_CFG;
        Nor_InitPrms_t     Nor_InitPrms;
        uint32_t v;
        int i;
    
        Board_PLLInit();
        Board_moduleClockInit();
        Board_pinmuxConfig();
    
        v = *(uint32_t*)0x21818014;
    
        /*MMC1 PAD Configuration*/
        padConfig_prcmEnable();
    
        /* Set the UART Parameters */
    /*    UARTConfigInit(uartBaseAddr, BAUD_RATE_115200, UART_WORD_LENGTH_8, UART_STOP_BIT_1, UART_NO_PARITY,
                       UART_16x_MODE);
    */
        GPMC_Init(&GPMC_ConfigNorDefault, GPMC_CS0);
    
        /* FOLLOWING IS NOR CHIP-SELECT CONFIGURATION */
    
        for (i = 0; i < 100; ++i)
        {
            if ((*GPMC_ERR_TYPE & 0x1) != 0)
            {
                *GPMC_ERR_TYPE = 0x1;
            }
    
            v = *(volatile uint8_t*)(0x30000000 + i*4);
        }
    
        v = *(volatile uint32_t*)0x30000020;
    
        *(volatile uint32_t*)0x30000000 = 45;
    
        UARTConfigPuts(uartBaseAddr,"\nNOR Flash Test App", -1);
    
        /* Initialize function pointer Default */
        NOR_InitParmsDefault(&Nor_InitPrms);
    
        Nor_InitPrms.norFlashInitPrintFxnPtr =
            (NOR_FlashInitPrintFxnPtr) (&local_DEBUGprintString);
        /* Initialize function pointer Default */
        NOR_Init(&Nor_InitPrms);
    
        /* Function to Test NOR Flash */
        NorTest();
    
        return 0;
    }
    
    static void NorTest(void)
    {
        NOR_InfoHandle    hNorInfo;
        uint32_t          baseAddress = 0;
        uint32_t          blockSize, blockAddr;
        uint32_t          count, i;
        uint32_t          flash_size;
        volatile uint32_t dstOffsetAddr;
        uint32_t          offset_addr, buf_size;
        signed char      *dst_addr;
        volatile uint32_t norTest = 0;
        uint32_t          retVal  = TRUE;
    
        srcBuffm = (signed char *) (_srcBuffm);
    
        while (1) {
            UARTConfigPuts(uartBaseAddr,
                "\nEnter the testcase number\n1: Read Manufacturer ID and Device ID of NOR\n2: Erase, Write/Read and Verify 1 block of NOR flash\n3: Erase, Write/Read and Verify entire NOR flash\nAny other number to quit\n",
                -1);
            norTest = 2;//UARTConfigGetNum(uartBaseAddr);
            UARTConfigPuts(uartBaseAddr,"\n", -1);
            if (norTest == 1)
            {
                UARTConfigPuts(uartBaseAddr,
                    "Running Test Case 1: Read Manufacturer ID and Device ID of NOR\n",
                    -1);
                /* Initialize NOR Flash */
                hNorInfo = NOR_open(NORStart, 2 /* 16 Bit */);
                if (hNorInfo == NULL)
                {
                    UARTConfigPuts(uartBaseAddr,"\tERROR: NOR Initialization failed.\r\n", -1);
                    retVal = FALSE;
                    break;
                }
                else
                {
                    UARTConfigPuts(uartBaseAddr,"\nTest Passed.\n", -1);
                }
            }
            else if (norTest == 2)
            {
                UARTConfigPuts(uartBaseAddr,
                    "\nRunning Test Case 2:Erase, Write/Read and Verify 1 block of NOR flash\n",
                    -1);
                hNorInfo = NOR_open(NORStart, 2 /* 16 Bit */);
                if (hNorInfo == NULL)
                {
                    UARTConfigPuts(uartBaseAddr,"\tERROR: NOR Initialization failed.\r\n", -1);
                    retVal = FALSE;
                    break;
                }
                /* Get NOR block size */
                NOR_getBlockInfo(hNorInfo, NORStart, &blockSize,
                                 &blockAddr);
    
                /* Set base address to start putting data at */
                baseAddress = hNorInfo->flashBase;
    
                /*Erase the entire NOR Flash*/
                if (NOR_erase(hNorInfo, baseAddress, FLASH_BLOCK_SIZE) != TRUE)
                {
                    UARTConfigPuts(uartBaseAddr,"\tERROR: Erasing NOR failed.\r\n", -1);
                    retVal = FALSE;
                    break;
                }
    
                /*
                 * Initialize the source address with a pattern
                 * initialize dst address with zero/another pattern (optional)
                 */
    
                for (count = 0U; count < (FLASH_BLOCK_SIZE); count++)
                {
                    srcBuffm[count] = (int) 0x55;
                }
                offset_addr = baseAddress;
    
                dstOffsetAddr = offset_addr;
                dst_addr      = (signed char *) dstOffsetAddr;
    
                /* Write the data pattern to the flash */
                if (NOR_writeBytes(hNorInfo, dstOffsetAddr, FLASH_BLOCK_SIZE,
                                   (uint32_t) srcBuffm) != TRUE)
                {
                    UARTConfigPuts(uartBaseAddr,"\tERROR: Writing NOR failed.\n", -1);
                    retVal = FALSE;
                    break;
                }
    
                for (i = 0; i < (FLASH_BLOCK_SIZE); i++)
                {
                    if (srcBuffm[i] != dst_addr[i])
                    {
                        retVal = FALSE;
                        UARTConfigPuts(uartBaseAddr,"\nError matching value at src and dst address\n",
                                 -1);
                        UARTConfigPuts(uartBaseAddr,"Value at src address ", -1);
                        UARTConfigPutNum(uartBaseAddr,(uint32_t) &srcBuffm[i]);
                        UARTConfigPuts(uartBaseAddr," is:", -1);
                        UARTConfigPutNum(uartBaseAddr,srcBuffm[i]);
                        UARTConfigPuts(uartBaseAddr,"\nValue at dst address ", -1);
                        UARTConfigPutNum(uartBaseAddr,(uint32_t) &dst_addr[i]);
                        UARTConfigPuts(uartBaseAddr," is:", -1);
                        UARTConfigPutNum(uartBaseAddr,dst_addr[i]);
                        break;
                    }
                }
                if (retVal == FALSE)
                {
                    UARTConfigPuts(uartBaseAddr,"\nError testing block : ", -1);
                    UARTConfigPuts(uartBaseAddr,"\nTest Failed.\n", -1);
                    break;
                }
                else
                {
                    UARTConfigPuts(uartBaseAddr,"\nTest Passed.\n", -1);
                }
            }
            else if (norTest == 3)
            {
                UARTConfigPuts(uartBaseAddr,
                    "\nRunning Test Case 3: Erase, Write/Read and Verify entire NOR flash",
                    -1);
                hNorInfo = NOR_open(NORStart, 2 /* 16 Bit */);
                if (hNorInfo == NULL)
                {
                    UARTConfigPuts(uartBaseAddr,"\tERROR: NOR Initialization failed.\r\n", -1);
                    retVal = FALSE;
                    break;
                }
                /* Get NOR block size */
                NOR_getBlockInfo(hNorInfo, NORStart, &blockSize,
                                 &blockAddr);
    
                UARTConfigPuts(uartBaseAddr,"NOR Init Done\n", -1);
    
                /* Set base address to start putting data at */
                baseAddress = hNorInfo->flashBase;
    
                /*Erase the entire NOR Flash*/
                if (NOR_erase(hNorInfo, baseAddress,
                              hNorInfo->flashSize) != TRUE)
                {
                    UARTConfigPuts(uartBaseAddr,"\tERROR: Erasing NOR failed.\r\n", -1);
                    retVal = FALSE;
                    break;
                }
    
                /*
                 * Initialize the source address with a pattern
                 * initialize dst address with zero/another pattern (optional)
                 */
    
                for (count = 0U; count < (FLASH_BLOCK_SIZE); count++)
                {
                    srcBuffm[count] = (int) 0x55;
                }
    
                /* Write the data pattern to the flash */
                flash_size  = hNorInfo->flashSize;
                offset_addr = baseAddress;
                buf_size    = FLASH_BLOCK_SIZE;
                while (flash_size != 0)
                {
                    dstOffsetAddr = offset_addr;
                    dst_addr      = (signed char *) dstOffsetAddr;
    
                    /* Write the data pattern to the flash */
                    if (NOR_writeBytes(hNorInfo, dstOffsetAddr, FLASH_BLOCK_SIZE,
                                       (uint32_t) srcBuffm) != TRUE)
                    {
                        UARTConfigPuts(uartBaseAddr,"\tERROR: Writing NOR failed.\n", -1);
                        retVal = FALSE;
                        break;
                    }
    
                    for (i = 0; i < (FLASH_BLOCK_SIZE); i++)
                    {
                        if (srcBuffm[i] != dst_addr[i])
                        {
                            retVal = FALSE;
                            UARTConfigPuts(uartBaseAddr,
                                "\nError matching value at src and dst address\n",
                                -1);
                            UARTConfigPuts(uartBaseAddr,"Value at src address ", -1);
                            UARTConfigPutNum(uartBaseAddr,(uint32_t) &srcBuffm[i]);
                            UARTConfigPuts(uartBaseAddr," is:", -1);
                            UARTConfigPutNum(uartBaseAddr,srcBuffm[i]);
                            UARTConfigPuts(uartBaseAddr,"\nValue at dst address ", -1);
                            UARTConfigPutNum(uartBaseAddr,(uint32_t) &dst_addr[i]);
                            UARTConfigPuts(uartBaseAddr," is:", -1);
                            UARTConfigPutNum(uartBaseAddr,dst_addr[i]);
                            break;
                        }
                    }
                    if (retVal == FALSE)
                    {
                        UARTConfigPuts(uartBaseAddr,"\nError testing block num: ", -1);
                        UARTConfigPutNum(uartBaseAddr,k);
                        break;
                    }
                    offset_addr += buf_size;
                    flash_size  -= buf_size;
    
                    UARTConfigPuts(uartBaseAddr,"Testing block no. ", -1);
                    UARTConfigPutNum(uartBaseAddr,k++);
                    UARTConfigPuts(uartBaseAddr," Completed\n", -1);
                }
                if (retVal == FALSE)
                {
                    break;
                }
            }
            else
            {
                break;
            }
        }
        if (retVal == FALSE)
        {
            UARTConfigPuts(uartBaseAddr,"\nTest Failed Exitting.\n", -1);
        }
        else
        {
            UARTConfigPuts(uartBaseAddr,"\nExiting the nor test\n", -1);
        }
    }
    /***************************** End Of File ***********************************/
    
    gpio_arm.cfg

  • Frederik,

    as this value 0x00000f40, /* Config 7 */ is also the reset default I don't think there is anything wrong with this. There might be a more general issue with mode setup or timing. I don't know what would cause such an error message and as such we need to wait until experts are back.

    Regards,
    Frank
  • Frederik,
    as usual a search helped...

    ERRORNOTSUPPADD occurs when an incoming system request address decoding does not match
    any valid chip-select region, or if two chip-select regions are defined as overlapped, or if a register file
    access is tried outside the valid address range of 1KB.

    So can you check your setup and code for this?
    Make sure you also check ERRORVALID bit when reading GPMC_ERR_TYPE.

    regards,
    Frank
  • Follow up by email