Part Number: AM4379
Tool/software: Linux
Hi all:
After I compiled a new U-BOOT, I burned the new SD card from the link :”processors.wiki.ti.com/.../Processor_SDK_Linux_create_SD_card_script
In the “Enter path for Boot Partition:“step ,I entered the folder path for my u-boot.img, as shown in the following figure
Then there are the following tips in the process of making the SD card:
After I finished the SD card, I checked the SD card boot partition and found that u-boot.img was not copied ,Only MLO file. How do I solve this problem? Thanks!