Part Number: AM5718
Other Parts Discussed in Thread: TPD12S016, TCA9800
Customer is designing AM5718 and looking at the AM5718 IDK but is currently bumping into some issues.
Looking at the HDMI portion of the schematic, it seems there’s a logic-levels mismatch between the AM5718 and TPD12S016 – please find below more details:
- TPD12S016
o Max Low Level Input Voltage (VIL) on SCL_A, SDA_A (Pag. 6 of Datasheet):
§ VIL = 0.082 x VCCA = 0.148V when VCCA = 1.8V
§ VIL = 0.082 x VCCA = 0.271V when VCCA = 3.3V
- AM5718
o Max Output Low Level Threshold open-drain at 3mA sink current (VOL3) (Pag. 168 of Datasheet)
§ VOL3 = 0.36V in standard mode at 1.8V
§ VOL3 = 0.4V in standard model at 3.3V
Same story holds true for other signals like CEC_A, CT_HPD and LS_OE on the TPS12S016. Please let me know your comments,.