Part Number: AM5728
Tool/software: Linux
Hi,
I am posting this for one of our customers.
"
I am capturing YUYV format camera frames from the VIP port on the AM5728. I am submitting those frames to the GC320 with the goal of format converting them to RGBA frames. The Galcore driver version is 5.0.11.33433. I am passing a V4L2 DMABUF directly to the GC320 and for debugging I save the raw YUYV file before and after the GC320 rendering. The input frame is 640x480 YUYV, and the output 640x480 RGBA. I've attached the images below. The image on the left is the YUYV from the camera ( reddish due to Ubuntu's image viewer ), and the image on the right is the RGBA frame converted by the GC320. It is apparent that the GC320 "Kind-Of" converts the image - the top half looks good. However, the bottom half of the image is some sort of artifact. This leads me to believe my configuration for the conversion using the GC320 API is wrong. I have studied the GC320 examples as part of the Arago/Yocto ti-gc320-test samples and have put my GC320 Conversion code below - I would greatly appreciate any help understanding what is wrong with it.
"
(will send attachment in separate post)
GC320 Format function:
/**
* gc320 renderFormatConvertYUYVtoRGBA()
* Purpose: Perform a render cycle for converting frame from YUYV to RGBA
*
* @return Return bool success or failure
*/
gctBOOL Gc320::renderFormatConvertYUYVtoRGBA() {
gceSTATUS status;
// Destination Rectangle
gcsRECT targetRect;
gcsRECT sourceRect;
// Destination Rectangle
targetRect.left = 0;
targetRect.top = 0;
targetRect.right = FRAME_WIDTH; // These affect the output image ( destination rect )
targetRect.bottom = FRAME_HEIGHT; // These affect the output image ( destination rect )
// Source Rectangle
sourceRect.left = 0;
sourceRect.top = 0;
sourceRect.right = FRAME_WIDTH; // These affect the input image ( source rect )
sourceRect.bottom = FRAME_HEIGHT; // These affect the input image ( source rect )
QElapsedTimer timer;
timer.restart();
// Set clipping rect for destination rectangle
gcmONERROR(gco2D_SetClipping(m_Engine2d, &targetRect));
// set kernel size
gcmONERROR(gco2D_SetKernelSize(m_Engine2d, 1, 1));
gcmONERROR(gco2D_FilterBlitEx2(m_Engine2d,
(gctUINT32_PTR)&m_SrcPhysAddr, 1,
(gctUINT32_PTR)&m_SrcStride, 1,
gcvLINEAR, m_SrcFormat, gcvSURF_0_DEGREE,
m_SrcWidth, m_SrcHeight, (gcsRECT_PTR)&sourceRect,
(gctUINT32_PTR)&m_DstPhysAddr, 1, (gctUINT32_PTR)&m_DstStride, 1,
gcvLINEAR, m_DstFormat, gcvSURF_0_DEGREE,
m_DstWidth, m_DstHeight, (gcsRECT_PTR)&targetRect,
gcvNULL));
gcmONERROR(gco2D_Flush(m_Engine2d));
// Commit the current command buffer to hardware and wait until the hardware is finished
gcmONERROR(gcoHAL_Commit(m_Hal, gcvTRUE));
qDebug() << "Rendered: " << timer.elapsed();
#if 1
////////////////////////////////////////////////////////////////////////////////
// Save RGB24
{
// convert -depth 8 -size 640x480+0 RGBA:gc320.rgb gc320.png ; eog gc320.png
qDebug() << QString("Writing the frame out to /home/root/gc320.rgb");
QString filename = QString("/home/root/gc320.rgb");
QFile d(filename);
d.open(QFile::WriteOnly);
QDataStream ds(&d);
qDebug() << "Writing data now...";
ds.writeRawData((const char*)m_DstVirtAddr,FRAME_WIDTH*FRAME_HEIGHT*4);
d.flush();
d.close();
sync();
qDebug() << "Done writing";
}
sleep(100);
#endif
return gcvTRUE;
OnError:
fprintf(stderr,"%s(%d) failed:%s\n",__FUNCTION__, __LINE__, gcoOS_DebugStatus2Name(status));
return gcvFALSE;
}
Linux Kernel Version:
uname -r
4.4.41
GC320 Galcore Driver Version:
cd /lib/modules/4.4.41/extra ; insmod galcore.ko baseAddress=0x80000
000 physSize=0x80000000
[ 8014.626644] GC320 IRQ: 304
[ 8014.629403] Galcore version 5.0.11.33433
Regards,
--Gunter