Hi all
For a new PCB design we are looking for a fast LVDS / Ethernet data Gateway. Instead of using a FPGA SoC device the Sitara AM437x Processors might be a good option.
So, is there a good and direct connect LVDS signals to the processor, implement a user protocol and do processing?
Specs:
two LVDS pairs with embedded clock, up and down communication (two LVDS Links), line frequency ~200MHz
user defined protocol, Ser/des, balanced signals
Is there a reference design or app note to start with?
Do I need to connect to the display port or are there any dedicated GPIOs?
Best regards