This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5728: GP EVM boot issue

Part Number: AM5728

Tool/software: Linux

Hello,

I am using EVM board of AM5728.

I have downloaded SDK of it from link as below:

http://software-dl.ti.com/processor-sdk-linux/esd/AM57X/latest/index_FDS.html

I have follow steps to flash sd_card as described in link as below:

Then,i have inserted SD_CARD to EVM.Then,connect usb cable with my system and setup serial communication.

And when start module i can see debug print on the terminal as below:

[ 3.464492] mmcblk1: mmc1:0001 S10004 3.56 GiB

[ 3.474667] mmcblk1boot0: mmc1:0001 S10004 partition 1 4.00 MiB

[ 3.484833] mmcblk1boot1: mmc1:0001 S10004 partition 2 4.00 MiB

[ 3.485485] mmcblk1: p1 p2 p3[ 3.498383] Console: switching to colour frame buffer device 100x30

[ 3.535441] omapdrm omapdrm.0: fb0: omapdrm frame buffer device

[ 3.541573] mmc0: error -110 whilst initialising SD card

[ 3.581810] input: gpio_keys as /devices/platform/gpio_keys/input/input0

[ 3.588758] hctosys: unable to open rtc device (rtc0)

[ 3.595548] aic_dvdd_fixed: disabling

[ 3.599240] vmmcwl_fixed: disabling

[ 3.603176] ldousb: disabling

[ 3.606408] ALSA device list:

[ 3.609386] No soundcards found.

[ 3.613462] Waiting for root device PARTUUID=7846ae34-02...

Now,here my device has hang up.

What should i do?

If any changes or configuration require,please tell me.

Thanks in advance.