Part Number: AM3352
Other Parts Discussed in Thread: TLV320AIC3106
Hi,
I previously raised a ticket in the data converters forum for details on interfacing a AM335x with some TLV320AIC3106 codecs in a TDM topology (https://e2e.ti.com/support/data_converters/audio_converters/f/64/p/664803/2443731). I'd like to confirm if the AM335x can master the required bit and frame clocks, without usage of the external high speed master clock (AHCLKX). We require up to 6 timeslots in each direction at 8 kHz / 16-bits.
Although the TLV320AIC3106 only seems to care for the frame timing, bit offset and slot width, reading the AM335x it appears that a) the XCLK will need to be an integral division of the internal 24 MHz AUXCLK, and b) the frame timing is configurable only in multiples of timeslots and not bit clocks. I.e. not possible to generate the bit clock at a multiple of 768 kbps, and not possible to support partial timeslots?
I.e. I'd like to confirm that there isn't anything obvious I'm missing before we update the design to either supply an appropriate AHCLKX (e.g. as per the BBB design), or have one of the codecs master the timing.
Regards,
Paul