Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI-RTOS
Hello,
I am having a problem when trying to use the BSD sockets. Attached is a small test program (test.c) that demonstrates what I am seeing. The problem is that I get CONFLICTING TYPE errors for IP6N and for select.
I have set an include path in my project to the NDK BSD directory. The INCLUDE PATHS FOR THE PROJECT:
The COMPILER OUTPUT:
and the test.c program:
/*
* test.c
*
* Created on: Feb 21, 2018
* Author: MSTEINMETZ_LA
*/
#include <stdio.h>
#include <string.h>
#include <stdlib.h>
#include <ctype.h>
#include <stdbool.h>
#include <xdc/std.h>
#include <xdc/runtime/Error.h>
#include <xdc/runtime/System.h>
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/knl/Semaphore.h>
#include <ti/sysbios/knl/Mailbox.h>
#include <xdc/cfg/global.h>
#include <ti/ndk/inc/usertype.h> // need this for osif.h ???? HANDLE,
#include <sys/socket.h> // include for BSD sockets
#include <ti/ndk/inc/os/osif.h>
#include "assert.h"
int BSD_test(void) {
int SocketHandle;
int rslt;
int rtn_addrlen;
struct sockaddr_in addr;
int sockAddrSize;
int msglen;
struct sockaddr from;
unsigned char buf[1024];
/* create the socket -- for UDP messaging */
SocketHandle = socket(AF_INET,SOCK_DGRAM,0);
if (-1 == SocketHandle)
{
/* could not create socket...report problem and then kill task */
xdc_runtime_System_printf("SOCKET CREATE FAIL\n");
xdc_runtime_System_flush();
}
/* next bind the socket to an IP address and Port */
sockAddrSize = sizeof(struct sockaddr_in);
memset( (char *) &addr, 0, sockAddrSize);
addr.sin_family=AF_INET;
addr.sin_port = htons(123);
addr.sin_addr.s_addr = htonl(INADDR_ANY); /* should this be any or the local IP???*/
rslt = bind (SocketHandle, (struct sockaddr *) &addr, sockAddrSize);
if (-1 == rslt)
{
/* could not bind port...report problem and then kill task */
//Fatal_error("UDP ADDR Binding ERROR");
//taskDelete(taskIdSelf());
xdc_runtime_System_printf("SOCKET BIND FAIL\n");
xdc_runtime_System_flush();
}
/* next, park on the socket waiting for a PEER PRIM UDP */
rtn_addrlen = sizeof(struct sockaddr_in);
msglen = recvfrom(SocketHandle, buf, 1024, 0, &from, &rtn_addrlen);
return msglen;
}
If I remove the usertype.h include, then the missing typedef's generate errors in the osif.h file.
I am unsure what includes I need to resolve the CONFLICTING TYPE errors and also satisfies the necessary typedef's for the osif.h.
Any help you can provide would be greatly appreciated. Note that I did search the forum and found another thread about CONFLICTING TYPES, but it seemed that there was no clear answer and the person just hacked things to make it work. I am hoping there is a cleaner answer.
thanks,
Mark