Part Number: PROCESSOR-SDK-AM335X
Tool/software: Linux
Hi,TI!
I'm using u-boot 2017.01 from SDK 04.01.00.06, and I disable rtc in ./arch/arm/match-omap2/board.c (function void early_system_init (void)) ;
I can launch SPL with our custom board (which is based on am335x-SK-EVM,boot from 2 partition sd card),but hange on in uboot,the console messages as following:
CCCCCCCC
U-Boot SPL 2017.01-00360-gc6c77f9-dirty (Apr 10 2018 - 23:19:01)
Trying to boot from MMC1
reading uboot.env
** Unable to read "uboot.env" from mmc0:1 **
Using default environment
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img
U-Boot 2017.01-00360-gc6c77f9-dirty (Apr 10 2018 - 23:19:01 -0400)
CPU : AM335X-GP rev 2.1
Model: TI AM335x EVM-SK
DRAM: 256 MiB
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
reading uboot.env
** Unable to read "uboot.env" from mmc0:1 **
Using default environment
<ethaddr> not set. Validating first E-fuse MAC
Net: cpsw, usb_ether
data abort
pc : [<8ff6c1c0>] lr : [<8ff603e3>]
reloc pc : [<8081a1c0>] lr : [<8080e3e3>]
sp : 8df28248 ip : 8ffaca04 fp : 00000017
r10: 808607a0 r9 : 8df31ed8 r8 : 4030cdcc
r7 : 8ffac97c r6 : 8ffac8e8 r5 : 8ffac980 r4 : 0f752000
r3 : 44e3e000 r2 : b0010000 r1 : 8ffac9c4 r0 : 00000000
Flags: nZcv IRQs off FIQs on Mode SVC_32
Resetting CPU ...
resetting ...
CCCCCCCC
What is causing the crash?
A solution or insight would be appreciated.
Best regards
Lily Chen