Other Parts Discussed in Thread: AMIC110, AM3359
Tool/software: TI-RTOS
Hi,
for some days I now try to get a second I²C module working in our Profinet project. We like to use the second module "I2C1" on pins E17 and E18 (pinmode 3).
-
I always read that we should use the PINMUX tool and a corresponding ".pinmux" file. But neither does that example have a "*.pinmux" file, nor does the SDK have one for the "iceAMIC110". The SDK file "am335x_amic11x_pinmux_data.c" – which states that it is auto-created by TI PinMux and seems to be used in that example – is also not importable into the PINMUX tool.
-
Why is Starterware necessary for that process? I didn’t need starterware for doing my SPI stuff, for example. It’s really hard to understand how this is handled and also the file "starterware/board/am335x/am335x_amic110.c" contains stuff for an I2C rotary switch – which isn’t even on the board…?!
-
I now tried to edit that "am335x_amic11x_pinux_data.c" file by hand, I removed the Ethercat-related code of the two pins E17 and E18 (those pins actually should be implemented in some generic way, as it’s not possible for me to tell if they’re actually used by Profinet or not) and added code for a second I²C module (`gI2c1PinCfg[]` / `gI2cPinCfg[]`), like it’s done in the MCSPI code below that. [Here is my file:
]/** * Note: This file was auto-generated by TI PinMux on 3/16/2017 at 12:53:28 AM. * * \file amic11x_pinmux_data.c * * \brief This file contains the pin mux configurations for the boards. * These are prepared based on how the peripherals are extended on * the boards. * * \copyright Copyright (CU) 2017 Texas Instruments Incorporated - * http://www.ti.com/ */ /* ========================================================================== */ /* Include Files */ /* ========================================================================== */ #include "types.h" #include "pinmux.h" #include "am335x_pinmux.h" /** Peripheral Pin Configurations */ #ifndef BUILDCFG_MOD_ADC #define BUILDCFG_MOD_ADC #endif /* BUILDCFG_MOD_ADC */ #ifndef BUILDCFG_MOD_PRU_ICSS #define BUILDCFG_MOD_PRU_ICSS #endif /* BUILDCFG_MOD_PRU_ICSS */ #ifndef BUILDCFG_MOD_I2C #define BUILDCFG_MOD_I2C #endif /* BUILDCFG_MOD_I2C */ #ifndef BUILDCFG_MOD_MCSPI #define BUILDCFG_MOD_MCSPI #endif /* BUILDCFG_MOD_MCSPI */ #ifndef BUILDCFG_MOD_GPIO #define BUILDCFG_MOD_GPIO #endif /* BUILDCFG_MOD_GPIO */ #ifndef BUILDCFG_MOD_MCASP #define BUILDCFG_MOD_MCASP #endif /* BUILDCFG_MOD_MCASP */ #ifndef BUILDCFG_MOD_GLUE #define BUILDCFG_MOD_GLUE #endif /* BUILDCFG_MOD_GLUE */ #ifndef BUILDCFG_MOD_EMIF #define BUILDCFG_MOD_EMIF #endif /* BUILDCFG_MOD_EMIF */ #ifndef BUILDCFG_MOD_UART #define BUILDCFG_MOD_UART #endif /* BUILDCFG_MOD_UART */ #ifndef BUILDCFG_MOD_OSC #define BUILDCFG_MOD_OSC #endif /* BUILDCFG_MOD_OSC */ #ifndef BUILDCFG_MOD_RTC #define BUILDCFG_MOD_RTC #endif /* BUILDCFG_MOD_RTC */ #ifndef BUILDCFG_MOD_DEBUGSS #define BUILDCFG_MOD_DEBUGSS #endif /* BUILDCFG_MOD_DEBUGSS */ #if defined(BUILDCFG_MOD_ADC) static pinmuxPerCfg_t gAdc0PinCfg[] = { {PINMUX_INVALID_PIN} }; static pinmuxModuleCfg_t gAdcPinCfg[] = { {0, TRUE, gAdc0PinCfg}, {CHIPDB_INVALID_INSTANCE_NUM} }; #endif /* if defined(BUILDCFG_MOD_ADC) */ #if defined(BUILDCFG_MOD_PRU_ICSS) static pinmuxPerCfg_t gPru_icss1PinCfg[] = { { /* MDIO_PRUSS1 -> pr1_mdio_mdclk -> V12 */ PIN_GPMC_CLK, (uint16_t)PINMUX_SS_PRU_ICSS_MDIO, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN) & (~PIN_PULL_TYPE_SEL & ~PIN_RX_ACTIVE)) \ ) \ }, { /* MDIO_PRUSS1 -> pr1_mdio_data -> T13 */ PIN_GPMC_CSN3, (uint16_t)PINMUX_SS_PRU_ICSS_MDIO, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MII0_PRUSS1 -> pr1_mii_mt0_clk -> R1 */ PIN_LCD_DATA0, (uint16_t)PINMUX_SS_PRU_ICSS_MII0, \ ( \ PIN_MODE(2) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MII0_PRUSS1 -> pr1_mii0_txd0 -> T2 */ PIN_LCD_DATA5, (uint16_t)PINMUX_SS_PRU_ICSS_MII0, \ ( \ PIN_MODE(2) | \ ((PIN_PULL_UD_EN) & (~PIN_PULL_TYPE_SEL & ~PIN_RX_ACTIVE)) \ ) \ }, { /* MII0_PRUSS1 -> pr1_mii0_txd1 -> T1 */ PIN_LCD_DATA4, (uint16_t)PINMUX_SS_PRU_ICSS_MII0, \ ( \ PIN_MODE(2) | \ ((PIN_PULL_UD_EN) & (~PIN_PULL_TYPE_SEL & ~PIN_RX_ACTIVE)) \ ) \ }, { /* MII0_PRUSS1 -> pr1_mii0_txd2 -> R4 */ PIN_LCD_DATA3, (uint16_t)PINMUX_SS_PRU_ICSS_MII0, \ ( \ PIN_MODE(2) | \ ((PIN_PULL_UD_EN) & (~PIN_PULL_TYPE_SEL & ~PIN_RX_ACTIVE)) \ ) \ }, { /* MII0_PRUSS1 -> pr1_mii0_txd3 -> R3 */ PIN_LCD_DATA2, (uint16_t)PINMUX_SS_PRU_ICSS_MII0, \ ( \ PIN_MODE(2) | \ ((PIN_PULL_UD_EN) & (~PIN_PULL_TYPE_SEL & ~PIN_RX_ACTIVE)) \ ) \ }, { /* MII0_PRUSS1 -> pr1_mii0_rxd0 -> U4 */ PIN_LCD_DATA11, (uint16_t)PINMUX_SS_PRU_ICSS_MII0, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MII0_PRUSS1 -> pr1_mii0_rxd1 -> U3 */ PIN_LCD_DATA10, (uint16_t)PINMUX_SS_PRU_ICSS_MII0, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MII0_PRUSS1 -> pr1_mii0_rxd2 -> U2 */ PIN_LCD_DATA9, (uint16_t)PINMUX_SS_PRU_ICSS_MII0, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MII0_PRUSS1 -> pr1_mii0_rxd3 -> U1 */ PIN_LCD_DATA8, (uint16_t)PINMUX_SS_PRU_ICSS_MII0, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MII0_PRUSS1 -> pr1_mii0_txen -> R2 */ PIN_LCD_DATA1, (uint16_t)PINMUX_SS_PRU_ICSS_MII0, \ ( \ PIN_MODE(2) | \ ((PIN_PULL_UD_EN) & (~PIN_PULL_TYPE_SEL & ~PIN_RX_ACTIVE)) \ ) \ }, { /* MII0_PRUSS1 -> pr1_mii_mr0_clk -> V4 */ PIN_LCD_DATA14, (uint16_t)PINMUX_SS_PRU_ICSS_MII0, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MII0_PRUSS1 -> pr1_mii0_rxdv -> T5 */ PIN_LCD_DATA15, (uint16_t)PINMUX_SS_PRU_ICSS_MII0, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MII0_PRUSS1 -> pr1_mii0_rxer -> V3 */ PIN_LCD_DATA13, (uint16_t)PINMUX_SS_PRU_ICSS_MII0, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MII0_PRUSS1 -> pr1_mii0_rxlink -> V2 */ PIN_LCD_DATA12, (uint16_t)PINMUX_SS_PRU_ICSS_MII0, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MII0_PRUSS1 -> pr1_mii0_crs -> V5 */ PIN_LCD_PCLK, (uint16_t)PINMUX_SS_PRU_ICSS_MII0, \ ( \ PIN_MODE(2) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MII0_PRUSS1 -> pr1_mii0_col -> T10 */ PIN_GPMC_AD9, (uint16_t)PINMUX_SS_PRU_ICSS_MII0, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MII1_PRUSS1 -> pr1_mii_mt1_clk -> R13 */ PIN_GPMC_A0, (uint16_t)PINMUX_SS_PRU_ICSS_MII1, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MII1_PRUSS1 -> pr1_mii1_txd0 -> R14 */ PIN_GPMC_A4, (uint16_t)PINMUX_SS_PRU_ICSS_MII1, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN) & (~PIN_PULL_TYPE_SEL & ~PIN_RX_ACTIVE)) \ ) \ }, { /* MII1_PRUSS1 -> pr1_mii1_txd1 -> T14 */ PIN_GPMC_A3, (uint16_t)PINMUX_SS_PRU_ICSS_MII1, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN) & (~PIN_PULL_TYPE_SEL & ~PIN_RX_ACTIVE)) \ ) \ }, { /* MII1_PRUSS1 -> pr1_mii1_txd2 -> U14 */ PIN_GPMC_A2, (uint16_t)PINMUX_SS_PRU_ICSS_MII1, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN) & (~PIN_PULL_TYPE_SEL & ~PIN_RX_ACTIVE)) \ ) \ }, { /* MII1_PRUSS1 -> pr1_mii1_txd3 -> V14 */ PIN_GPMC_A1, (uint16_t)PINMUX_SS_PRU_ICSS_MII1, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN) & (~PIN_PULL_TYPE_SEL & ~PIN_RX_ACTIVE)) \ ) \ }, { /* MII1_PRUSS1 -> pr1_mii1_rxd0 -> V16 */ PIN_GPMC_A8, (uint16_t)PINMUX_SS_PRU_ICSS_MII1, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MII1_PRUSS1 -> pr1_mii1_rxd1 -> T15 */ PIN_GPMC_A7, (uint16_t)PINMUX_SS_PRU_ICSS_MII1, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MII1_PRUSS1 -> pr1_mii1_rxd2 -> U15 */ PIN_GPMC_A6, (uint16_t)PINMUX_SS_PRU_ICSS_MII1, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MII1_PRUSS1 -> pr1_mii1_rxd3 -> V15 */ PIN_GPMC_A5, (uint16_t)PINMUX_SS_PRU_ICSS_MII1, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MII1_PRUSS1 -> pr1_mii1_txen -> U17 */ PIN_GPMC_WPN, (uint16_t)PINMUX_SS_PRU_ICSS_MII1, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN) & (~PIN_PULL_TYPE_SEL & ~PIN_RX_ACTIVE)) \ ) \ }, { /* MII1_PRUSS1 -> pr1_mii_mr1_clk -> U16 */ PIN_GPMC_A9, (uint16_t)PINMUX_SS_PRU_ICSS_MII1, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MII1_PRUSS1 -> pr1_mii1_rxdv -> T16 */ PIN_GPMC_A10, (uint16_t)PINMUX_SS_PRU_ICSS_MII1, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MII1_PRUSS1 -> pr1_mii1_rxer -> V17 */ PIN_GPMC_A11, (uint16_t)PINMUX_SS_PRU_ICSS_MII1, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MII1_PRUSS1 -> pr1_mii1_rxlink -> U18 */ PIN_GPMC_BE1N, (uint16_t)PINMUX_SS_PRU_ICSS_MII1, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MII1_PRUSS1 -> pr1_mii1_crs -> R6 */ PIN_LCD_AC_BIAS_EN, (uint16_t)PINMUX_SS_PRU_ICSS_MII1, \ ( \ PIN_MODE(2) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MII1_PRUSS1 -> pr1_mii1_col -> T17 */ PIN_GPMC_WAIT0, (uint16_t)PINMUX_SS_PRU_ICSS_MII1, \ ( \ PIN_MODE(5) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* eCAP0_PRUSS1 -> pr1_ecap0_ecap_capin_apwm_o -> C18 */ PIN_ECAP0_IN_PWM0_OUT, (uint16_t)PINMUX_SS_PRU_ICSS_ECAP0, \ ( \ PIN_MODE(3) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, /* { // ECAT_PRUSS1 -> pr1_edc_sync0_out -> E18 PIN_UART0_CTSN, (uint16_t)PINMUX_SS_PRU_ICSS_ECAT, \ ( \ PIN_MODE(6) | \ ((PIN_PULL_UD_EN) & (~PIN_PULL_TYPE_SEL & ~PIN_RX_ACTIVE)) \ ) \ }, { // ECAT_PRUSS1 -> pr1_edc_sync1_out -> E17 PIN_UART0_RTSN, (uint16_t)PINMUX_SS_PRU_ICSS_ECAT, \ ( \ PIN_MODE(6) | \ ((PIN_PULL_UD_EN) & (~PIN_PULL_TYPE_SEL & ~PIN_RX_ACTIVE)) \ ) \ }, */ { // ECAT_PRUSS1 -> pr1_edc_latch0_in -> D18 PIN_UART1_CTSN, (uint16_t)PINMUX_SS_PRU_ICSS_ECAT, \ ( \ PIN_MODE(6) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* ECAT_PRUSS1 -> pr1_edc_latch1_in -> D17 */ PIN_UART1_RTSN, (uint16_t)PINMUX_SS_PRU_ICSS_ECAT, \ ( \ PIN_MODE(6) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, {PINMUX_INVALID_PIN} }; static pinmuxModuleCfg_t gPru_icssPinCfg[] = { {1, TRUE, gPru_icss1PinCfg}, {CHIPDB_INVALID_INSTANCE_NUM} }; #endif /* if defined(BUILDCFG_MOD_PRU_ICSS) */ #if defined(BUILDCFG_MOD_I2C) static pinmuxPerCfg_t gI2c0PinCfg[] = { { // I2C0 -> I2C0_SCL -> C16 PIN_I2C0_SCL, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { // I2C0 -> I2C0_SDA -> C17 PIN_I2C0_SDA, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, {PINMUX_INVALID_PIN} }; static pinmuxPerCfg_t gI2c1PinCfg[] = { { // E18: I2C1_SDA // HIER GEÄNDERT PIN_UART0_CTSN, 0, \ ( \ PIN_MODE(3) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { // E17: I2C1_SCL // HIER GEÄNDERT PIN_UART0_RTSN, 0, \ ( \ PIN_MODE(3) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, {PINMUX_INVALID_PIN} }; static pinmuxModuleCfg_t gI2cPinCfg[] = { {0, TRUE, gI2c0PinCfg}, {1, TRUE, gI2c1PinCfg}, {CHIPDB_INVALID_INSTANCE_NUM} }; #endif /* if defined(BUILDCFG_MOD_I2C) */ #if defined(BUILDCFG_MOD_MCSPI) static pinmuxPerCfg_t gMcspi0PinCfg[] = { { /* SPI0_flash -> spi0_sclk -> A17 */ PIN_SPI0_SCLK, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* SPI0_flash -> spi0_d0 -> B17 */ PIN_SPI0_D0, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* SPI0_flash -> spi0_d1 -> B16 */ PIN_SPI0_D1, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN) & (~PIN_PULL_TYPE_SEL & ~PIN_RX_ACTIVE)) \ ) \ }, { /* SPI0_flash -> spi0_cs0 -> A16 */ PIN_SPI0_CS0, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN) & (~PIN_PULL_TYPE_SEL & ~PIN_RX_ACTIVE)) \ ) \ }, { /* SPI0_flash -> spi0_cs1 -> C15 */ PIN_SPI0_CS1, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN) & (~PIN_PULL_TYPE_SEL & ~PIN_RX_ACTIVE)) \ ) \ }, {PINMUX_INVALID_PIN} }; static pinmuxPerCfg_t gMcspi1PinCfg[] = { { /* SPI1_launchpad -> spi1_sclk -> H16 */ PIN_GMII1_COL, 0, \ ( \ PIN_MODE(2) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* SPI1_launchpad -> spi1_d0 -> H17 */ PIN_GMII1_CRS, 0, \ ( \ PIN_MODE(2) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* SPI1_launchpad -> spi1_d1 -> J15 */ PIN_GMII1_RXER, 0, \ ( \ PIN_MODE(2) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* SPI1_launchpad -> spi1_cs0 -> H18 */ PIN_RMII1_REFCLK, 0, \ ( \ PIN_MODE(2) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, {PINMUX_INVALID_PIN} }; static pinmuxModuleCfg_t gMcspiPinCfg[] = { {0, TRUE, gMcspi0PinCfg}, {1, TRUE, gMcspi1PinCfg}, {CHIPDB_INVALID_INSTANCE_NUM} }; #endif /* if defined(BUILDCFG_MOD_MCSPI) */ #if defined(BUILDCFG_MOD_GPIO) static pinmuxPerCfg_t gGpio3PinCfg[] = { { /* GPIO3 -> gpio3[9] -> K18 */ PIN_GMII1_TXCLK, 9, \ ( \ PIN_MODE(7) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* GPIO3 -> gpio3[16] -> D12 */ PIN_MCASP0_AXR0, 16, \ ( \ PIN_MODE(7) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* GPIO3 -> gpio3[17] -> C12 */ PIN_MCASP0_AHCLKR, 17, \ ( \ PIN_MODE(7) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* GPIO3 -> gpio3[18] -> B12 */ PIN_MCASP0_ACLKR, 18, \ ( \ PIN_MODE(7) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* GPIO3 -> gpio3[19] -> C13 */ PIN_MCASP0_FSR, 19, \ ( \ PIN_MODE(7) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* GPIO3 -> gpio3[20] -> D13 */ PIN_MCASP0_AXR1, 20, \ ( \ PIN_MODE(7) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, {PINMUX_INVALID_PIN} }; static pinmuxPerCfg_t gGpio0PinCfg[] = { { /* GPIO0 -> gpio0[16] -> J18 */ PIN_GMII1_TXD3, 16, \ ( \ PIN_MODE(7) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* GPIO0 -> gpio0[17] -> K15 */ PIN_GMII1_TXD2, 17, \ ( \ PIN_MODE(7) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* GPIO0 -> gpio0[19] -> A15 */ PIN_XDMA_EVENT_INTR0, 19, \ ( \ PIN_MODE(7) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* GPIO0 -> gpio0[20] -> D14 */ PIN_XDMA_EVENT_INTR1, 20, \ ( \ PIN_MODE(7) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* GPIO0 -> gpio0[27] -> U12 */ PIN_GPMC_AD11, 27, \ ( \ PIN_MODE(7) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, {PINMUX_INVALID_PIN} }; static pinmuxPerCfg_t gGpio1PinCfg[] = { { /* GPIO1 -> gpio1[1] -> V7 */ PIN_GPMC_AD1, 1, \ ( \ PIN_MODE(7) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* GPIO1 -> gpio1[12] -> T12 */ PIN_GPMC_AD12, 12, \ ( \ PIN_MODE(7) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* GPIO1 -> gpio1[13] -> R12 */ PIN_GPMC_AD13, 13, \ ( \ PIN_MODE(7) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* GPIO1 -> gpio1[14] -> V13 */ PIN_GPMC_AD14, 14, \ ( \ PIN_MODE(7) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* GPIO1 -> gpio1[15] -> U13 */ PIN_GPMC_AD15, 15, \ ( \ PIN_MODE(7) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* GPIO1 -> gpio1[30] -> U9 */ PIN_GPMC_CSN1, 30, \ ( \ PIN_MODE(7) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, {PINMUX_INVALID_PIN} }; static pinmuxPerCfg_t gGpio2PinCfg[] = { { /* GPIO2 -> gpio2[12] -> T3 */ PIN_LCD_DATA6, 12, \ ( \ PIN_MODE(7) | \ ((PIN_RX_ACTIVE) & (~PIN_PULL_UD_EN & ~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* GPIO2 -> gpio2[13] -> T4 */ PIN_LCD_DATA7, 13, \ ( \ PIN_MODE(7) | \ ((PIN_RX_ACTIVE) & (~PIN_PULL_UD_EN & ~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* GPIO2 -> gpio2[18] -> L17 */ PIN_GMII1_RXD3, 18, \ ( \ PIN_MODE(7) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* GPIO2 -> gpio2[19] -> L16 */ PIN_GMII1_RXD2, 19, \ ( \ PIN_MODE(7) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* GPIO2 -> gpio2[21] -> M16 */ PIN_GMII1_RXD0, 21, \ ( \ PIN_MODE(7) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* GPIO2 -> gpio2[27] -> F18 */ PIN_MMC0_DAT2, 27, \ ( \ PIN_MODE(7) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, {PINMUX_INVALID_PIN} }; static pinmuxModuleCfg_t gGpioPinCfg[] = { {3, TRUE, gGpio3PinCfg}, {0, TRUE, gGpio0PinCfg}, {1, TRUE, gGpio1PinCfg}, {2, TRUE, gGpio2PinCfg}, {CHIPDB_INVALID_INSTANCE_NUM} }; #endif /* if defined(BUILDCFG_MOD_GPIO) */ #if defined(BUILDCFG_MOD_MCASP) static pinmuxPerCfg_t gMcasp1PinCfg[] = { { /* MCASP1_launchpad -> mcasp1_aclkr -> K17 */ PIN_GMII1_TXD0, 0, \ ( \ PIN_MODE(4) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MCASP1_launchpad -> mcasp1_fsr -> L15 */ PIN_GMII1_RXD1, 0, \ ( \ PIN_MODE(4) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MCASP1_launchpad -> mcasp1_axr0 -> J16 */ PIN_GMII1_TXEN, 0, \ ( \ PIN_MODE(4) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* MCASP1_launchpad -> mcasp1_axr1 -> K16 */ PIN_GMII1_TXD1, 0, \ ( \ PIN_MODE(4) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, {PINMUX_INVALID_PIN} }; static pinmuxModuleCfg_t gMcaspPinCfg[] = { {1, TRUE, gMcasp1PinCfg}, {CHIPDB_INVALID_INSTANCE_NUM} }; #endif /* if defined(BUILDCFG_MOD_MCASP) */ #if defined(BUILDCFG_MOD_GLUE) static pinmuxPerCfg_t gGlue0PinCfg[] = { { /* GLUE -> nRESETIN_OUT -> A10 */ PIN_NRESETIN_OUT, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* GLUE -> nNMI -> B18 */ PIN_NNMI, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, {PINMUX_INVALID_PIN} }; static pinmuxModuleCfg_t gGluePinCfg[] = { {0, TRUE, gGlue0PinCfg}, {CHIPDB_INVALID_INSTANCE_NUM} }; #endif /* if defined(BUILDCFG_MOD_GLUE) */ #if defined(BUILDCFG_MOD_EMIF) static pinmuxPerCfg_t gEmif4PinCfg[] = { {PINMUX_INVALID_PIN} }; static pinmuxModuleCfg_t gEmifPinCfg[] = { {4, TRUE, gEmif4PinCfg}, {CHIPDB_INVALID_INSTANCE_NUM} }; #endif /* if defined(BUILDCFG_MOD_EMIF) */ #if defined(BUILDCFG_MOD_UART) static pinmuxPerCfg_t gUart0PinCfg[] = { { /* UART0_console -> uart0_rxd -> E15 */ PIN_UART0_RXD, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* UART0_console -> uart0_txd -> E16 */ PIN_UART0_TXD, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN) & (~PIN_PULL_TYPE_SEL & ~PIN_RX_ACTIVE)) \ ) \ }, {PINMUX_INVALID_PIN} }; static pinmuxPerCfg_t gUart1PinCfg[] = { { /* UART1_launchpad -> uart1_rxd -> D16 */ PIN_UART1_RXD, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* UART1_launchpad -> uart1_txd -> D15 */ PIN_UART1_TXD, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN) & (~PIN_PULL_TYPE_SEL & ~PIN_RX_ACTIVE)) \ ) \ }, {PINMUX_INVALID_PIN} }; static pinmuxModuleCfg_t gUartPinCfg[] = { {0, TRUE, gUart0PinCfg}, {1, TRUE, gUart1PinCfg}, {CHIPDB_INVALID_INSTANCE_NUM} }; #endif /* if defined(BUILDCFG_MOD_UART) */ #if defined(BUILDCFG_MOD_OSC) static pinmuxPerCfg_t gOsc0PinCfg[] = { {PINMUX_INVALID_PIN} }; static pinmuxModuleCfg_t gOscPinCfg[] = { {0, TRUE, gOsc0PinCfg}, {CHIPDB_INVALID_INSTANCE_NUM} }; #endif /* if defined(BUILDCFG_MOD_OSC) */ #if defined(BUILDCFG_MOD_RTC) static pinmuxPerCfg_t gRtc0PinCfg[] = { { /* RTC -> RTC_PORz -> B5 */ PIN_RTC_PORZ, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* RTC -> EXT_WAKEUP -> C5 */ PIN_EXT_WAKEUP, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN) & (~PIN_PULL_TYPE_SEL & ~PIN_RX_ACTIVE)) \ ) \ }, { /* RTC -> PMIC_POWER_EN -> C6 */ PIN_PMIC_POWER_EN, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* RTC -> ENZ_KALDO_1P8V -> B4 */ PIN_ENZ_KALDO_1P8V, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, {PINMUX_INVALID_PIN} }; static pinmuxModuleCfg_t gRtcPinCfg[] = { {0, TRUE, gRtc0PinCfg}, {CHIPDB_INVALID_INSTANCE_NUM} }; #endif /* if defined(BUILDCFG_MOD_RTC) */ #if defined(BUILDCFG_MOD_DEBUGSS) static pinmuxPerCfg_t gDebugss0PinCfg[] = { { /* JTAG -> TMS -> C11 */ PIN_TMS, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* JTAG -> TDI -> B11 */ PIN_TDI, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* JTAG -> TDO -> A11 */ PIN_TDO, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN) & (~PIN_PULL_TYPE_SEL & ~PIN_RX_ACTIVE)) \ ) \ }, { /* JTAG -> TCK -> A12 */ PIN_TCK, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* JTAG -> nTRST -> B10 */ PIN_NTRST, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* JTAG -> EMU0 -> C14 */ PIN_EMU0, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* JTAG -> EMU1 -> B14 */ PIN_EMU1, 0, \ ( \ PIN_MODE(0) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, { /* JTAG -> EMU4 -> A14 */ PIN_MCASP0_AHCLKX, 0, \ ( \ PIN_MODE(4) | \ ((PIN_PULL_UD_EN | PIN_RX_ACTIVE) & (~PIN_PULL_TYPE_SEL)) \ ) \ }, {PINMUX_INVALID_PIN} }; static pinmuxModuleCfg_t gDebugssPinCfg[] = { {0, TRUE, gDebugss0PinCfg}, {CHIPDB_INVALID_INSTANCE_NUM} }; #endif /* if defined(BUILDCFG_MOD_DEBUGSS) */ pinmuxBoardCfg_t gAMIC11xPinmuxData[] = { #if defined(BUILDCFG_MOD_ADC) {CHIPDB_MOD_ID_ADC, gAdcPinCfg}, #endif /* if defined(BUILDCFG_MOD_ADC) */ #if defined(BUILDCFG_MOD_PRU_ICSS) {CHIPDB_MOD_ID_PRU_ICSS, gPru_icssPinCfg}, #endif /* if defined(BUILDCFG_MOD_PRU_ICSS) */ #if defined(BUILDCFG_MOD_I2C) {CHIPDB_MOD_ID_I2C, gI2cPinCfg}, #endif /* if defined(BUILDCFG_MOD_I2C) */ #if defined(BUILDCFG_MOD_MCSPI) {CHIPDB_MOD_ID_MCSPI, gMcspiPinCfg}, #endif /* if defined(BUILDCFG_MOD_MCSPI) */ #if defined(BUILDCFG_MOD_GPIO) {CHIPDB_MOD_ID_GPIO, gGpioPinCfg}, #endif /* if defined(BUILDCFG_MOD_GPIO) */ #if defined(BUILDCFG_MOD_MCASP) {CHIPDB_MOD_ID_MCASP, gMcaspPinCfg}, #endif /* if defined(BUILDCFG_MOD_MCASP) */ #if defined(BUILDCFG_MOD_GLUE) {CHIPDB_MOD_ID_GLUE, gGluePinCfg}, #endif /* if defined(BUILDCFG_MOD_GLUE) */ #if defined(BUILDCFG_MOD_EMIF) {CHIPDB_MOD_ID_EMIF, gEmifPinCfg}, #endif /* if defined(BUILDCFG_MOD_EMIF) */ #if defined(BUILDCFG_MOD_UART) {CHIPDB_MOD_ID_UART, gUartPinCfg}, #endif /* if defined(BUILDCFG_MOD_UART) */ #if defined(BUILDCFG_MOD_OSC) {CHIPDB_MOD_ID_OSC, gOscPinCfg}, #endif /* if defined(BUILDCFG_MOD_OSC) */ #if defined(BUILDCFG_MOD_RTC) {CHIPDB_MOD_ID_RTC, gRtcPinCfg}, #endif /* if defined(BUILDCFG_MOD_RTC) */ #if defined(BUILDCFG_MOD_DEBUGSS) {CHIPDB_MOD_ID_DEBUGSS, gDebugssPinCfg}, #endif /* if defined(BUILDCFG_MOD_DEBUGSS) */ {CHIPDB_MOD_ID_INVALID} }; -
After editing that file, I tried to make use of that new module by including `PRCMModuleEnable (CHIPDB_MOD_ID_I2C, 1U, 0U);` and `PINMUXModuleConfig (CHIPDB_MOD_ID_I2C, 1U, NULL);` into my application code, which both return without errors. But `I2C_open ()` afterwards fails every time.
-
How should anyone tell, when to use "[…]/starterware/board/" files and when to use "[<PDK>]/board/" code? For some reason, the example uses the Starterware stuff (at least to some extent?). But why does also the PDK board abstractions exist? As far as I understand, Starterware is a deprecated SDK – but then why is the current Profinet example of the new AMIC processor partly based on the new PDK and partly based on the deprecated Starterware?
-
Could someone please give me some guidance in how to get a second I²C instance to work on the iceAMIC110 board?
-
I’d like to not having to rebuild the SDK or create a new board abstraction, but instead include that code part into the project, so that my colleagues don’t have to make changes to the SDK, just for enabling an additional module on a device.
- The Profinet example also imports "soc_am335x/I2C_soc.c" from the SDK ["<PDK>/packages/ti/drv/i2c/soc/am335x/I2C_soc.c"] with functions `I2C_socSetInitCfg ()` and `I2C_socGetInitCfg ()`, but these aren’t used anywhere. Why are files like these imported in the project, and should these maybe used? I assume that these are driver-interal and don’t understand why these are pulled into the project.