Part Number: PROCESSOR-SDK-AM437X
Hi all,
I have a custom board based on am437x-gp-evm. I am using ti-rt-Linux SDK, Processor SDK Linux for AM437x v04.02.00.09. I want to compile an OpenGL application for the target board but I am not able to build it. the error follows is:
arm-linux-gnueabihf-g++ test.cpp -o am335x_part1 -lGL -lGLU -lglut
test.cpp:1:21: fatal error: GL/glut.h: No such file or directory compilation terminated.
The sample program I am compiling is :
#include <GL/glut.h>
void display(void)
{
glClearColor(0,0,0,0);
glClear(GL_COLOR_BUFFER_BIT);
glBegin(GL_TRIANGLES);
{
glColor3f(1,0,0);
glVertex2f(0,0);
glColor3f(0,1,0);
glVertex2f(.5,0);
glColor3f(0,0,1);
glVertex2f(.5,.5);
}
glEnd();
glutSwapBuffers();
}
void reshape(int w, int h)
{
}
int main(int argc, char **argv) {
glutInit(&argc, argv);
glutInitDisplayMode(GLUT_DEPTH | GLUT_DOUBLE | GLUT_RGBA);
glutInitWindowPosition(200,200);
glutInitWindowSize(320,240);
glutCreateWindow("Part 1");
glutDisplayFunc(display);
glutReshapeFunc(reshape);
glutMainLoop();
return 0;
}
I have compiled programmes based on OpenGL-ES, but I want to know if OpenGL and glut support is there for this platform?
How can I build the OpenGL application?
best regards,
Vimal Kumar