Part Number: TDA2
Please follow the below steps to Train, Import and run OD use case in VSDK.
- Download pre-trained model (deploy.prototxt and caffemodel) from gitHub link. And update below parameters in the “deploy.prototxt”. (Otherwise, DSP will run slow)
- keep_top_k: 20
- confidence_threshold: 0.15
- Use the attached import config file with “tidl_model_import.out.exe” available in TIDL 01.01.00.00 release to generate NET and PRM files
- Build VSDK with below one line change. (original use case had only 4 classes, but this new model as 21 classes)
- File : vision_sdk\apps\src\rtos\alg_plugins\objectdetection\objectDrawLink_algPlugin.c
- Line : tempoutPutList->objDesc[tempoutPutList->numObjects].objType = (label - 1)%3;
- Copy the NET , PRM bin files along with AppImage and Video input files of OD use case. Select the TIDL OD use case to run and see the detection on the Display
Note :
- The release is mainly intended to give a complete reference for Train, Import, and run of OD use case in VSDK.
- The accuracy of this model will not be as good as the one available in the VSDK3.3 release. This model is trained using PASCAL VOC dataset.
- The VSDK demo model was trained using TI internal dataset and this is not available publicly so to re-produce the training step, we have trained this reference model using PASCAL VOC.
Regards,
Kumar.A.D