This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2EVM5777: Comparison between Sparse and Dense Model ?

Part Number: TDA2EVM5777


Hi,

I have copied object detection trained models from caffe-jacinto-models github repo ( github.com/.../ssd512x512_ds_PSP_dsFac_32_fc_0_hdDS8_1_kerMbox_3_1stHdSameOpCh_1)

And i am trying to compare the execustion time for Dense Model and Sparse Model.
As per the datasheet, Sparse model execution must be faster than dense model. But, I am getting different result.

Setup :
1. TDA2x EVM Board is connected to CCS using XDS560 JTAG.
2. Build and generated eve_test_dl_algo.out (release mode) for test app (in tidl folder)
3. Using CCS Load Program eve_test_dl_algo.out executed on EVE

Output:

1. Sparse Model:

TEST_REPORT_INIT_PROFILE_DATA : TSC cycles = 2117750600, SCTM VCOP BUSY cycles = 0, SCTM VCOP Overhead = 0
I/O Bytes : 0 ( 0 + 0 ) : 0 ( 0 + 0 )

Processing Frame Number : 0

TEST_REPORT_PROCESS_PROFILE_DATA : TSC cycles = 69244619476, SCTM VCOP BUSY cycles = 108141852, SCTM VCOP Overhead = 0
I/O Bytes : 0 ( 0 + 0 ) : 0 ( 0 + 0 )


- Execution Time = TSC cycles / EVE Frequncy
- Considering only PROCESS PROFILE DATA
- Execution Time: 129.4291953 seconds (EVE Frequncy: 535 MHz)


2. Dense Model:

TEST_REPORT_INIT_PROFILE_DATA : TSC cycles = 3165035504, SCTM VCOP BUSY cycles = 0, SCTM VCOP Overhead = 0
I/O Bytes : 0 ( 0 + 0 ) : 0 ( 0 + 0 )

Processing Frame Number : 0

TEST_REPORT_PROCESS_PROFILE_DATA : TSC cycles = 62898624182, SCTM VCOP BUSY cycles = 275218342, SCTM VCOP Overhead = 0
I/O Bytes : 0 ( 0 + 0 ) : 0 ( 0 + 0 )


- Execution Time = TSC cycles / EVE Frequncy
- Considering only PROCESS PROFILE DATA
- Execution Time: 117.5675218 seconds (EVE Frequncy: 535 MHz)

Whether this setup is correct ? 

Sparse Model execution time is more that Dense Model ?

Regards,

Sagar

Attached Log:

tidl_object_detection_eve_JTAG_emulation_log.zip

  • Hi Sagar,

    >>As per the datasheet, Sparse model execution must be faster than dense model. But, I am getting different result.

    Yes, but this not true for small image sizes as we optimised the dense convolution kernels (1x1 and 3x3) for small ROI processing.
    Please refer to FAQ 8 in the user guide for more information on these.

    Thanks,
    Praveen
  • Hi Praveen,

    If i want to reproduce the same result that TI has provided in the datasheet, Which models shall i compare and what should be procedure?
    Can you please provide me the link for Initial Model and Sparse Model ?
    And whether my setup (with JTAG) is correct to validate the same?

    Regards,
    Sagar
  • Hi Sagar,

    Please use the segmentation model bin files (jsegnet21) available in the release package to reproduce the profile numbers in datasheet.
    Link for models is github.com/.../caffe-jacinto-models.
    Yes, your setup looks fine.

    Thanks,
    Praveen
  • Hi I will check segmentation model files. But, I am specifically interested in object detection model comparison. Can you please share the link for that ?

    And I also While Importing, We get GigaMacs requirement for the model. Can we calculate the execution time for that model on EVE/DSP ?

    Assume that for a model GigaMacs requirement is 1.6 GMacs. And according to EVE datasheet , EVE can process 16 MACs per Cycle.
    So, Considering EVE Freq = 535MHz
    Execution Time = (Total Macs required / 16 ) * (1 / 535MHz) secs = 1.6 G /( 16 * 535 M) = 0.18 seconds

    Whether the above calculation is correct and Can we assume we will get actual execution time on board same or nearby to this value?

    Regards,
    Sagar
  • >> I am specifically interested in object detection model comparison. Can you please share the link for that ?
    Github link that I shared has both segmentation and SSD models.

    >> Whether the above calculation is correct and Can we assume we will get actual execution time on board same or nearby to this value?
    Yes, the calculation is correct, but considering the 16 MACs per Cycle is not correct, please refer to datasheet for actual MACs/cycle for different layers with different configuration. Do consider those values for calculating the execution time.

    Thanks,
    Praveen