Other Parts Discussed in Thread: AM3359, SYSBIOS
Tool/software: TI-RTOS
I'm back...
Let me detail my steps, so the TI support people can see the hours and hours and day and days wasted trying to make this stuff work...
Create a simple new project, in my case for BBB, as a "typical" Sys/Bios project. Include the symbols: am3359, SOC_AM335x, bbbAM335x and the packages EDMA and PDK.
Build it. Okay, we're happy. Except we can't do any board access. So add this:
#include <ti/board/board.h>
/* Call board init functions */
Board_initCfg boardCfg;
boardCfg = BOARD_INIT_PINMUX_CONFIG | BOARD_INIT_MODULE_CLOCK ;
Board_init(boardCfg);
No problem. But we get this, which is expected....
makefile:146: recipe for target 'WillNotBuild.out' failed ./main.o: In function `main': C:\Source\Embeded\Beagle\WillNotBuild\Debug/../main.c:39: undefined reference to `Board_init' collect2.exe: error: ld returned 1 exit status
But what follows isn't:
Okay, so go into the CFG file, and add this:
var Board = xdc.loadPackage('ti.board');
Board.Settings.boardName = "bbbAM335x";
And now when we build it, we get this:
C:\ti\pdk_am335x_1_0_7\packages\ti\board\lib\bbbAM335x\a8\release\ti.board.aa8fg(bbbAM335x_lld_init.oa8fg): In function `Board_uartStdioInit': bbbAM335x_lld_init.c:(.text.Board_uartStdioInit+0x10): undefined reference to `UART_stdioInit' collect2.exe: error: ld returned 1 exit status
So, based on what I learned from my post in e2e.ti.com/.../2560250 I also add this, in the correct location
var UartPackage = xdc.loadPackage('ti.drv.uart');
And try to build it. but now we get this:
makefile:146: recipe for target 'WillNotBuild.out' failed C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_stdio.oa8fg): In function `UART_stdioInit': UART_stdio.c:(.text.UART_stdioInit+0x50): undefined reference to `SemaphoreP_Params_init' UART_stdio.c:(.text.UART_stdioInit+0x70): undefined reference to `SemaphoreP_create' C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_drv.oa8fg): In function `UART_init': UART_drv.c:(.text.UART_init+0x20): undefined reference to `UART_config' UART_drv.c:(.text.UART_init+0x28): undefined reference to `UART_config' C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_drv.oa8fg): In function `UART_open': UART_drv.c:(.text.UART_open+0x4): undefined reference to `UART_config' UART_drv.c:(.text.UART_open+0x8): undefined reference to `UART_config' collect2.exe: error: ld returned 1 exit status gmake[1]: *** [WillNotBuild.out] Error 1
Well, UART_Config is something that the end user needs to supply. So I added a "DummyUARTc" file that supplies the missing symbols. But what is "SemaphoreP_Params_init"?? The Semaphore package is already present in the CFG file.
So I added these to the CFG file, again, in the correct place.
var socType = "am335x";
var osType = "tirtos";
var Csl = xdc.loadPackage('ti.csl');
Csl.Settings.deviceType = socType;
// ....
var Osal = xdc.useModule('ti.osal.Settings');
Osal.osType = osType;
Osal.socType = socType;
Now it's getting REALLY bad. The errors are now these:
makefile:147: recipe for target 'WillNotBuild.out' failed C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_v1.oa8fg): In function `UART_v1_callback': UART_v1.c:(.text.UART_v1_callback+0x68): undefined reference to `SemaphoreP_post' UART_v1.c:(.text.UART_v1_callback+0x70): undefined reference to `SemaphoreP_post' C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_v1.oa8fg): In function `UART_open_v1': UART_v1.c:(.text.UART_open_v1+0x40): undefined reference to `HwiP_disable' UART_v1.c:(.text.UART_open_v1+0x58): undefined reference to `HwiP_restore' UART_v1.c:(.text.UART_open_v1+0x18c): undefined reference to `Osal_RegisterInterrupt_initParams' UART_v1.c:(.text.UART_open_v1+0x1c0): undefined reference to `Osal_RegisterInterrupt' UART_v1.c:(.text.UART_open_v1+0x1d8): undefined reference to `SemaphoreP_Params_init' UART_v1.c:(.text.UART_open_v1+0x20c): undefined reference to `SemaphoreP_create' UART_v1.c:(.text.UART_open_v1+0x24c): undefined reference to `SemaphoreP_create' UART_v1.c:(.text.UART_open_v1+0x260): undefined reference to `HwiP_restore' C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_v1.oa8fg): In function `UART_close_v1': UART_v1.c:(.text.UART_close_v1+0x6c): undefined reference to `Osal_DeleteInterrupt' UART_v1.c:(.text.UART_close_v1+0x8c): undefined reference to `SemaphoreP_delete' UART_v1.c:(.text.UART_close_v1+0x98): undefined reference to `SemaphoreP_delete' C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_v1.oa8fg): In function `UART_writeCancelNoCB.isra.0': UART_v1.c:(.text.UART_writeCancelNoCB.isra.0+0x2c): undefined reference to `HwiP_disable' UART_v1.c:(.text.UART_writeCancelNoCB.isra.0+0x60): undefined reference to `HwiP_restore' UART_v1.c:(.text.UART_writeCancelNoCB.isra.0+0x6c): undefined reference to `HwiP_restore' C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_v1.oa8fg): In function `UART_readCancelNoCB.isra.3': UART_v1.c:(.text.UART_readCancelNoCB.isra.3+0x20): undefined reference to `HwiP_disable' UART_v1.c:(.text.UART_readCancelNoCB.isra.3+0x54): undefined reference to `HwiP_restore' UART_v1.c:(.text.UART_readCancelNoCB.isra.3+0x70): undefined reference to `HwiP_restore' C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_v1.oa8fg): In function `UART_charPut_v1.isra.5': UART_v1.c:(.text.UART_charPut_v1.isra.5+0x20): undefined reference to `Osal_delay' C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_v1.oa8fg): In function `UART_readPolling_v1': UART_v1.c:(.text.UART_readPolling_v1+0x50): undefined reference to `Osal_delay' C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_v1.oa8fg): In function `UART_read2_v1': UART_v1.c:(.text.UART_read2_v1+0x34): undefined reference to `_DebugP_assert' UART_v1.c:(.text.UART_read2_v1+0x5c): undefined reference to `HwiP_disable' UART_v1.c:(.text.UART_read2_v1+0x94): undefined reference to `HwiP_restore' UART_v1.c:(.text.UART_read2_v1+0x1fc): undefined reference to `SemaphoreP_pend' UART_v1.c:(.text.UART_read2_v1+0x224): undefined reference to `HwiP_restore' C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_v1.oa8fg): In function `UART_read_v1': UART_v1.c:(.text.UART_read_v1+0x30): undefined reference to `HwiP_disable' UART_v1.c:(.text.UART_read_v1+0x40): undefined reference to `HwiP_restore' UART_v1.c:(.text.UART_read_v1+0x78): undefined reference to `HwiP_restore' C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_v1.oa8fg): In function `UART_write2_v1': UART_v1.c:(.text.UART_write2_v1+0x30): undefined reference to `_DebugP_assert' UART_v1.c:(.text.UART_write2_v1+0x50): undefined reference to `HwiP_disable' UART_v1.c:(.text.UART_write2_v1+0x88): undefined reference to `HwiP_restore' UART_v1.c:(.text.UART_write2_v1+0x218): undefined reference to `SemaphoreP_pend' UART_v1.c:(.text.UART_write2_v1+0x254): undefined reference to `HwiP_restore' C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_v1.oa8fg): In function `UART_write_v1': UART_v1.c:(.text.UART_write_v1+0x30): undefined reference to `HwiP_disable' UART_v1.c:(.text.UART_write_v1+0x40): undefined reference to `HwiP_restore' UART_v1.c:(.text.UART_write_v1+0x78): undefined reference to `HwiP_restore' C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_stdio.oa8fg): In function `UART_stdioInit': UART_stdio.c:(.text.UART_stdioInit+0x50): undefined reference to `SemaphoreP_Params_init' UART_stdio.c:(.text.UART_stdioInit+0x70): undefined reference to `SemaphoreP_create' collect2.exe: error: ld returned 1 exit status
Getting really annoyed, and swearing at this eco-system, I start throwing EVERYTHING from my config file that I modified and was working based on the other post... That's mmu, profile, I2C, etc... Try another clean/rebuild. The results are still:
makefile:147: recipe for target 'WillNotBuild.out' failed C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_v1.oa8fg): In function `UART_v1_callback': UART_v1.c:(.text.UART_v1_callback+0x68): undefined reference to `SemaphoreP_post' UART_v1.c:(.text.UART_v1_callback+0x70): undefined reference to `SemaphoreP_post' C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_v1.oa8fg): In function `UART_open_v1': UART_v1.c:(.text.UART_open_v1+0x40): undefined reference to `HwiP_disable' UART_v1.c:(.text.UART_open_v1+0x58): undefined reference to `HwiP_restore' UART_v1.c:(.text.UART_open_v1+0x18c): undefined reference to `Osal_RegisterInterrupt_initParams' UART_v1.c:(.text.UART_open_v1+0x1c0): undefined reference to `Osal_RegisterInterrupt' UART_v1.c:(.text.UART_open_v1+0x1d8): undefined reference to `SemaphoreP_Params_init' UART_v1.c:(.text.UART_open_v1+0x20c): undefined reference to `SemaphoreP_create' UART_v1.c:(.text.UART_open_v1+0x24c): undefined reference to `SemaphoreP_create' UART_v1.c:(.text.UART_open_v1+0x260): undefined reference to `HwiP_restore' C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_v1.oa8fg): In function `UART_close_v1': UART_v1.c:(.text.UART_close_v1+0x6c): undefined reference to `Osal_DeleteInterrupt' UART_v1.c:(.text.UART_close_v1+0x8c): undefined reference to `SemaphoreP_delete' UART_v1.c:(.text.UART_close_v1+0x98): undefined reference to `SemaphoreP_delete' C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_v1.oa8fg): In function `UART_writeCancelNoCB.isra.0': UART_v1.c:(.text.UART_writeCancelNoCB.isra.0+0x2c): undefined reference to `HwiP_disable' UART_v1.c:(.text.UART_writeCancelNoCB.isra.0+0x60): undefined reference to `HwiP_restore' UART_v1.c:(.text.UART_writeCancelNoCB.isra.0+0x6c): undefined reference to `HwiP_restore' C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_v1.oa8fg): In function `UART_readCancelNoCB.isra.3': UART_v1.c:(.text.UART_readCancelNoCB.isra.3+0x20): undefined reference to `HwiP_disable' UART_v1.c:(.text.UART_readCancelNoCB.isra.3+0x54): undefined reference to `HwiP_restore' UART_v1.c:(.text.UART_readCancelNoCB.isra.3+0x70): undefined reference to `HwiP_restore' C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_v1.oa8fg): In function `UART_read2_v1': UART_v1.c:(.text.UART_read2_v1+0x5c): undefined reference to `HwiP_disable' UART_v1.c:(.text.UART_read2_v1+0x94): undefined reference to `HwiP_restore' UART_v1.c:(.text.UART_read2_v1+0x1fc): undefined reference to `SemaphoreP_pend' UART_v1.c:(.text.UART_read2_v1+0x224): undefined reference to `HwiP_restore' C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_v1.oa8fg): In function `UART_read_v1': UART_v1.c:(.text.UART_read_v1+0x30): undefined reference to `HwiP_disable' UART_v1.c:(.text.UART_read_v1+0x40): undefined reference to `HwiP_restore' UART_v1.c:(.text.UART_read_v1+0x78): undefined reference to `HwiP_restore' C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_v1.oa8fg): In function `UART_write2_v1': UART_v1.c:(.text.UART_write2_v1+0x50): undefined reference to `HwiP_disable' UART_v1.c:(.text.UART_write2_v1+0x88): undefined reference to `HwiP_restore' UART_v1.c:(.text.UART_write2_v1+0x218): undefined reference to `SemaphoreP_pend' UART_v1.c:(.text.UART_write2_v1+0x254): undefined reference to `HwiP_restore' C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_v1.oa8fg): In function `UART_write_v1': UART_v1.c:(.text.UART_write_v1+0x30): undefined reference to `HwiP_disable' UART_v1.c:(.text.UART_write_v1+0x40): undefined reference to `HwiP_restore' UART_v1.c:(.text.UART_write_v1+0x78): undefined reference to `HwiP_restore' C:\ti\pdk_am335x_1_0_7\packages\ti\drv\uart\lib\a8\release\ti.drv.uart.aa8fg(UART_stdio.oa8fg): In function `UART_stdioInit': UART_stdio.c:(.text.UART_stdioInit+0x50): undefined reference to `SemaphoreP_Params_init' UART_stdio.c:(.text.UART_stdioInit+0x70): undefined reference to `SemaphoreP_create' collect2.exe: error: ld returned 1 exit status gmake[1]: *** [WillNotBuild.out] Error 1
Really?? HWI_xxx symbols are missing?? OSAL_xxx symbols are missing?? Even though they are listed in the CFG file??
This is the RAT HOLE that I've been dragged down, simply trying to add ONE SINGLE function call to an otherwise childishly simple example program. And is why I normally throw my hands up, erase the ENTIRE project, and drag out the older version of StarterWare. At least I can link to those without this nightmare (and I can build the libs so I can debug them too... Not like the stuff in this PDK that won't build, and you can't pull into CCS and build debug versions - But that's another post, which also never got solved).
Here's the project.
.