Part Number: TMDSLCDK6748
Other Parts Discussed in Thread: OMAP-L138, TMS320C6748
Hi,
When using AISgen and CCS project NANDWriter_DSP to write a large image (68 KB or more) to the NAND Flash of the TMDSLCDK6748 board the tools do not report an error, but when restarting the board nothing happens. It works fine when the image is smaller (45 KB or less). Also the large image works fine when loaded with the debug probe.
Here are the hardware and software that are used:
- TMDSLCDK6748 board revision A7A: processors.wiki.ti.com/.../C6748_Development_Kit_(LCDK)
- AISgen d800k008 v1.13
- CCS project NANDWriter_DSP, with NAND width set to 16 bits
- CCS 7.2
What could be wrong?
Best regards,
Ad