This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TMDXEVM3358: GPIO read example

Part Number: TMDXEVM3358

Tool/software: Linux

Hi All, 

   I'm new to embedded Linux and Processor SDK Linux development so I wanted to ramp up my knwoledge with some basic program. Let's say I would like to use one of the pins on the EVM's EXT1 connector as input and inside my code I would like to read the logical state of this pin and print it out using the stdout. This is trivial on HW like Arduino, but I just can't figure out how I should do it on the EVM?

I'm going through the traininigs, wikis and documentation but I just can't find some hands-on example of this type of source code.

I would appreciate any type of help. 

Regards, 

Karol