Other Parts Discussed in Thread: TVP5158
Our processor is DRA74X, with 3.02.00.03 SDK version.
At our custom board, there is video converter(ADV7611), and it's 8-bit BT656 output directly connect to Vin-3a port of DRA74X. And DRA74X use i2c-1 to control this converter.
I already modify dts file to make a connection between vin3a & ADV7611. I can see /dev/video1 by " ls /dev/video* ", but after i use " v4l2-ctl --list-device ", there is no /dev/video1.
I also try to open it at my AP program, still fail. What is the possible reson to cause this?
Here is the boot log =>
U-Boot SPL 2016.05-g9694c57-dirty (Jul 06 2018 - 16:04:55)
DRA752-GP ES2.0
no pinctrl for hs200_1_8v
no pinctrl for ddr_1_8v
@SD max clock = 10000000@
*** Warning - bad CRC, using default environment
Trying to boot from MMC1
*** Warning - bad CRC, using default environment
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img
U-Boot 2016.05-g9694c57-dirty (Jul 06 2018 - 16:04:55 +0800)
CPU : DRA752-GP ES2.0
Model: TI DRA742
Board: DRA74x EVM REV
DRAM: 2 GiB
NAND: 256 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - bad CRC, using default environment
current ID is 7
Warning: fastboot.board_rev: unknown board revision
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid GPT ***
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid Backup GPT ***
ERROR: cannot find partition: 'userdata'
at arch/arm/cpu/armv7/omap-common/utils.c:199/mmc_get_part_size()
Warning: fastboot.userdata_size: unable to calc
SCSI: SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net:
Warning: ethernet@48484000 using MAC address from ROM
eth0: ethernet@48484000
Hit any key to stop autoboot: 0
load MAN2020_original.dtb
load MAN2020_3g
switch to partitions #0, OK
mmc0 is current device
@SD max clock = 10000000@
SD/MMC found on device 0
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
222 bytes read in 3 ms (72.3 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc0 ...
@SD max clock = 10000000@
switch to partitions #0, OK
mmc0 is current device
@SD max clock = 10000000@
SD/MMC found on device 0
3651816 bytes read in 785 ms (4.4 MiB/s)
112109 bytes read in 86 ms (1.2 MiB/s)
Booting from mmc0 ...
Kernel image @ 0x82000000 [ 0x000000 - 0x37b8e8 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ffe1000, end 8ffff5ec ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpuset
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.4.45-g0422030-dirty (hsuyz@hsuyz-VirtualBox) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #55 SMP PREEMPT Fri Jul 6 16:05:16 CST 2018
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] Machine model: TI DRA742
[ 0.000000] cma: Reserved 64 MiB at 0x00000000fac00000
[ 0.000000] Forcing write-allocate cache policy for SMP
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] DRA752 ES2.0
[ 0.000000] PERCPU: Embedded 11 pages/cpu @eed9f000 s14848 r8192 d22016 u45056
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 517952
[ 0.000000] Kernel command line: console=ttyO3,115200n8 elevator=noop root=/dev/mmcblk0p2 rw rootwait earlyprintk fixrtc omapdrm.num_crtc=2 consoleblank=0 cma=64M rootfstype=ext4 snd.slots_reserved=1,1
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 1983276K/2078720K available (6663K kernel code, 364K rwdata, 2500K rodata, 336K init, 302K bss, 29908K reserved, 65536K cma-reserved, 1226752K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc08fb09c (9165 kB)
[ 0.000000] .init : 0xc08fc000 - 0xc0950000 ( 336 kB)
[ 0.000000] .data : 0xc0950000 - 0xc09ab390 ( 365 kB)
[ 0.000000] .bss : 0xc09ad000 - 0xc09f8a78 ( 303 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] ti_dt_clocks_register: failed to lookup clock node gmac_gmii_ref_clk_div
[ 0.000000] OMAP clockevent source: timer1 at 31475 Hz
[ 0.000000] Architected cp15 timer(s) running at 5.90MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x15c70fb29, max_idle_ns: 440795202138 ns
[ 0.000004] sched_clock: 56 bits at 5MHz, resolution 169ns, wraps every 4398046511093ns
[ 0.000016] Switching to timer-based delay loop, resolution 169ns
[ 0.000331] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000339] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000793] Console: colour dummy device 80x30
[ 0.000810] WARNING: Your 'console=ttyO3' has been replaced by 'ttyS3'
[ 0.000817] This ensures that you still see kernel messages. Please
[ 0.000822] update your kernel commandline.
[ 0.000835] Calibrating delay loop (skipped), value calculated using timer frequency.. 11.80 BogoMIPS (lpj=59016)
[ 0.000847] pid_max: default: 32768 minimum: 301
[ 0.000941] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000952] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001531] Initializing cgroup subsys io
[ 0.001548] Initializing cgroup subsys memory
[ 0.001573] Initializing cgroup subsys devices
[ 0.001585] Initializing cgroup subsys freezer
[ 0.001597] Initializing cgroup subsys perf_event
[ 0.001608] Initializing cgroup subsys pids
[ 0.001634] CPU: Testing write buffer coherency: ok
[ 0.001845] /cpus/cpu@0 missing clock-frequency property
[ 0.001862] /cpus/cpu@1 missing clock-frequency property
[ 0.001872] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.001909] Setting up static identity map for 0x800082c0 - 0x80008320
[ 0.080107] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.080169] Brought up 2 CPUs
[ 0.080183] SMP: Total of 2 processors activated (23.60 BogoMIPS).
[ 0.080189] CPU: All CPU(s) started in HYP mode.
[ 0.080195] CPU: Virtualization extensions available.
[ 0.080579] devtmpfs: initialized
[ 0.110989] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.111991] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.309786] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.311303] pinctrl core: initialized pinctrl subsystem
[ 0.312153] NET: Registered protocol family 16
[ 0.313148] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.340224] cpuidle: using governor ladder
[ 0.370249] cpuidle: using governor menu
[ 0.378547] OMAP GPIO hardware version 0.1
[ 0.382666] GPIO line 161 (radio_rst) hogged as output/low
[ 0.385006] irq: no irq domain found for /ocp/l4@4a000000/scm@2000/pinmux@1400 !
[ 0.401836] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 0.401849] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 0.412006] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.412016] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.412815] OMAP DMA hardware revision 0.0
[ 0.451884] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
[ 0.453059] edma 43300000.edma: memcpy is disabled
[ 0.457801] edma 43300000.edma: TI EDMA DMA engine driver
[ 0.464792] palmas 0-0058: IRQ missing: skipping irq request
[ 0.481476] palmas 0-0058: Muxing GPIO a, PWM 0, LED 0
[ 0.481597] @@@@1
[ 0.481815] @@@@3
[ 0.481827] @@@@4
[ 0.481836] @@@@5
[ 0.482191] @@@@6
[ 0.482354] @@@@7
[ 0.491128] @@@@8
[ 0.553168] @@@@9(0)
[ 0.553185] @@@@2
[ 0.553332] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[ 0.553760] omap_i2c 48072000.i2c: bus 1 rev0.12 at 400 kHz
[ 0.554124] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz
[ 0.554483] omap_i2c 4807a000.i2c: bus 3 rev0.12 at 400 kHz
[ 0.554843] omap_i2c 4807c000.i2c: bus 4 rev0.12 at 400 kHz
[ 0.555038] media: Linux media interface: v0.10
[ 0.555088] Linux video capture interface: v2.00
[ 0.555126] pps_core: LinuxPPS API ver. 1 registered
[ 0.555133] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.555155] PTP clock support registered
[ 0.555201] EDAC MC: Ver: 3.0.0
[ 0.556001] Advanced Linux Sound Architecture Driver Initialized.
[ 0.556902] clocksource: Switched to clocksource arch_sys_counter
[ 0.567620] NET: Registered protocol family 2
[ 0.568120] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.568183] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.568308] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.568364] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.568394] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.568610] NET: Registered protocol family 1
[ 0.568852] RPC: Registered named UNIX socket transport module.
[ 0.568861] RPC: Registered udp transport module.
[ 0.568868] RPC: Registered tcp transport module.
[ 0.568874] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.569938] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[ 0.572609] futex hash table entries: 512 (order: 3, 32768 bytes)
[ 0.580361] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.581030] NFS: Registering the id_resolver key type
[ 0.581057] Key type id_resolver registered
[ 0.581065] Key type id_legacy registered
[ 0.581129] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.583108] bounce: pool size: 64 pages
[ 0.583270] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
[ 0.583287] io scheduler noop registered (default)
[ 0.583299] io scheduler deadline registered
[ 0.583334] io scheduler cfq registered
[ 0.588674] pinctrl-single 4a003400.pinmux: 282 pins at pa fc003400 size 1128
[ 0.652247] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.655691] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 299, base_baud = 3000000) is a 8250
[ 0.656578] 4806c000.serial: ttyS1 at MMIO 0x4806c000 (irq = 300, base_baud = 3000000) is a 8250
[ 0.657475] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 301, base_baud = 3000000) is a 8250
[ 0.658307] console [ttyS3] disabled
[ 0.658353] 4806e000.serial: ttyS3 at MMIO 0x4806e000 (irq = 302, base_baud = 3000000) is a 8250
[ 1.459438] console [ttyS3] enabled
[ 1.463793] 48066000.serial: ttyS4 at MMIO 0x48066000 (irq = 303, base_baud = 3000000) is a 8250
[ 1.473446] 48422000.serial: ttyS7 at MMIO 0x48422000 (irq = 304, base_baud = 3000000) is a 8250
[ 1.483097] 48424000.serial: ttyS8 at MMIO 0x48424000 (irq = 305, base_baud = 3000000) is a 8250
[ 1.492754] 4ae2b000.serial: ttyS9 at MMIO 0x4ae2b000 (irq = 306, base_baud = 3000000) is a 8250
[ 1.502838] [drm] Initialized drm 1.1.0 20060810
[ 1.508943] OMAP DSS rev 6.1
[ 1.512715] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops)
[ 1.528812] loop: module loaded
[ 1.532822] nand: No NAND device found
[ 1.536594] omap2-nand 8000000.nand: scan failed, may be bus-width mismatch
[ 1.549059] m25p80 spi32766.0: s25fl256s1 (32768 Kbytes)
[ 1.554454] 7 ofpart partitions found on MTD device spi32766.0
[ 1.560334] Creating 7 MTD partitions on "spi32766.0":
[ 1.565497] 0x000000000000-0x000000040000 : "QSPI.MLO"
[ 1.571581] 0x000000040000-0x000000140000 : "QSPI.u-boot"
[ 1.577890] 0x000000140000-0x0000001c0000 : "QSPI.DRA7-evm.dtb"
[ 1.584711] 0x0000001c0000-0x0000001d0000 : "QSPI.u-boot-env"
[ 1.591368] 0x0000001d0000-0x0000001e0000 : "QSPI.u-boot-env.backup1"
[ 1.598723] 0x0000001e0000-0x0000009e0000 : "QSPI.uImage"
[ 1.604975] 0x0000009e0000-0x000002000000 : "QSPI.IPU-exe"
[ 1.612361] libphy: Fixed MDIO Bus: probed
[ 1.617077] CAN device driver interface
[ 1.621301] pinctrl-single 4a003400.pinmux: pin 4a003818.0 already requested by 4a003400.pinmux; cannot claim for 4ae3c000.can
[ 1.632761] pinctrl-single 4a003400.pinmux: pin-262 (4ae3c000.can) status -22
[ 1.639946] pinctrl-single 4a003400.pinmux: could not request pin 262 (4a003818.0) from group dcan1_pins_sleep on device pinctrl-single
[ 1.652278] c_can_platform 4ae3c000.can: Error applying setting, reverse things back
[ 1.660721] c_can_platform 4ae3c000.can: c_can_platform device registered (regs=fce3c000, irq=357)
[ 1.716934] davinci_mdio 48485000.mdio: davinci mdio revision 1.6
[ 1.723059] libphy: 48485000.mdio: probed
[ 1.727109] mdio_bus 48485000.mdio: /ocp/ethernet@48484000/mdio@48485000/micrel_phy_config has invalid PHY address
[ 1.737519] mdio_bus 48485000.mdio: /ocp/ethernet@48484000/mdio@48485000/rmii-ref has invalid PHY address
[ 1.747145] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 0
[ 1.756655] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 1
[ 1.764519] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 2
[ 1.772319] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 3
[ 1.780119] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 4
[ 1.789268] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 5
[ 1.797277] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 6
[ 1.805078] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 7
[ 1.812879] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 8
[ 1.820679] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 9
[ 1.828479] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 10
[ 1.836277] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 11
[ 1.844078] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 12
[ 1.851878] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 13
[ 1.859678] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 14
[ 1.867478] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 15
[ 1.875277] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 16
[ 1.883075] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 17
[ 1.890878] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 18
[ 1.898678] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 19
[ 1.906477] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 20
[ 1.914277] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 21
[ 1.922078] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 22
[ 1.929878] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 23
[ 1.937677] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 24
[ 1.945477] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 25
[ 1.953278] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 26
[ 1.961077] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 27
[ 1.968878] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 28
[ 1.976677] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 29
[ 1.984478] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 30
[ 1.992278] mdio_bus 48485000.mdio: scan phy micrel_phy_config at address 31
[ 2.000080] mdio_bus 48485000.mdio: scan phy rmii-ref at address 1
[ 2.006837] mdio_bus 48485000.mdio: scan phy rmii-ref at address 2
[ 2.013597] mdio_bus 48485000.mdio: scan phy rmii-ref at address 3
[ 2.020358] mdio_bus 48485000.mdio: scan phy rmii-ref at address 5
[ 2.027115] mdio_bus 48485000.mdio: scan phy rmii-ref at address 6
[ 2.033877] mdio_bus 48485000.mdio: scan phy rmii-ref at address 7
[ 2.041158] mdio_bus 48485000.mdio: scan phy rmii-ref at address 8
[ 2.047918] mdio_bus 48485000.mdio: scan phy rmii-ref at address 9
[ 2.054677] mdio_bus 48485000.mdio: scan phy rmii-ref at address 10
[ 2.061957] mdio_bus 48485000.mdio: scan phy rmii-ref at address 11
[ 2.069238] mdio_bus 48485000.mdio: scan phy rmii-ref at address 12
[ 2.076516] mdio_bus 48485000.mdio: scan phy rmii-ref at address 13
[ 2.083798] mdio_bus 48485000.mdio: scan phy rmii-ref at address 14
[ 2.091077] mdio_bus 48485000.mdio: scan phy rmii-ref at address 15
[ 2.098357] mdio_bus 48485000.mdio: scan phy rmii-ref at address 16
[ 2.105637] mdio_bus 48485000.mdio: scan phy rmii-ref at address 17
[ 2.112918] mdio_bus 48485000.mdio: scan phy rmii-ref at address 18
[ 2.120198] mdio_bus 48485000.mdio: scan phy rmii-ref at address 19
[ 2.127478] mdio_bus 48485000.mdio: scan phy rmii-ref at address 20
[ 2.134757] mdio_bus 48485000.mdio: scan phy rmii-ref at address 21
[ 2.142037] mdio_bus 48485000.mdio: scan phy rmii-ref at address 22
[ 2.149318] mdio_bus 48485000.mdio: scan phy rmii-ref at address 23
[ 2.156597] mdio_bus 48485000.mdio: scan phy rmii-ref at address 24
[ 2.163878] mdio_bus 48485000.mdio: scan phy rmii-ref at address 25
[ 2.171158] mdio_bus 48485000.mdio: scan phy rmii-ref at address 26
[ 2.178437] mdio_bus 48485000.mdio: scan phy rmii-ref at address 27
[ 2.185717] mdio_bus 48485000.mdio: scan phy rmii-ref at address 28
[ 2.192997] mdio_bus 48485000.mdio: scan phy rmii-ref at address 29
[ 2.200278] mdio_bus 48485000.mdio: scan phy rmii-ref at address 30
[ 2.207558] mdio_bus 48485000.mdio: scan phy rmii-ref at address 31
[ 2.214839] davinci_mdio 48485000.mdio: phy[0]: device 48485000.mdio:00, driver Micrel KSZ8081 or KSZ8091
[ 2.224462] davinci_mdio 48485000.mdio: phy[4]: device 48485000.mdio:04, driver Micrel KSZ8081 or KSZ8091
[ 2.234482] cpsw 48484000.ethernet: No slave[0] phy_id, phy-handle, or fixed-link property
[ 2.242944] cpsw 48484000.ethernet: Detected MACID = f0:45:da:8a:80:e6
[ 2.249606] cpsw 48484000.ethernet: cpts: overflow check period 800
[ 2.257745] mousedev: PS/2 mouse device common for all mice
[ 2.273954] i2c /dev entries driver
[ 2.278247] @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@
[ 2.283757] 11111111111111111111111@@@@@@@@@@@@@@@@@@@@@@@@
[ 2.289370] 22222222222222222222222@@@@@@@@@@@@@@@@@@@@@@@@
[ 2.294966] 3333333333333333333333333333@@@@@@@@@@@@@@@@@@@@@@@@
[ 2.301013] 44444444444444444444444444444@@@@@@@@@@@@@@@@@@@@@@@@
[ 2.307433] 55555555555555555555555555555@@@@@@@@@@@@@@@@@@@@@@@@
[ 2.313552] 8888888888888888888888888888888@@@@@@@@@@@@@
[ 2.354257] adv7611 0-004c: adv7611 found @ 0x98 (OMAP I2C adapter)
[ 2.361469] vpe 489d0000.vpe: loading firmware vpdma-1b8.bin
[ 2.368578] vip 48990000.vip: loading firmware vpdma-1b8.bin
[ 2.378800] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 2.387090] vpe 489d0000.vpe: Device registered as /dev/video0
[ 2.396925] vip 48990000.vip: VPDMA firmware loaded
[ 2.401944] vip2-s0: Port A: Using subdev adv7611 0-004c for capture
[ 2.408731] vip2-s0: device registered as video1
[ 2.427606] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
[ 2.433989] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
[ 2.440551] evm_3v3_sw: supplied by sysen1
[ 2.477283] omap_hsmmc 480ad000.mmc: no pinctrl state for sdr50 mode
[ 2.483669] omap_hsmmc 480ad000.mmc: no pinctrl state for sdr25 mode
[ 2.490066] omap_hsmmc 480ad000.mmc: no pinctrl state for sdr12 mode
[ 2.496449] omap_hsmmc 480ad000.mmc: no pinctrl state for hs mode
[ 2.537681] ledtrig-cpu: registered to indicate activity on CPUs
[ 2.547876] hwspinlock_user gatemp: requested 10 hwspinlocks
[ 2.554260]
[ 2.554260] [spidrv_init]
[ 2.558393] spidrv_init called
[ 2.561469]
[ 2.561469] [mcaspdrv_init]
[ 2.565754] mcaspdrv_init called
[ 2.570100] davinci-mcasp 48460000.mcasp: DAI is shared
[ 2.575371]
[ 2.575371] [McASP1][mcasp->base][FA460000]
[ 2.581105]
[ 2.581105] [McASP]not return
[ 2.581105]
[ 2.587643] davinci-mcasp 48464000.mcasp: DAI is shared
[ 2.592907]
[ 2.592907] [McASP2][mcasp->base][FA464000]
[ 2.592907]
[ 2.600090]
[ 2.600090] [McASP]not return
[ 2.600090]
[ 2.606254] davinci-mcasp 48468000.mcasp: DAI is shared
[ 2.611538]
[ 2.611538] [McASP3][mcasp->base][FA468000]
[ 2.611538]
[ 2.618716]
[ 2.618716] [McASP]not return
[ 2.618716]
[ 2.626218] NET: Registered protocol family 10
[ 2.641469] sit: IPv6 over IPv4 tunneling driver
[ 2.646645] NET: Registered protocol family 17
[ 2.651160] can: controller area network core (rev 20120528 abi 9)
[ 2.657433] NET: Registered protocol family 29
[ 2.661910] can: raw protocol (rev 20120528)
[ 2.666399] Key type dns_resolver registered
[ 2.670850] omap_voltage_late_init: Voltage driver support not added
[ 2.677878] Power Management for TI OMAP4+ devices.
[ 2.683023] Registering SWP/SWPB emulation handler
[ 2.690578] dmm 4e000000.dmm: initialized all PAT entries
[ 2.710492] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 2.717166] [drm] No driver support for vblank timestamp query.
[ 2.734375] [drm] Enabling DMM ywrap scrolling
[ 2.745940] mmc0: host does not support reading read-only switch, assuming write-enable
[ 2.747925] @SD max clock = 10000000@
[ 2.748010] mmc0: new high speed SDHC card at address 59b4
[ 2.758505] mmcblk0: mmc0:59b4 SD 14.7 GiB
[ 2.760268] mmcblk0: p1 p2
[ 2.787297] Console: switching to colour frame buffer device 160x50
[ 2.802966] mmc1: MAN_BKOPS_EN bit is not set
[ 2.812173] @eMMC max clock = 25000000@
[ 2.819468] mmc1: new MMC card at address 0001
[ 2.830004] mmcblk1: mmc1:0001 MMC04G 3.57 GiB
[ 2.840269] mmcblk1boot0: mmc1:0001 MMC04G partition 1 8.00 MiB
[ 2.848982] omapdrm omapdrm.0: fb0: omapdrm frame buffer device
[ 2.850543] mmcblk1boot1: mmc1:0001 MMC04G partition 2 8.00 MiB
[ 2.860932] mmcblk1: p1 p2
[ 2.890270] [drm] Initialized omapdrm 1.0.0 20110917 on minor 0
[ 2.907245] hctosys: unable to open rtc device (rtc0)
[ 2.924411] aic_dvdd: disabling
[ 2.927605] vmmcwl_fixed: disabling
[ 2.931336] ldousb: disabling
[ 2.934815] ALSA device list:
[ 2.937852] No soundcards found.
[ 4.083086] EXT4-fs (mmcblk0p2): recovery complete
[ 4.091778] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 4.099962] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 4.138827] devtmpfs: mounted
[ 4.142020] Freeing unused kernel memory: 336K (c08fc000 - c0950000)
[ 4.148425] This architecture does not have kernel memory protection.
[ 4.956804] systemd[1]: System time before build time, advancing clock.
[ 5.066603] random: systemd: uninitialized urandom read (16 bytes read, 23 bits of entropy available)
[ 5.080446] random: systemd: uninitialized urandom read (16 bytes read, 23 bits of entropy available)
[ 5.092140] systemd[1]: systemd 229 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT +GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN)
[ 5.110663] systemd[1]: Detected architecture arm.
Welcome to Arago 2016.12!
[ 5.138510] systemd[1]: Set hostname to <dra7xx-evm>.
[ 5.313308] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 24 bits of entropy available)
[ 5.329424] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 24 bits of entropy available)
[ 5.339892] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 25 bits of entropy available)
[ 5.370354] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 25 bits of entropy available)
[ 5.386293] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 25 bits of entropy available)
[ 5.687845] random: systemd: uninitialized urandom read (16 bytes read, 29 bits of entropy available)
[ 5.697383] random: systemd: uninitialized urandom read (16 bytes read, 29 bits of entropy available)
[ 5.707353] random: systemd: uninitialized urandom read (16 bytes read, 29 bits of entropy available)
[ 5.873480] systemd[1]: Configuration file /etc/systemd/system/multi-user.target.wants/MAN2020.service is marked executable. Please remove executable permission bits. Proceeding anyway.
[ 5.890546] systemd[1]: Configuration file /etc/systemd/system/multi-user.target.wants/MAN2020.service is marked world-writable. Please remove world writability permission bits. Proceeding anyway.
[ 5.912440] systemd[1]: gplv3-notice.service: Service lacks both ExecStart= and ExecStop= setting. Refusing.
[ 6.044402] systemd[1]: gplv3-notice.service: Cannot add dependency job, ignoring: Unit gplv3-notice.service is not loaded properly: Invalid argument.
[ 6.058516] systemd[1]: sysinit.target: Found ordering cycle on sysinit.target/start
[ 6.066306] systemd[1]: sysinit.target: Found dependency on alignment.service/start
[ 6.074089] systemd[1]: sysinit.target: Found dependency on basic.target/start
[ 6.081391] systemd[1]: sysinit.target: Found dependency on sockets.target/start
[ 6.088839] systemd[1]: sysinit.target: Found dependency on avahi-daemon.socket/start
[ 6.096707] systemd[1]: sysinit.target: Found dependency on sysinit.target/start
[ 6.104160] systemd[1]: sysinit.target: Breaking ordering cycle by deleting job alignment.service/start
[ 6.113615] systemd[1]: alignment.service: Job alignment.service/start deleted to break ordering cycle starting with sysinit.target/start
[ SKIP ] Ordering cycle found, skipping alignment.service
[ 6.151102] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 6.177120] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 6.197304] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 6.290942] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 6.317229] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[ OK ] Listening on /dev/initctl Compatibility Named Pipe.
[ 6.347193] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 6.377167] systemd[1]: Listening on Syslog Socket.
[ OK ] Listening on Syslog Socket.
[ 6.397181] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 6.417791] systemd[1]: Created slice System Slice.
[ OK ] Created slice System Slice.
[ 6.487173] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 6.519458] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 6.549608] systemd[1]: Starting Setup Virtual Console...
Starting Setup Virtual Console...
[ 6.577412] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ 6.579671] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ 6.657422] systemd[1]: Starting Create list of required static device nodes for the current kernel...
Starting Create list of required st... nodes for the current kernel...
[ 6.687334] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ 6.717103] systemd[1]: Reached target Paths.
[ OK ] Reached target Paths.
[ 6.737108] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 6.787173] systemd[1]: Mounting Temporary Directory...
Mounting Temporary Directory...
[ 6.824991] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 6.849661] systemd[1]: Mounting Debug File System...
Mounting Debug File System...
[ 6.877106] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 6.907217] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 6.967393] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 6.987943] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 7.024541] systemd[1]: Mounted Debug File System.
[ OK ] Mounted Debug File System.
[ 7.047172] systemd[1]: Mounted POSIX Message Queue File System.
[ OK ] Mounted POSIX Message Queue File System.
[ 7.077124] systemd[1]: Mounted Temporary Directory.
[ OK ] Mounted Temporary Directory.
[ 7.096054] systemd[1]: Started Remount Root and Kernel File Systems.
[ OK ] Started Remount Root and Kernel File Systems.
[ 7.128358] systemd[1]: Started Setup Virtual Console.
[ OK ] Started Setup Virtual Console.
[ 7.158252] systemd[1]: Started Create list of required static device nodes for the current kernel.
[ OK ] Started Create list of required sta...ce nodes for the current kernel.
[ 7.188044] systemd[1]: systemd-modules-load.service: Main process exited, code=exited, status=1/FAILURE
[ 7.198892] systemd[1]: Failed to start Load Kernel Modules.
[FAILED] Failed to start Load Kernel Modules.
See 'systemctl status systemd-modules-load.service' for details.
[ 7.237027] systemd[1]: systemd-modules-load.service: Unit entered failed state.
[ 7.244470] systemd[1]: systemd-modules-load.service: Failed with result 'exit-code'.
[ 7.253327] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
Starting Apply Kernel Variables...
Starting Create Static Device Nodes in /dev...
Starting udev Coldplug all Devices...
Starting Flush Journal to Persistent Storage...
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create Static Device Nodes in /dev.
[ 8.086592] systemd-journald[130]: Received request to flush runtime journal from PID 1
Starting udev Kernel Device Manager...
[ OK ] Reached target Local File Systems (Pre).
Mounting /var/volatile...
Mounting /media/ram...
[ OK ] Mounted /var/volatile.
[ OK ] Mounted /media/ram.
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started udev Coldplug all Devices.
[ OK ] Reached target Local File Systems.
[ 8.992380] omap_rng 48090000.rng: OMAP Random Number Generator ver. 20
Starting Create Volatile Files and Directories...
Starting Load/Save Random Seed...
[ 9.106726] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
[ 9.154894] alg: skcipher: setkey failed on test 5 for ecb-des-omap: flags=100
[ OK ] Found device /dev/ttyS3.[ 9.209480] alg: skcipher-ddst: setkey failed on test 5 for ecb-des-omap: flags=100
[ 9.221155] alg: skcipher-ddst: setkey failed on test 5 for ecb-des-omap: flags=100
[ OK ] Started Load/Save Random Seed.
[ OK ] Started Create Volatile Files and Directories.
[ 9.315046] omap_rtc 48838000.rtc: rtc core: registered 48838000.rtc as rtc0
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ 9.718532] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 9.727538] omap-sham 4b101000.sham: hw accel on OMAP rev 4.3
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Time Synchronized.
[ 9.805902] SCSI subsystem initialized
Starting Synchronize System and HW clocks...
[ OK ] Started Synchronize System and HW clocks.
[ OK ] Reached target System Initialization.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timers.
[ OK ] Listening on dropbear.socket.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
[ OK ] Started System Logging Service.
[ OK ] Started Start helloworld.
[ OK ] Started D-Bus System Message Bus.
[ 10.493543] omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3
[ 10.570047] omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3
[ 10.579706] ahci 4a140000.sata: SSS flag set, parallel bus scan disabled
[ 10.594465] ahci 4a140000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
[INFO] VERSION: B0.0.0.0004[ 10.620591] ahci 4a140000.sata: flags: 64bit ncq sntf stag pm led clo only pmp pio slum part ccc apst
[SYS ] paring option: token=3, option=(null)
[INFO] R3 init, iface=/dev/ttyS7
[INFO] R2 init
[INFO] watchdog init
[INFO] CLIENT ready
[ 10.667248] scsi host0: ahci
[ 10.670562] ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a1410ff] port 0x100 irq 339
[ 10.718119] [drm] Initialized pvr 1.14.3699939 20110701 on minor 1
[ 11.046969] ata1: SATA link down (SStatus 0 SControl 300)
[ 11.204663] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
Starting Network Service...
[ OK ] Started strongSwan IPsec IKEv1/IKEv2 daemon using ipsec.conf.
Starting Telephony service...
Starting Permit User Sessions...
Starting hw-id.service...
Starting Login Service...
Starting Avahi mDNS/DNS-SD Stack...
Starting uim-sysfs.service...
[ OK ] Started Kernel Logging Service.
[ OK ] Started Permit User Sessions.
[ OK ] Started hw-id.service.
[ 12.065940] net eth0: initializing cpsw version 1.15 (0)
[ 12.085624] net eth0: initialized cpsw ale version 1.4
[ 12.091516] FAT-fs (mmcblk1p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 12.109759] net eth0: ALE Table size 1024
[ 12.115792] libphy: PHY not found
[ 12.137325] EXT4-fs (mmcblk1p2): recovery complete
[ 12.146336] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
[ OK ] Started Network Service.
[ 12.195952] net eth0: phy "" not found on slave 0, err -19
[ 12.305966] net eth0: phy found : id is : 0x221560
[ 12.340777] cpsw-phy-sel 4a002554.cpsw-phy-sel: RMII External clock is not supported
[ 12.446567] Bluetooth: Core ver 2.21
[ 12.459668] NET: Registered protocol family 31
[ 12.498372] Bluetooth: HCI device and connection manager initialized
[ 12.504784] Bluetooth: HCI socket layer initialized
[ 12.556991] Bluetooth: L2CAP socket layer initialized
[ 12.562120] Bluetooth: SCO socket layer initialized
[ 12.569817] NET: Registered protocol family 15
[ 12.605481] @@USB2PHY_TERMINATION_CONTROL=0x220004
[ 12.833130] Initializing XFRM netlink socket
[ 13.150525] @@USB2PHY_TERMINATION_CONTROL=0x220004
[ 13.782874] usbcore: registered new interface driver usbfs
[ 13.804934] usbcore: registered new interface driver hub
[ 13.827968] usbcore: registered new device driver usb
[ 13.882276] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 13.900972] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[ 13.930702] xhci-hcd xhci-hcd.0.auto: hcc params 0x0220f04c hci version 0x100 quirks 0x00210010
[ 13.957021] xhci-hcd xhci-hcd.0.auto: irq 434, io mem 0x48890000
[ 13.977631] hub 1-0:1.0: USB hub found
[ 13.987192] hub 1-0:1.0: 1 port detected
[ 13.997396] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 14.002923] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[ 14.027049] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 14.048642] hub 2-0:1.0: USB hub found
[ 14.052450] hub 2-0:1.0: 1 port detected
[ 14.057091] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 14.062627] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 3
[ 14.087335] xhci-hcd xhci-hcd.1.auto: hcc params 0x0220f04c hci version 0x100 quirks 0x00210010
[ 14.096131] xhci-hcd xhci-hcd.1.auto: irq 435, io mem 0x488d0000
[ 14.128273] hub 3-0:1.0: USB hub found
[ 14.132440] hub 3-0:1.0: 1 port detected
[ 14.147512] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 14.153042] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 4
[ OK ] Started Avahi mDNS/DNS-SD Stack.[ 14.204177] usb usb4: We don't know the algorithms for LPM for this host, disabling LPM.
[ OK ] Started Telephony service.
[ OK ] Started Login Service.
[ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
[ OK ] Reached target Network.
Starting Network Name Resolution...
Starting Lightning Fast Webserver With Light System Requirements...[ 14.269159] hub 4-0:1.0: USB hub found
[ OK ] Started Serial Getty on ttyS3.
[ OK ] Reached target Login Prompts.[ 14.276887] hub 4-0:1.0: 1 port detected
[[032m OK ]Started uim-sysfs.service.
[[032m OK ]Started Lightning Fast Webserver With Light Sstem Requirements.
[ OK ] Started Network Name Resolution.
Starting rc.pvr.service...
[ 14.918173] PVR_K: UM DDK-(3699939) and KM DDK-(3699939) match. [ OK ]
[ OK ] Started rc.pvr.service.
Starting telnetd.service...
Starting tiipclad-daemon.service...
[ OK ] Started telnetd.service.
[ OK ] Started tiipclad-daemon.service.
Starting thttpd.service...
[ OK ] Started thttpd.service.
Starting rng-tools.service...
[ OK ] Started rng-tools.service.
[ 15.386683] random: nonblocking pool is initialized
Starting gdbserverproxy.service...
[ OK ] Started gdbserverproxy.service.
Starting matrix-gui-2.0.service...
[ OK ] Started matrix-gui-2.0.service.
Starting thermal-zone-init.service...
[ OK ] Started thermal-zone-init.service.
[ OK ] Reached target Multi-User System.
Starting Update UTMP about System Runlevel Changes...
[ OK ] Started Update UTMP about System Runlevel Changes.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org dra7xx-evm ttyS3
Arago 2016.12 dra7xx-evm ttyS3
dra7xx-evm login: root (automatic login)
root@dra7xx-evm:~#
root@dra7xx-evm:~#
root@dra7xx-evm:~# ls /dev/video*
/dev/video0 /dev/video1 /dev/video10 /dev/video11
root@dra7xx-evm:~#
root@dra7xx-evm:~#
root@dra7xx-evm:~#
root@dra7xx-evm:~#
root@dra7xx-evm:~# v4l2-ctl --list-device
wbcap (platform:omapwb-cap):
/dev/video11
omapwb-m2m (platform:omapwb-m2m):
/dev/video10
vpe (platform:vpe):
/dev/video0
root@dra7xx-evm:~#
Here is our dts file =>
/*
* Copyright (C) 2016 Texas Instruments Incorporated - http://www.ti.com/
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*/
//#include "dra7-evm.dts"
#include "dra7-evm-lcd-lg.dts"
/ {
memory {
device_type = "memory";
reg = <0x0 0x80000000 0x0 0x80000000>; /* 2 GB */
//reg = <0x0 0x80000000 0x0 0xC0000000>; /* 3 GB */
};
leds {
status = "disabled";
};
gpio_keys {
status = "disabled";
};
jamr3_sound{
status = "disabled";
};
primary_sound{
status = "disabled";
};
};
&evm_3v3_sd {
gpio = <>;
};
&snd0 {
status = "disabled";
};
&hdmi0 {
status = "disabled";
};
&tpd12s015 {
status = "disabled";
};
&pcf_lcd {
status = "disabled";
};
&pcf_gpio_21 {
status = "disabled";
};
&lcd_fpd {
status = "disabled";
};
&extcon_usb1 {
//fake gpio
id-gpios = <&gpio3 24 GPIO_ACTIVE_HIGH>;
};
&extcon_usb2 {
//fake gpio
id-gpios = <&gpio3 25 GPIO_ACTIVE_HIGH>;
};
&usb1 {
dr_mode = "host";
};
&tlv320aic3106 {
status = "disabled";
};
&pcf_hdmi {
status = "disabled";
};
&i2c_p3_exp {
ov10633@37 {
status = "disabled";
};
};
&tvp_5158 {
status = "disabled";
};
&disp_ser {
status = "disabled";
};
&pcie1_rc {
status = "disabled";
};
&elm {
status = "okay";
};
#if 1
&gpmc {
status = "okay";
ranges = <0 0 0x08000000 0x01000000>; /* minimum GPMC partition = 16MB */
nand@0,0 {
compatible = "ti,omap2-nand";
reg = <0 0 4>; /* device IO registers */
interrupt-parent = <&gpmc>;
interrupts = <0 IRQ_TYPE_NONE>, /* fifoevent */
<1 IRQ_TYPE_NONE>; /* termcount */
rb-gpios = <&gpmc 0 GPIO_ACTIVE_HIGH>; /* gpmc_wait0 pin */
ti,nand-ecc-opt = "bch8";
ti,elm-id = <&elm>;
nand-bus-width = <16>;
gpmc,device-width = <2>;
gpmc,sync-clk-ps = <0>;
gpmc,cs-on-ns = <0>;
gpmc,cs-rd-off-ns = <80>;
gpmc,cs-wr-off-ns = <80>;
gpmc,adv-on-ns = <0>;
gpmc,adv-rd-off-ns = <60>;
gpmc,adv-wr-off-ns = <60>;
gpmc,we-on-ns = <10>;
gpmc,we-off-ns = <50>;
gpmc,oe-on-ns = <4>;
gpmc,oe-off-ns = <40>;
gpmc,access-ns = <40>;
gpmc,wr-access-ns = <80>;
gpmc,rd-cycle-ns = <80>;
gpmc,wr-cycle-ns = <80>;
gpmc,bus-turnaround-ns = <0>;
gpmc,cycle2cycle-delay-ns = <0>;
gpmc,clk-activation-ns = <0>;
gpmc,wr-data-mux-bus-ns = <0>;
/* MTD partition table */
/* All SPL-* partitions are sized to minimal length
* which can be independently programmable. For
* NAND flash this is equal to size of erase-block */
#address-cells = <1>;
#size-cells = <1>;
partition@0 {
label = "NAND.device.0";
reg = <0x00000000 0x10000000>; /*256 MB*/
};
/*
partition@0 {
label = "NAND.SPL";
reg = <0x00000000 0x000020000>;
};
partition@1 {
label = "NAND.SPL.backup1";
reg = <0x00020000 0x00020000>;
};
partition@2 {
label = "NAND.SPL.backup2";
reg = <0x00040000 0x00020000>;
};
partition@3 {
label = "NAND.SPL.backup3";
reg = <0x00060000 0x00020000>;
};
partition@4 {
label = "NAND.u-boot-spl-os";
reg = <0x00080000 0x00040000>;
};
partition@5 {
label = "NAND.u-boot";
reg = <0x000c0000 0x00100000>;
};
partition@6 {
label = "NAND.u-boot-env";
reg = <0x001c0000 0x00020000>;
};
partition@7 {
label = "NAND.u-boot-env.backup1";
reg = <0x001e0000 0x00020000>;
};
partition@8 {
label = "NAND.kernel";
reg = <0x00200000 0x00800000>;
};
partition@9 {
label = "NAND.file-system";
reg = <0x00a00000 0x0f600000>;
};
*/
};
};
#endif
&qspi {
status = "okay";
spi-max-frequency = <76800000>;
m25p80@0 {
compatible = "s25fl256s1";
spi-max-frequency = <76800000>;
reg = <0>;
spi-tx-bus-width = <1>;
spi-rx-bus-width = <4>;
#address-cells = <1>;
#size-cells = <1>;
/* MTD partition table.
* The ROM checks the first four physical blocks
* for a valid file to boot and the flash here is
* 64KiB block size.
*/
partition@0 {
label = "QSPI.MLO";
reg = <0x00000000 0x000040000>;
};
partition@1 {
label = "QSPI.u-boot";
reg = <0x00040000 0x00100000>;
};
partition@2 {
label = "QSPI.DRA7-evm.dtb";
reg = <0x00140000 0x00080000>;
};
partition@3 {
label = "QSPI.u-boot-env";
reg = <0x001c0000 0x00010000>;
};
partition@4 {
label = "QSPI.u-boot-env.backup1";
reg = <0x001d0000 0x0010000>;
};
partition@5 {
label = "QSPI.uImage";
reg = <0x001e0000 0x0800000>;
};
partition@6 {
label = "QSPI.IPU-exe";
reg = <0x009e0000 0x01620000>;
};
};
};
&mailbox5 {
status = "disabled";
};
&mailbox6 {
status = "disabled";
};
&mmu0_dsp1 {
status = "disabled";
};
&mmu1_dsp1 {
status = "disabled";
};
&mmu0_dsp2 {
status = "disabled";
};
&mmu1_dsp2 {
status = "disabled";
};
&mmu_ipu1 {
status = "disabled";
};
&mmu_ipu2 {
status = "disabled";
};
&ipu2 {
status = "disabled";
};
&ipu1 {
status = "disabled";
};
&dsp1 {
status = "disabled";
};
&dsp2 {
status = "disabled";
};
&dss {
status = "okay";
ports {
port {
reg = <1>;
};
};
};
&hdmi {
status = "disabled";
};
&vip1 {
status = "disabled";
};
&video_in {
status = "disabled";
};
&reserved_mem {
status = "disabled";
};
&pcf_jamr3_21 {
status = "disabled";
};
&tlv320aic3106a {
status = "disabled";
};
&tlv320aic3106b {
status = "disabled";
};
&tlv320aic3106c {
status = "disabled";
};
&mcasp7 {
status = "disabled";
};
&mcasp8 {
status = "disabled";
};
&mcasp2 {
status = "okay";
};
&mcasp3 {
status = "okay";
};
&mcasp6 {
status = "disabled";
};
&ipu2_cma_pool {
status = "disabled";
};
&dsp1_cma_pool {
status = "disabled";
};
&ipu1_cma_pool {
status = "disabled";
};
&dsp2_cma_pool {
status = "disabled";
};
&cmem_radio {
status = "disabled";
};
&dsp1_sr0 {
status = "disabled";
};
&uart4 {
status = "okay";
};
&uart8 {
status = "okay";
};
&uart5 {
status = "okay";
};
&uart9 {
status = "okay";
};
&uart10 {
status = "okay";
};
&mmc4 {
status = "disabled";
};
/*********************************below for video port enable test***************************************/
/* VIN2A pins mapped to VIP1 */
&vip2 {
status = "okay";
//pinctrl-names = "default";
/*
Pinmux conflict between vin1a:16-23 & vin2a:0-8
Either use full 24bit of vin1a or use 16bit vin1a and 8bitvin2a
TO enable cam2, uncomment this
pinctrl-0 = <&vin1a_pins &vin2a>;
*/
//pinctrl-0 = <&vin3a_pins >;
};
&vin3a {
status = "okay";
endpoint@0 {
slave-mode;
remote-endpoint = <&hdmi_receiver>;
};
};
&i2c1 {
status = "okay";
clock-frequency = <400000>;
adv7611: adv7611@4c {
compatible = "adi,adv7611";
reg = <0x4c>;
port {
hdmi_receiver: endpoint {
remote-endpoint = <&vin3a>;
hsync-active = <1>;
vsync-active = <1>;
pclk-sample = <1>;
};
};
};
};
/**********************************up for video port enable test*****************************************/
&i2c1 {
status = "okay";
clock-frequency = <400000>;
};
&i2c2 {
status = "okay";
clock-frequency = <400000>;
};
&i2c3 {
status = "okay";
clock-frequency = <400000>;
};
&i2c4 {
status = "okay";
clock-frequency = <400000>;
};
&i2c5 {
status = "okay";
clock-frequency = <400000>;
};
&mcspi1 {
status = "okay";
spidev@0 {
spi-max-frequency = <24000000>;
reg = <0>;
compatible = "rohm,dh2228fv";
/*compatible = "linux,spidev";*/
};
};
&mcspi2 {
status = "okay";
spidev@1 {
spi-max-frequency = <24000000>;
reg = <0>;
compatible = "rohm,dh2228fv";
};
};
&mcspi3 {
status = "okay";
spidev@2 {
spi-max-frequency = <24000000>;
reg = <0>;
compatible = "rohm,dh2228fv";
};
};
&mcspi4 {
status = "okay";
spidev@3 {
spi-max-frequency = <24000000>;
reg = <0>;
compatible = "rohm,dh2228fv";
};
};
&mcasp1 {
#sound-dai-cells = <0>;
assigned-clocks = <&mcasp1_ahclkx_mux>;
assigned-clock-parents = <&atl_clkin1_ck>;
status = "okay";
op-mode = <0>; // MCASP_IIS_MODE //
tdm-slots = <2>;
// 4 serializer //
serial-dir = < // 0: INACTIVE, 1: TX, 2: RX //
0 0 1 2
>;
tx-num-evt = <32>;
rx-num-evt = <32>;
};
&mcasp2 {
#sound-dai-cells = <0>;
assigned-clocks = <&mcasp2_ahclkx_mux>;
assigned-clock-parents = <&atl_clkin1_ck>;
status = "okay";
op-mode = <0>; // MCASP_IIS_MODE //
tdm-slots = <2>;
// 4 serializer //
serial-dir = < // 0: INACTIVE, 1: TX, 2: RX //
0 0 1 2
>;
tx-num-evt = <32>;
rx-num-evt = <32>;
};
&mcasp3 {
#sound-dai-cells = <0>;
assigned-clocks = <&mcasp3_ahclkx_mux>;
assigned-clock-parents = <&atl_clkin1_ck>;
status = "okay";
op-mode = <0>; // MCASP_IIS_MODE //
tdm-slots = <2>;
// 4 serializer //
serial-dir = < // 0: INACTIVE, 1: TX, 2: RX //
0 0 1 2
>;
tx-num-evt = <32>;
rx-num-evt = <32>;
};
&atl {
assigned-clock-parents = <&sys_clkin1>, <&dpll_abe_m2_ck>;
};
&mac {
status = "okay";
active_slave = <1>;
};
&davinci_mdio {
status = "okay";
micrel_phy_config {
#address-cells = <1>;
#size-cells = <0>;
micrel,led-mode = <1>;
clock-names = "rmii-ref";
clocks = <&rmii_50M_clock>;
};
rmii_50M_clock: rmii-ref{
#clock-cells = <0>;
compatible ="fixed-clock";
clock-frequency = <50000000>;
};
};
&cpsw_emac1 {
phy_id = <&davinci_mdio>, <4>;
phy-mode = "rmii";
status = "okay";
};
&phy_sel {
rmii-clock-ext;
};
&oppdm_mpu {
status = "disabled";
};
&epwmss0 {
status = "okay";
};
#if 0
&ehrpwm0 {
status = "okay";
};
#endif
&ecap0 {
status = "okay";
};
&epwmss1 {
status = "okay";
};
#if 0
&ehrpwm1 {
status = "okay";
};
#endif
&ecap1 {
status = "okay";
};
&epwmss2 {
status = "okay";
};
#if 0
&ehrpwm2 {
status = "okay";
};
#endif
&ecap2 {
status = "okay";
};
&dra7_pmx_core {
pinctrl-names = "default";
pinctrl-0 = <&man2020_pins>;
man2020_pins: man2020_pins {
pinctrl-single,pins = <
0x3B0 (MUX_MODE0 | PIN_INPUT_PULLUP) /* spi1_cs0.spi1_cs0 */
0x3B4 (MUX_MODE0 | PIN_INPUT_PULLUP) /* spi1_cs1.spi1_cs1 */
0x3A4 (MUX_MODE0 | PIN_INPUT_PULLDOWN) /* spi1_sclk.spi1_sclk */
0x3AC (MUX_MODE0 | PIN_INPUT_PULLDOWN) /* spi1_d0.spi1_d0 */
0x3A8 (MUX_MODE0 | PIN_INPUT_PULLDOWN) /* spi1_d1.spi1_d1 */
0x3C8 (MUX_MODE0 | PIN_INPUT_PULLDOWN) /* spi2_d0.spi2_d0 */
0x3C4 (MUX_MODE0 | PIN_INPUT_PULLDOWN) /* spi2_d1.spi2_d1 */
0x3CC (MUX_MODE0 | PIN_INPUT_PULLUP) /* spi2_cs0.spi2_cs0 */
0x3C0 (MUX_MODE0 | PIN_INPUT_PULLDOWN) /* spi2_sclk.spi2_sclk */
0x264 (MUX_MODE7 | PIN_INPUT_PULLDOWN) /* rgmii0_txd0.spi4_cs0 */
0x260 (MUX_MODE7 | PIN_INPUT_PULLDOWN) /* rgmii0_txd1.spi4_d0 */
0x25C (MUX_MODE7 | PIN_INPUT_PULLDOWN) /* rgmii0_txd2.spi4_d1 */
0x258 (MUX_MODE7 | PIN_INPUT_PULLDOWN) /* RGMII0_TXD3.spi4_sclk */
0x40C (MUX_MODE0 | PIN_INPUT_PULLUP) /* i2c2_scl.i2c2_scl */
0x408 (MUX_MODE0 | PIN_INPUT_PULLUP) /* i2c2_sda.i2c2_sda */
0x378 (MUX_MODE2 | PIN_INPUT_PULLUP) /* gpio6_11.i2c3_scl */
0x374 (MUX_MODE2 | PIN_INPUT_PULLUP) /* gpio6_10.i2c3_sda */
0x2AC (MUX_MODE10 | PIN_INPUT_PULLUP) /* mcasp1_aclkr.i2c4_sda */
0x2B0 (MUX_MODE10 | PIN_INPUT_PULLUP) /* mcasp1_fsr.i2c4_scl */
0x2B4 (MUX_MODE10 | PIN_INPUT | SLEWCONTROL) /* mcasp1_axr0.i2c5_sda */
0x2B8 (MUX_MODE10 | PIN_INPUT | SLEWCONTROL) /* mcasp1_axr1.i2c5_scl */
0x314 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp2_axr4.gpio1_4 */
0x3D4 (MUX_MODE14 | PIN_INPUT_PULLUP | SLEWCONTROL) /* dcan1_rx.gpio1_15 */
0x06C (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* gpmc_a11.gpio2_1 */
0x070 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* GPMC_A12.gpio2_2 */
0x0C0 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* gpmc_clk.gpio2_22 */
0x0D4 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* gpmc_ben1.gpio2_27 */
0x31C (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp2_axr6.gpio2_29 */
0x154 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* vin2a_clk0.gpio3_28 */
0x2E8 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp1_axr13.gpio6_4 */
0x288 (MUX_MODE0 | PIN_INPUT_PULLDOWN) /* gpio6_14.gpio6_14 */
0x418 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* Wakeup0.gpio1_0 */
0x41C (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* WAKEUP1.gpio1_1 */
0x320 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp2_axr7.gpio1_5 */
0x2E0 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp1_axr11.gpio4_17 */
0x2E4 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp1_axr12.gpio4_18 */
0x2CC (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp1_axr6.gpio5_8 */
0x2D0 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp1_axr7.gpio5_9 */
0x2D4 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp1_axr8.gpio5_10 */
0x2D8 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp1_axr9.gpio5_11 */
0x2DC (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp1_axr10.gpio5_12 */
0x23C (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mdio_mclk.gpio5_15 */
0x240 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mdio_d.gpio5_16 */
0x24C (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* uart3_txd.gpio5_19 */
0x274 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* rgmii0_rxd2.gpio5_29 */
0x278 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* rgmii0_rxd1.gpio5_30 */
0x27C (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* rgmii0_rxd0.gpio5_31 */
0x2EC (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp1_axr14.gpio6_5 */
0x2F0 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp1_axr15.gpio6_6 */
0x318 (MUX_MODE14 | PIN_INPUT_PULLDOWN | MUX_VIRTUAL_MODE12) /* mcasp2_axr5.gpio6_7 */
0x30C (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* mcasp2_axr2.gpio6_8 */
0x284 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* usb2_drvvbus.gpio6_13 */
0x28C (MUX_MODE0 | PIN_INPUT_PULLDOWN) /* gpio6_15.gpio6_15 */
0x290 (MUX_MODE0 | PIN_INPUT_PULLDOWN) /* gpio6_16.gpio6_16 */
0x298 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* xref_clk1.gpio6_18 */
0x29C (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* xref_clk2.gpio6_19 */
0x2A0 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* xref_clk3.gpio6_20 */
0x3E8 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* uart1_ctsn.gpio7_24 */
0x3EC (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* uart1_rtsn.gpio7_25 */
0x3F0 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* uart2_rxd.gpio7_26 */
0x3F4 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* uart2_txd.gpio7_27 */
0x204 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* VOUT1_D10.gpio8_10 */
0x1E4 (MUX_MODE14 | PIN_INPUT_PULLDOWN) /* VOUT1_D2.gpio8_2 */
0x3E4 (MUX_MODE0 | PIN_INPUT_PULLUP | SLEWCONTROL) /* uart1_txd.uart1_txd */
0x3E0 (MUX_MODE0 | PIN_INPUT_PULLUP | SLEWCONTROL) /* uart1_rxd.uart1_rxd */
0x3F8 (MUX_MODE2 | PIN_INPUT_PULLUP) /* uart2_ctsn.uart3_rxd */
0x3FC (MUX_MODE1 | PIN_INPUT_PULLUP) /* uart2_rtsn.uart3_txd */
0x33C (MUX_MODE4 | PIN_INPUT_SLEW) /* mcasp4_axr0.uart4_rxd */
0x340 (MUX_MODE4 | PIN_INPUT_SLEW) /* mcasp4_axr1.uart4_txd */
0x32C (MUX_MODE4 | PIN_INPUT_PULLUP) /* mcasp3_axr0.uart5_rxd */
0x330 (MUX_MODE4 | PIN_INPUT_PULLUP) /* mcasp3_axr1.uart5_txd */
0x334 (MUX_MODE3 | PIN_INPUT_PULLUP) /* mcasp4_aclkx.uart8_rxd */
0x338 (MUX_MODE3 | PIN_INPUT_PULLUP) /* mcasp4_fsx.uart8_txd */
0x344 (MUX_MODE3 | PIN_INPUT_PULLUP) /* mcasp5_aclkx.uart9_rxd */
0x348 (MUX_MODE3 | PIN_INPUT_PULLUP) /* mcasp5_fsx.uart9_txd */
0x394 (MUX_MODE2 | PIN_INPUT_PULLUP) /* mmc3_dat4.uart10_rxd */
0x398 (MUX_MODE2 | PIN_INPUT_PULLUP) /* MMC3_DAT5.uart10_txd */
0x39C (MUX_MODE2 | PIN_INPUT_PULLUP) /* MMC3_DAT6.uart10_ctsn */
0x3A0 (MUX_MODE2 | PIN_INPUT_PULLUP) /* MMC3_DAT7.uart10_rtsn */
0x2BC (MUX_MODE0 | PIN_INPUT_SLEW) /* mcasp1_axr2.mcasp1_axr2 */
0x2C0 (MUX_MODE0 | PIN_INPUT_SLEW) /* mcasp1_axr3.mcasp1_axr3 */
0x2C4 (MUX_MODE0 | PIN_INPUT_SLEW) /* mcasp1_axr4.mcasp1_axr4 */
0x2C8 (MUX_MODE0 | PIN_INPUT_SLEW) /* mcasp1_axr5.mcasp1_axr5 */
0x2A4 (MUX_MODE0 | PIN_INPUT_PULLDOWN) /* mcasp1_aclkx.mcasp1_aclkx */
0x2A8 (MUX_MODE0 | PIN_INPUT_SLEW) /* mcasp1_fsx.mcasp1_fsx */
0x2F8 (MUX_MODE0 | PIN_INPUT_SLEW | MUX_VIRTUAL_MODE9) /* mcasp2_fsx.mcasp2_fsx */
0x2F4 (MUX_MODE0 | PIN_INPUT_PULLDOWN | MUX_VIRTUAL_MODE9) /* mcasp2_aclkx.mcasp2_aclkx */
0x304 (MUX_MODE0 | PIN_INPUT_PULLDOWN | MUX_VIRTUAL_MODE12) /* mcasp2_axr0.mcasp2_axr0 */
0x308 (MUX_MODE0 | PIN_INPUT_PULLDOWN | MUX_VIRTUAL_MODE12) /* mcasp2_axr1.mcasp2_axr1 */
0x310 (MUX_MODE1 | PIN_INPUT_SLEW | MUX_VIRTUAL_MODE9) /* mcasp2_axr3.mcasp3_axr3 */
0x324 (MUX_MODE0 | PIN_INPUT_PULLDOWN) /* mcasp3_aclkx.mcasp3_aclkx */
0x328 (MUX_MODE0 | PIN_INPUT_SLEW) /* mcasp3_fsx.mcasp3_fsx */
0x158 MUX_MODE4 /* vin2a_de0.VOUT2_DE */
0x1C4 MUX_MODE4 /* vin2a_d23.VOUT2_D0 */
0x1C0 MUX_MODE4 /* VIN2A_D22.VOUT2_D1 */
0x1BC MUX_MODE4 /* VIN2A_D21.vout2_d2 */
0x1B8 MUX_MODE4 /* VIN2A_D20.vout2_d3 */
0x1B4 MUX_MODE4 /* vin2a_d19.VOUT2_D4 */
0x1B0 MUX_MODE4 /* VIN2A_D18.VOUT2_D5 */
0x1AC MUX_MODE4 /* vin2a_d17.VOUT2_D6 */
0x1A8 MUX_MODE4 /* VIN2A_D16.vout2_d7 */
0x1A4 MUX_MODE4 /* VIN2A_D15.vout2_d8 */
0x1A0 MUX_MODE4 /* VIN2A_D14.VOUT2_D9 */
0x19C MUX_MODE4 /* vin2a_d13.VOUT2_D10 */
0x198 MUX_MODE4 /* vin2a_d12.VOUT2_D11 */
0x194 MUX_MODE4 /* VIN2A_D11.VOUT2_D12 */
0x190 MUX_MODE4 /* VIN2A_D10.VOUT2_D13 */
0x18C MUX_MODE4 /* vin2a_d9.VOUT2_D14 */
0x188 MUX_MODE4 /* vin2a_d8.VOUT2_D15 */
0x184 MUX_MODE4 /* VIN2A_D7.VOUT2_D16 */
0x180 MUX_MODE4 /* VIN2A_D6.vout2_d17 */
0x17C MUX_MODE4 /* vin2a_d5.VOUT2_D18 */
0x178 MUX_MODE4 /* vin2a_d4.VOUT2_D19 */
0x174 MUX_MODE4 /* VIN2A_D3.vout2_d20 */
0x170 MUX_MODE4 /* VIN2A_D2.vout2_d21 */
0x16C MUX_MODE4 /* vin2a_d1.VOUT2_D22 */
0x168 MUX_MODE4 /* vin2a_d0.VOUT2_D23 */
0x160 MUX_MODE4 /* VIN2A_HSYNC0.vout2_hsync */
0x164 MUX_MODE4 /* vin2a_vsync0.VOUT2_VSYNC */
0x15C MUX_MODE4 /* VIN2A_FLD0.VOUT2_CLK */
0x000 MUX_MODE3 /* gpmc_ad0.VOUT3_D0 */
0x004 MUX_MODE3 /* gpmc_ad1.VOUT3_D1 */
0x008 MUX_MODE3 /* gpmc_ad2.VOUT3_D2 */
0x00C MUX_MODE3 /* GPMC_AD3.vout3_d3 */
0x010 MUX_MODE3 /* gpmc_ad4.VOUT3_D4 */
0x014 MUX_MODE3 /* gpmc_ad5.VOUT3_D5 */
0x018 MUX_MODE3 /* GPMC_AD6.vout3_d6 */
0x01C MUX_MODE3 /* GPMC_AD7.vout3_d7 */
0x020 MUX_MODE3 /* GPMC_AD8.vout3_d8 */
0x024 MUX_MODE3 /* GPMC_AD9.vout3_d9 */
0x028 MUX_MODE3 /* GPMC_AD10.vout3_d10 */
0x02C MUX_MODE3 /* GPMC_AD11.vout3_d11 */
0x030 MUX_MODE3 /* gpmc_ad12.VOUT3_D12 */
0x034 MUX_MODE3 /* gpmc_ad13.VOUT3_D13 */
0x038 MUX_MODE3 /* gpmc_ad14.VOUT3_D14 */
0x03C MUX_MODE3 /* gpmc_ad15.vout3_d15 */
0x050 MUX_MODE3 /* GPMC_A4.VOUT3_D20 */
0x054 MUX_MODE3 /* GPMC_A5.VOUT3_D21 */
0x044 MUX_MODE3 /* GPMC_A1.VOUT3_D17 */
0x048 MUX_MODE3 /* gpmc_a2.VOUT3_D18 */
0x04C MUX_MODE3 /* GPMC_A3.vout3_d19 */
0x040 MUX_MODE3 /* GPMC_A0.VOUT3_D16 */
0x058 MUX_MODE3 /* GPMC_A6.VOUT3_D22 */
0x05C MUX_MODE3 /* GPMC_A7.VOUT3_D23 */
0x060 MUX_MODE3 /* GPMC_A7.VOUT3_HSYNC */
0x064 MUX_MODE3 /* GPMC_A9.vout3_vsync */
0x0BC MUX_MODE3 /* GPMC_CS3.vout3_clk */
0x21C MUX_MODE4 /* VOUT1_D16.VIN3A_D0 */
0x228 MUX_MODE4 /* VOU1_D19.VIN3A_D3 */
0x238 MUX_MODE4 /* VOU1_D23.VIN3A_D7 */
0x220 MUX_MODE4 /* VOU1_D17.VIN3A_D1 */
0x22C MUX_MODE4 /* VOU1_D20.VIN3A_D4 */
0x224 MUX_MODE4 /* VOU1_D18.VIN3A_D2 */
0x230 MUX_MODE4 /* VOU1_D21.VIN3A_D5 */
0x234 MUX_MODE4 /* VOU1_D22.VIN3A_D6 */
0x1D0 MUX_MODE4 /* vout1_fld.VIN3A_CLK0 */
0x36C MUX_MODE0 /* MMC1_SDCD.MMC1_SDCD */
0x370 MUX_MODE0 /* MMC1_SDWP.MMC1_SDWP */
0x254 (MUX_MODE2 | PIN_INPUT ) /* rgmii0_txctl.rmii1_rxd0 */
0x250 (MUX_MODE2 | PIN_INPUT ) /* rgmii0_txc.rmii1_rxd1 */
0x270 (MUX_MODE2 | PIN_OUTPUT ) /* rgmii0_rxd3.rmii1_txd0 */
0x26C (MUX_MODE2 | PIN_OUTPUT ) /* rgmii0_rxctl.rmii1_txd1 */
0x248 (MUX_MODE2 | PIN_INPUT ) /* uart3_rxd.rmii1_crs */
0x268 (MUX_MODE2 | PIN_OUTPUT ) /* rgmii0_rxc.rmii1_txen */
0x244 (MUX_MODE0 | PIN_INPUT ) /* RMII_MHZ_50_CLK.RMII_MHZ_50_CLK */
0x3B8 (MUX_MODE5 | PIN_INPUT_PULLDOWN) /* spi1_cs2.MDIO_MCLK */
0x3BC (MUX_MODE5 | PIN_INPUT_PULLDOWN) /* spi1_cs3.MDIO_D */
0x434 MUX_MODE0 /* TDI.TDI */
0x444 MUX_MODE0 /* RTCK.RTCK */
0x448 MUX_MODE0 /* EMU0.EMU0 */
0x44C MUX_MODE0 /* EMU1.EMU1 */
0x294 (MUX_MODE9 | PIN_INPUT) /* xref_clk0.clkout2 */
0x280 MUX_MODE0 /* usb1_drvvbus.usb1_drvvbus */
0x000 MUX_MODE0 /* gpmc_ad0 */
0x004 MUX_MODE0 /* gpmc_ad1 */
0x008 MUX_MODE0 /* gpmc_ad2 */
0x00C MUX_MODE0 /* GPMC_AD3.gpmc_ad3 */
0x010 MUX_MODE0 /* gpmc_ad4 */
0x014 MUX_MODE0 /* gpmc_ad5 */
0x018 MUX_MODE0 /* GPMC_AD6.gpmc_ad6 */
0x01C MUX_MODE0 /* GPMC_AD7.gpmc_ad7 */
0x020 MUX_MODE0 /* GPMC_AD8.gpmc_ad8 */
0x024 MUX_MODE0 /* GPMC_AD9.gpmc_ad9 */
0x028 MUX_MODE0 /* GPMC_AD10.gpmc_ad10 */
0x02C MUX_MODE0 /* GPMC_AD11.gpmc_ad11 */
0x030 MUX_MODE0 /* gpmc_ad12 */
0x034 MUX_MODE0 /* gpmc_ad13 */
0x038 MUX_MODE0 /* gpmc_ad14 */
0x03C MUX_MODE0 /* gpmc_ad15 */
0x0B4 (MUX_MODE0 | PIN_OUTPUT) /* gpmc_cs0.gpmc_cs0 */
0x0C4 (MUX_MODE0 | PIN_OUTPUT) /* gpmc_advn_ale.gpmc_advn_ale */
0x0C8 (MUX_MODE0 | PIN_OUTPUT) /* gpmc_oen_ren.gpmc_oen_ren */
0x0CC (MUX_MODE0 | PIN_OUTPUT) /* gpmc_wen.gpmc_wen */
0x0D0 (MUX_MODE0 | PIN_OUTPUT) /* gpmc_ben0.gpmc_ben0 */
0x0D8 (MUX_MODE0 | PIN_INPUT | SLEWCONTROL) /* gpmc_wait0.gpmc_wait0 */
>;
};
mmc3_pins_default: pinmux_mmc3_default_pins {
pinctrl-single,pins = <
0x380 (MUX_MODE0 | PIN_INPUT_PULLUP) /* MMC3_CMD.MMC3_CMD */
0x37C (MUX_MODE0 | PIN_INPUT_PULLUP) /* mmc3_clk.mmc3_clk */
0x384 (MUX_MODE0 | PIN_INPUT_PULLUP) /* mmc3_dat0.mmc3_dat0 */
0x388 (MUX_MODE0 | PIN_INPUT_PULLUP) /* mmc3_dat1.mmc3_dat1 */
0x38C (MUX_MODE0 | PIN_INPUT_PULLUP) /* mmc3_dat2.mmc3_dat2 */
0x390 (MUX_MODE0 | PIN_INPUT_PULLUP) /* mmc3_dat3.mmc3_dat3 */
>;
};
vin3a_pins: pinmux_vin3a_pins {
pinctrl-single,pins = <
0x21C MUX_MODE4 /* VOUT1_D16.VIN3A_D0 */
0x228 MUX_MODE4 /* VOU1_D19.VIN3A_D3 */
0x238 MUX_MODE4 /* VOU1_D23.VIN3A_D7 */
0x220 MUX_MODE4 /* VOU1_D17.VIN3A_D1 */
0x22C MUX_MODE4 /* VOU1_D20.VIN3A_D4 */
0x224 MUX_MODE4 /* VOU1_D18.VIN3A_D2 */
0x230 MUX_MODE4 /* VOU1_D21.VIN3A_D5 */
0x234 MUX_MODE4 /* VOU1_D22.VIN3A_D6 */
0x1D0 MUX_MODE4 /* vout1_fld.VIN3A_CLK0 */
>;
};
};
&pbias_mmc_reg {
regulator-max-microvolt = <3300000>;
};
&mmc3 {
/* from mmc-1 */
status = "okay";
vmmc-supply = <&evm_3v3_sw>;
bus-width = <4>;
ti,non-removable;
/*
* SDCD signal is not being used here - using the fact that GPIO mode
* is always hardwired.
*/
//cd-gpios = <&gpio7 12 GPIO_ACTIVE_LOW>;
max-frequency = <64000000>;
pinctrl-names = "default";
pinctrl-0 = <&mmc3_pins_default>;
};
&lcd {
enable-gpios = <>; /* P15, CON_LCD_PWR_DN */
};
Regards,
Shawn