Part Number: AM5728
Tool/software: Linux
Hello,
How can i install and use TensorFlow on the arago- linux i.e AM5728 evm.
Thanks and Regards,
Hiren Kumbhare
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM5728
Tool/software: Linux
Hello,
How can i install and use TensorFlow on the arago- linux i.e AM5728 evm.
Thanks and Regards,
Hiren Kumbhare
Hi Hiren,
Can you please elaborate your requirement? What are you trying to do on AM57x? I would like to highlight that AM57x device supports running only the inference side of Deep Learning and doesn't support training. Do you already have some network model developed using Tensor Flow?
We have Processor SDK 5.0 release coming up (scheduled early next week) and will be packaged with TI Deep Learning solution. The release will have document on TIDL, that can help explain our offerings.
Regards,
Manisha
Hello Manisha,
Thanks for your support.
Our project requirement are face recognition using 4 ip cameras. We are currently working on the OpenCV 3.1. We are facing lots of issuses with opencv so wanted to try Tensorflow.
Problems faced in OpenCV
1) When we play rtsp stream directly using gstreamer (1080p resolution) it play correctly but when i just use the opencv api (even threading) the video lags a lot.
2) If this is the case for the 1 IP camera this is not gonna work for 4 Camera stream.
If there is any solutions to this issue then we can use opencv only.
How to use the hardware decoder to speedup the video processing in opencv?
Thanks and Regards,
Hiren Kumbhare
Hello Rex,
Actually, we are working with together. Please, check the code in attached file.
Regards,
Kishan Patel.g_opencv.cpp
Hello Rex,
Thanks for your valuable time.
But we are not clear about the solution.
As Margarita suggested to bitbake "omapdrmtest" we did that and facing some error. Mentioning the Error below.
As per you it is not needed, then what we need to do to solve this issue please guide us.
We have also tried to use the direct OpenCV "Videocapture cap" to use rtsp stream.
Bitbake error:
MACHINE=am57xx-evm bitbake omapdrmtest --force -c compile
Loading cache: 100% |###########################################################################################################| Time: 0:00:01
Loaded 4043 entries from dependency cache.
Parsing recipes: 100% |#########################################################################################################| Time: 0:00:11
Parsing of 3137 .bb files complete (3134 cached, 3 parsed). 4046 targets, 439 skipped, 0 masked, 0 errors.
WARNING: No recipes available for:
/home/hiren/Facial/tisdk/sources/meta-arago/meta-arago-distro/recipes-multimedia/gstreamer/gstreamer1.0-plugins-base_1.8.3.bbappend
/home/hiren/Facial/tisdk/sources/meta-processor-sdk/recipes-devtools/python/python3-native_3.5.2.bbappend
/home/hiren/Facial/tisdk/sources/meta-processor-sdk/recipes-graphics/wayland/weston_1.11.0.bbappend
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "1.36.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-16.04"
TARGET_SYS = "arm-linux-gnueabi"
MACHINE = "am57xx-evm"
DISTRO = "arago"
DISTRO_VERSION = "2018.04"
TUNE_FEATURES = "arm armv7a vfp thumb neon callconvention-hard"
TARGET_FPU = "hard"
meta-processor-sdk = "HEAD:264dc66c689e0e4212c43358382986ee470619d4"
meta-ros = "HEAD:e2566402ab108a19634354a934788109422cf409"
meta-arago-distro
meta-arago-extras = "HEAD:d54e9d6c1d461dbf3189e691088d328bf4c4fb19"
meta-browser = "HEAD:26d50665e2f7223c5f4ad7481a8d2431e7cb55fb"
meta-qt5 = "HEAD:682ad61c071a9710e9f9d8a32ab1b5f3c14953d1"
meta-networking
meta-python
meta-oe
meta-gnome
meta-multimedia = "HEAD:352531015014d1957d6444d114f4451e241c4d23"
meta-ti = "HEAD:8555084679dc5c668e5fb60a16425ca32b10ff21"
meta-linaro-toolchain
meta-optee = "HEAD:75dfb67bbb14a70cd47afda9726e2e1c76731885"
meta = "HEAD:931a52e8698f684ccbb26ddec18764ad9d9a3e8f"
NOTE: Tainting hash to force rebuild of task /home/hiren/Facial/tisdk/sources/meta-arago/meta-arago-extras/recipes-graphics/omapdrmtest/omapdrmtest_1.0.0.bb, do_compile
WARNING: /home/hiren/Facial/tisdk/sources/meta-arago/meta-arago-extras/recipes-graphics/omapdrmtest/omapdrmtest_1.0.0.bb.do_compile is tainted from a forced run
Initialising tasks: 100% |######################################################################################################| Time: 0:00:03
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: bc-native-1.06-r3 do_fetch: Failed to fetch URL ftp.gnu.org/.../bc-1.06.tar.gz, attempting MIRRORS if available
WARNING: gperf-native-3.1-r0 do_fetch: Failed to fetch URL ftp.gnu.org/.../gperf-3.1.tar.gz, attempting MIRRORS if available
WARNING: libpng-native-1.6.31-r0 do_fetch: Failed to fetch URL downloads.sourceforge.net/.../libpng-1.6.31.tar.xz, attempting MIRRORS if available
WARNING: libogg-1.3.2-r0 do_fetch: Checksum mismatch for local file /home/hiren/Facial/tisdk/downloads/libogg-1.3.2.tar.xz
Cleaning and trying again.
WARNING: libogg-1.3.2-r0 do_fetch: Renaming /home/hiren/Facial/tisdk/downloads/libogg-1.3.2.tar.xz to /home/hiren/Facial/tisdk/downloads/libogg-1.3.2.tar.xz_bad-checksum_5429e1811b045912a85cf29761b57fb3
WARNING: libogg-1.3.2-r0 do_fetch: Checksum failure encountered with download of downloads.xiph.org/.../libogg-1.3.2.tar.xz - will attempt other sources if available
ERROR: linux-ti-staging-4.14.40+gitAUTOINC+4796173fc5-r7a.arago5.tisdk0.1 do_create_srcipk: Function failed: do_create_srcipk (log file is located at /home/hiren/Facial/tisdk/build/arago-tmp-external-linaro-toolchain/work/am57xx_evm-linux-gnueabi/linux-ti-staging/4.14.40+gitAUTOINC+4796173fc5-r7a.arago5.tisdk0.1/temp/log.do_create_srcipk.10040)
ERROR: Logfile of failure stored in: /home/hiren/Facial/tisdk/build/arago-tmp-external-linaro-toolchain/work/am57xx_evm-linux-gnueabi/linux-ti-staging/4.14.40+gitAUTOINC+4796173fc5-r7a.arago5.tisdk0.1/temp/log.do_create_srcipk.10040
Log data follows:
| DEBUG: Executing python function sstate_task_prefunc
| DEBUG: Python function sstate_task_prefunc finished
| DEBUG: Executing shell function do_create_srcipk
| Cloning into '/home/hiren/Facial/tisdk/build/arago-tmp-external-linaro-toolchain/work/am57xx_evm-linux-gnueabi/linux-ti-staging/4.14.40+gitAUTOINC+4796173fc5-r7a.arago5.tisdk0.1/temp-git-shallow-clone'...
| error: --shallow-file died of signal 9
| error: git upload-pack: git-pack-objects died with error.
| fatal: git upload-pack: aborting due to possible repository corruption on the remote side.
| remote: aborting due to possible repository corruption on the remote side.
| fatal: early EOF
| fatal: index-pack failed
| WARNING: /home/hiren/Facial/tisdk/build/arago-tmp-external-linaro-toolchain/work/am57xx_evm-linux-gnueabi/linux-ti-staging/4.14.40+gitAUTOINC+4796173fc5-r7a.arago5.tisdk0.1/temp/run.do_create_srcipk.10040:1 exit 128 from 'git clone --depth 400 --branch processor-sdk-linux-4.14.y file://$PWD/.git $gitshallowclone'
| ERROR: Function failed: do_create_srcipk (log file is located at /home/hiren/Facial/tisdk/build/arago-tmp-external-linaro-toolchain/work/am57xx_evm-linux-gnueabi/linux-ti-staging/4.14.40+gitAUTOINC+4796173fc5-r7a.arago5.tisdk0.1/temp/log.do_create_srcipk.10040)
ERROR: Task (/home/hiren/Facial/tisdk/sources/meta-ti/recipes-kernel/linux/linux-ti-staging_4.14.bb:do_create_srcipk) failed with exit code '1'
NOTE: Tasks Summary: Attempted 930 tasks of which 355 didn't need to be rerun and 1 failed.
Summary: 1 task failed:
/home/hiren/Facial/tisdk/sources/meta-ti/recipes-kernel/linux/linux-ti-staging_4.14.bb:do_create_srcipk
Summary: There were 8 WARNING messages shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.
Thanks and Regards,
Hiren Kumbhare