Other Parts Discussed in Thread: AM5728
Hello team,
Hope you are doing well. When you get a chance please provide some feedback to below customer questions on AM5718:
1) Are the codecs readily available for the IVA-HD on the AM5718? Which codecs are available?
2) This appears to be contained in an SDK, is that available?
3) It appears to use the same linked M4 system as on the DM8107. What codecs have been tested on the AM5718?
4) Is there documentation detailing the internal routing from the VIP to the IVA-HD like there is on the DM8107? Is it available? How do we access this?
5) In the errata it appears that there are issues with the SATA. How serious are these issues and do they usually affect the operation of the SATA? On the DM8107 from time to time we get SATA unlocks.
6) It says that the BGA is thermally enhanced plastic with a plastic lid. From the drawing it almost appears as if it is metal. Since it dissipates almost 3W at full power, we were just wondering.