Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: AM3352, TPS65910
Tool/software: Linux
Hey Team !
I am trying to interface lan9514 with am335x but it is not getting enumerated .Can you give some light to move forward. I am attaching the log of my boot process. The device tree entity which i have used is like
&usb0 {
status = "okay";
dr_mode = "host";
};
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.4.91-g9d9bc78b62 (dell@dell-Inspiron-3543) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.18
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: TI AM335x EVM
[ 0.000000] cma: Reserved 48 MiB at 0x9d000000
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 129920
[ 0.000000] Kernel command line: console=tty0 console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 459300K/524288K available (7231K kernel code, 291K rwdata, 2416K rodata, 276K init, 275K bss, 15836K reserved, 49152K c)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xe0800000 - 0xff800000 ( 496 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0974034 (9649 kB)
[ 0.000000] .init : 0xc0975000 - 0xc09ba000 ( 276 kB)
[ 0.000000] .data : 0xc09ba000 - 0xc0a02d40 ( 292 kB)
[ 0.000000] .bss : 0xc0a02d40 - 0xc0a47be0 ( 276 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 25000000 Hz
[ 0.000014] sched_clock: 32 bits at 25MHz, resolution 40ns, wraps every 85899345900ns
[ 0.000031] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 76450417870 ns
[ 0.000040] OMAP clocksource: timer1 at 25000000 Hz
[ 0.000185] clocksource_probe: no matching clocksources found
[ 0.000357] Console: colour dummy device 80x30
[ 0.001098] console [tty0] enabled
[ 0.001133] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.001159] This ensures that you still see kernel messages. Please
[ 0.001185] update your kernel commandline.
[ 0.001220] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)
[ 0.089241] pid_max: default: 32768 minimum: 301
[ 0.089369] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.089403] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.090049] Initializing cgroup subsys io
[ 0.090107] Initializing cgroup subsys memory
[ 0.090159] Initializing cgroup subsys devices
[ 0.090191] Initializing cgroup subsys freezer
[ 0.090223] Initializing cgroup subsys perf_event
[ 0.090252] Initializing cgroup subsys pids
[ 0.090296] CPU: Testing write buffer coherency: ok
[ 0.090692] Setting up static identity map for 0x80008200 - 0x80008260
[ 0.092554] devtmpfs: initialized
[ 0.102867] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.116141] omap_hwmod: debugss: _wait_target_disable failed
[ 0.170898] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.170981] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.174471] pinctrl core: initialized pinctrl subsystem
[ 0.175687] NET: Registered protocol family 16
[ 0.177697] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.199219] cpuidle: using governor ladder
[ 0.229207] cpuidle: using governor menu
[ 0.233183] OMAP GPIO hardware version 0.1
[ 0.242832] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.286384] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.289797] SCSI subsystem initialized
[ 0.290113] usbcore: registered new interface driver usbfs
[ 0.290209] usbcore: registered new interface driver hub
[ 0.290343] usbcore: registered new device driver usb
[ 0.290760] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring e
[ 0.290857] omap_i2c 4802a000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c1_pins, deferring e
[ 0.291012] media: Linux media interface: v0.10
[ 0.291082] Linux video capture interface: v2.00
[ 0.291147] pps_core: LinuxPPS API ver. 1 registered
[ 0.291172] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.291232] PTP clock support registered
[ 0.291296] EDAC MC: Ver: 3.0.0
[ 0.292325] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.292674] Advanced Linux Sound Architecture Driver Initialized.
[ 0.294332] clocksource: Switched to clocksource timer1
[ 0.303685] NET: Registered protocol family 2
[ 0.304510] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.304587] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.304645] TCP: Hash tables configured (established 4096 bind 4096)
[ 0.304747] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.304785] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.304940] NET: Registered protocol family 1
[ 0.305324] RPC: Registered named UNIX socket transport module.
[ 0.305367] RPC: Registered udp transport module.
[ 0.305390] RPC: Registered tcp transport module.
[ 0.305414] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.306342] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.315113] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.315886] NFS: Registering the id_resolver key type
[ 0.315981] Key type id_resolver registered
[ 0.316005] Key type id_legacy registered
[ 0.316095] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.320820] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
[ 0.320900] io scheduler noop registered
[ 0.320931] io scheduler deadline registered
[ 0.321086] io scheduler cfq registered (default)
[ 0.322282] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.325066] backlight supply power not found, using dummy regulator
[ 0.377083] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.380709] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 158, base_baud = 3000000) is a 8250
[ 1.022879] console [ttyS0] enabled
[ 1.027582] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 159, base_baud = 3000000) is a 8250
[ 1.037478] [drm] Initialized drm 1.1.0 20060810
[ 1.042997] panel panel: pins are not configured
[ 1.049050] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.055848] [drm] No driver support for vblank timestamp query.
[ 1.085108] Console: switching to colour frame buffer device 100x30
[ 1.095705] tilcdc 4830e000.lcdc: fb0: frame buffer device
[ 1.124504] [drm] Initialized tilcdc 1.0.0 20121205 on minor 0
[ 1.137926] loop: module loaded
[ 1.144664] pinctrl-single 44e10800.pinmux: pin 44e10954.0 already requested by 44e10800.pinmux; cannot claim for 48030000.spi
[ 1.159599] pinctrl-single 44e10800.pinmux: pin-85 (48030000.spi) status -22
[ 1.168413] pinctrl-single 44e10800.pinmux: could not request pin 85 (44e10954.0) from group myspi0_pins_default on device pinctrl-single
[ 1.184274] omap2_mcspi 48030000.spi: Error applying setting, reverse things back
[ 1.196736] libphy: Fixed MDIO Bus: probed
[ 1.264352] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[ 1.272357] davinci_mdio 4a101000.mdio: detected phy mask ffffffef
[ 1.281116] libphy: 4a101000.mdio: probed
[ 1.287016] davinci_mdio 4a101000.mdio: phy[4]: device 4a101000.mdio:04, driver SMSC LAN8710/LAN8720
[ 1.300540] cpsw 4a100000.ethernet: Detected MACID = 98:5d:ad:30:cf:76
[ 1.309344] cpsw 4a100000.ethernet: cpts: overflow check period 850
[ 1.318544] usbcore: registered new interface driver rndis_wlan
[ 1.326607] usbcore: registered new interface driver cdc_ether
[ 1.334385] usbcore: registered new interface driver smsc95xx
[ 1.341997] usbcore: registered new interface driver rndis_host
[ 1.350085] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.358485] ehci-pci: EHCI PCI platform driver
[ 1.364749] ehci-platform: EHCI generic platform driver
[ 1.371865] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 1.380108] usbcore: registered new interface driver usb-storage
[ 1.389837] 47401300.usb-phy supply vcc not found, using dummy regulator
[ 1.400735] musb-hdrc musb-hdrc.0.auto: Failed to request rx1.
[ 1.408587] musb-hdrc musb-hdrc.0.auto: musb_init_controller failed with status -517
[ 1.419227] 47401b00.usb-phy supply vcc not found, using dummy regulator
[ 1.430066] musb-hdrc musb-hdrc.1.auto: Failed to request rx1.
[ 1.437942] musb-hdrc musb-hdrc.1.auto: musb_init_controller failed with status -517
[ 1.453454] mousedev: PS/2 mouse device common for all mice
[ 1.461714] i2c /dev entries driver
[ 1.468116] cpuidle: enable-method property 'ti,am3352' found operations
[ 1.554995] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.565619] NET: Registered protocol family 10
[ 1.573084] sit: IPv6 over IPv4 tunneling driver
[ 1.580228] NET: Registered protocol family 17
[ 1.586818] Key type dns_resolver registered
[ 1.592912] omap_voltage_late_init: Voltage driver support not added
[ 1.609677] mmc0: host does not support reading read-only switch, assuming write-enable
[ 1.623524] mmc0: new high speed SDHC card at address aaaa
[ 1.630872] tps65910 0-002d: No interrupt support, no core IRQ
[ 1.638929] mmcblk0: mmc0:aaaa SU04G 3.69 GiB
[ 1.645823] tps65910 0-002d: Error in configuring external control EN1
[ 1.654807] tps65910 0-002d: Failed to initialise ext control config
[ 1.662902] mmcblk0: p1 p2
[ 1.667716] tps65910 0-002d: Error in configuring external control EN1
[ 1.676815] tps65910 0-002d: Failed to initialise ext control config
[ 1.686415] vio: failed to enable
[ 1.693511] tps65910 0-002d: failed to register tps65910-pmic regulator
[ 1.702116] tps65910-pmic: probe of tps65910-pmic failed with error -121
[ 1.712826] rtc-ds1307 0-006f: rtc core: registered mcp7940x as rtc0
[ 1.721125] rtc-ds1307 0-006f: 64 bytes nvram
[ 1.730578] pinctrl-single 44e10800.pinmux: pin 44e10954.0 already requested by 44e10800.pinmux; cannot claim for 0-0070
[ 1.744964] pinctrl-single 44e10800.pinmux: pin-85 (0-0070) status -22
[ 1.753260] pinctrl-single 44e10800.pinmux: could not request pin 85 (44e10954.0) from group gpio_pins on device pinctrl-single
[ 1.768332] pca954x 0-0070: Error applying setting, reverse things back
[ 1.777010] pca954x 0-0070: probe failed
[ 1.783463] input: ft5x06_ts as /devices/platform/ocp/44e0b000.i2c/i2c-0/0-0038/input/input0
[ 1.794472] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 1.803238] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 100 kHz
[ 1.810817] mmc1: MAN_BKOPS_EN bit is not set
[ 1.817281] backlight supply power not found, using dummy regulator
[ 1.827541] mmc1: new high speed MMC card at address 0001
[ 1.839521] musb-hdrc musb-hdrc.0.auto: MUSB HDRC host driver
[ 1.847854] mmcblk1: mmc1:0001 004G60 3.69 GiB
[ 1.854476] musb-hdrc musb-hdrc.0.auto: new USB bus registered, assigned bus number 1
[ 1.864397] mmcblk1boot0: mmc1:0001 004G60 partition 1 2.00 MiB
[ 1.872377] mmcblk1boot1: mmc1:0001 004G60 partition 2 2.00 MiB
[ 1.881028]
[ 1.881028] ++++++++++++++hub_probe++++++++++++++
[ 1.891572] hub 1-0:1.0: USB hub found
[ 1.897263] mmcblk1: p1 p2
[ 1.902030] hub 1-0:1.0: 1 port detected
[ 1.915891] musb-hdrc musb-hdrc.1.auto: MUSB HDRC host driver
[ 1.923498] musb-hdrc musb-hdrc.1.auto: new USB bus registered, assigned bus number 2
[ 1.933951]
[ 1.933951] ++++++++++++++hub_probe++++++++++++++
[ 1.943761] hub 2-0:1.0: USB hub found
[ 1.949207] hub 2-0:1.0: 1 port detected
[ 1.955733] backlight supply power not found, using dummy regulator
[ 1.965122] rtc-ds1307 0-006f: setting system clock to 2018-08-28 12:53:06 UTC (1535460786)
[ 1.978457] lis3_reg: disabling
[ 1.983407] ALSA device list:
[ 1.988136] No soundcards found.
[ 2.139319] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 2.148888] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 2.161174] devtmpfs: mounted
[ 2.165867] Freeing unused kernel memory: 276K
[ 2.171784] This architecture does not have kernel memory protection.
with regards
pranav