Part Number: 66AK2L06
Other Parts Discussed in Thread: RFSDK, ADC14X250, DAC38J84
Hi All,
We want to sample analog signal in high speed with 66AK2L EVM.
We setup the boards by using the Optimized Radar System Design Using 66AK2L06 - DSP+ARM SoC and ADC14X250
We fed the ADC by the signal generator. We only want to sample the analog signal. Thats why we use only the ADC board and the LMK board. LMK and ADC is configured.
Setup photo is attached.
We follow RFSDK Installation Guide Release 02.00.07.00 Notes.
But we cannot make 1x1-1xLTE80-HC-JESD121121x-DEMO2 work.
On the last step, in linux console;
radio reset
radio select 1x1-1xLTE80-HC-JESD121121x-DEMO2
radio init
Program LMK and ADC (66AK2L06_dac491_adc245_demo2.cfg & ADC14X250_Cal.cfg)
Playback program
Playback start
all are ok. But when we open the browser;
we can not change the radio state to on --> Radio Control "on", error occurs
"Operation failed (Response header: 'rfsdk.error: rfsdkService.Iqn2Start() API call failed with status 'RFSDK_API_RESULT_APISEQ_IQN_INVALID_STATE' (86) '"
Similary load playback gives error. And also reset gives errors.
We check all the steps, what can you advise?
WEB Page :
Test Setup :