This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/BEAGLEBK: McASP in I2S master mode - clock rate issue (BLCK, WS)

Part Number: BEAGLEBK


Tool/software: Linux

Hi, I am having an issue with the WS and BCLK rate being produced by my system as running the McASP in I2S master mode.  I am interfacing the Beaglebone Black over I2S with a BT radio. 

When I play the 44.1kHz audio my printk() statements produce the following parameters with good audio and a scoped output to match.

[ 1022.052468] sample_size=16
[ 1022.052482] rate=44100
[ 1022.052493] sysclk=24000000
[ 1022.052496] bclk_freq=1411200

When I play the 8kHz audio my printk() statements produce the following parameters but the audio us speed up and the scoped output does not match the parameters.

[ 1081.128650] sample_size=16
[ 1081.128664] rate=8000
[ 1081.128673] sysclk=24000000
[ 1081.128677] bclk_freq=256000

My scope output produces a BCLK at 827.8kHz (rather then 256kHz) and a WS signal at 25.86kHz (rather then 8kHz).  My guess would be this has to-do with a mis-match in mapping the rates to the clock divider circuitry described in section 22.3.5.1 of spruh73p.pdf.  I am just not sure where to find this mapping inside the linux kernel drivers.  I am using 4.14.40 from the TI sdk and my drivers have been largely taken from the steps in: http://processors.wiki.ti.com/index.php/Sitara_Linux_Audio_DAC_Example.

  • Hi Galen,

    Do you use BEAGLEBK or custom board that is based on BEAGLEBK?

    Do you use AM335x McASP module in master mode?

    The McASP BCLK and WS are configured in McASP driver:

    linux-4.14.40/sound/soc/davinci/davinci-mcasp.c

    In this driver are configured McASP registers XFMT, AFSXCTL, ACLKXCTL, AHCLKXCTL, etc

    You can also explore below file:

    linux-4.14.40/sound/soc/soc-core.c

    Regards,
    Pavel
  • Hi Pavel,

    Thank you, soc-core.c looks very useful in finding the issue.  The Beaglebone-Black is stock, then interfaced through P9 to my custom board.  I am using the McASP is in master mode on McASP0.  The device tree is configured as follows:

    	mcasp0_pins: mcasp0_pins {
    		pinctrl-single,pins = <
    			AM33XX_IOPAD(0x990, PIN_OUTPUT_PULLDOWN | MUX_MODE0)	/* MCASP0_ACLKX.mcasp0_aclkx */
    			AM33XX_IOPAD(0x9AC, PIN_OUTPUT_PULLDOWN | MUX_MODE0)	/* MCASP0_AHCLKX.mcasp0_ahclkx*/
    			AM33XX_IOPAD(0x994, PIN_OUTPUT_PULLDOWN | MUX_MODE0)	/* MCASP0_FSX.mcasp0_fsx */
    			AM33XX_IOPAD(0x998, PIN_OUTPUT_PULLDOWN | MUX_MODE0)	/* MCASP0_AXR0.mcasp0_axr0*/
    			AM33XX_IOPAD(0x99C, PIN_INPUT_PULLDOWN | MUX_MODE2)	    /* MCASP0_AHCLKR.mcasp0_axr2 */
    		>;
    	};

    Regards,
    Galen

  • Galen,

    You can also refer to the below documents, where McASP clock scheme is explained:

    www.ti.com/.../sprac97.pdf
    www.ti.com/.../sprac09a.pdf
    www.ti.com/.../sprac10.pdf

    Regards,
    Pavel
  • Hi Pavel,

    Thanks for the documents they look very interesting.  I believe I located where the issue is.  My driver along with the example are only setting clock div_id 1 which corresponds to the BCLK which sets ACLKXCRL[4-0].  When I am running at 8kHz the divider is calculated as 93 (0x5D).  When masked out in the function (as this divider is only 1-32) __davinci_mcasp_set_clkdiv() I get 0x1D which corresponds to the rates I see on the scope. 

    I think if I modify my diver to handle not only setting the divider ACLKXCRL[4-0] but also the larger divider AHLKXCTL[11-0] which feeds BCLK it should be able to work with these slower rates.

    Thanks for the help,
    Galen