This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5708: Pin PR2_MIIx_RXLINK pin additional information

Part Number: AM5708


Looking for some additional information on the PR2_MII0_RXLINK and PR2_MII1_RXLINK  input pins.  I assume these pins originate from the PHY with regard to Link Status.  Are they required to implement PRP?  If yes, what is the polarity when LINK is ACTIVE?   If not required, is a pull-up or pull-down required.

Thanks

RD