Part Number: TMS320C6678
Tool/software: TI-RTOS
Hi, Experts
We have some issues with 6678 phy when our board is connected to a 100Mbps PHY. It's performance can only reach 10% of full rate (10Mbps) . Then we connected it to a 1000M phy the number is 40%(400Mbps).
The PHY/SGMII is set as 1000MBps, auto neg, dulplex full as default in both cases.
My question is
a. Why the board work so bad with a 100M Switch when we set it as 1000MBps,auto neg ?
b. How to make the 6678 sgmii work in 100M mode ? I tried to modify sgmiiCfg.linkSpeed = CSL_SGMII_100_MBPS in evmc66x_phy.c ,mcsdk_2_01_02_05 but it does not work, still in 1000Mbps from a PC view when the board is connected directly with it. I also tried to enable master mode and disable auto neg, neither works.
Looking forward to your replies.
striker