Part Number: AM5728
Tool/software: TI-RTOS
Hi all,
We plan to interface an asynchronous memory to GPMC of AM5728. We understand that the GPMC_FCLK is 133MHz.
From the GPMC timing parameters, I find that maximum RDACCESSTIME / WTACCESSTIME of GPMC is 233ns (7.5187ns*31clk).
But the memory device choosen has 575ns of read/write accesstime.
1. Is there a way the GPMC can be interfaced with this memory device of higher read access time with the same GPMC_FCLK of 133MHz?
2. lowering GPMC_FCLK or L3 Clock (such that the readaccess time of memory device is met) is the only option. Is this correct?
3. Please, tell me how to lower the GPMC_FCLK.
Thanks.
Regards,
SangWook