Tool/software: Linux
Hi All,
We have developed one custom board based on AM5718. We are able to configure PWM successfully for LED. But when we trigger the command for set the PWM period or Duty Cycle.
We will get the below error.
44000000.ocp:L3 Custom Error: MASTER MPU TARGET L4_PER1_P3 (Idle): Data Access in Supervisor mode during Functional access
[ 305.308519] Modules linked in: dwc3 udc_core usb_common snd_soc_simple_card snd_soc_simple_card_utils leds_gpio snd_soc_omap_hdmi_audio ahci_platform libahci_platform libahci omap_aes_driver libata ti)
[ 305.349843] CPU: 0 PID: 398 Comm: sh Tainted: G W O 4.9.59-g9a257488d4 #419
[ 305.357788] Hardware name: Generic DRA72X (Flattened Device Tree)
[ 305.363902] Backtrace:
[ 305.366365] [<c020b29c>] (dump_backtrace) from [<c020b558>] (show_stack+0x18/0x1c)
[ 305.373963] r7:00000009 r6:600c0193 r5:00000000 r4:c1022668
[ 305.379645] [<c020b540>] (show_stack) from [<c04cd558>] (dump_stack+0x8c/0xa0)
[ 305.386896] [<c04cd4cc>] (dump_stack) from [<c022e3d0>] (__warn+0xec/0x104)
[ 305.393883] r7:00000009 r6:c0bc95bc r5:00000000 r4:ed0cdb68
[ 305.399563] [<c022e2e4>] (__warn) from [<c022e428>] (warn_slowpath_fmt+0x40/0x48)
[ 305.407074] r9:00000006 r8:ec1c8c50 r7:c0bc9428 r6:00000000 r5:c0bc94e8 r4:c0bc958c
[ 305.414849] [<c022e3ec>] (warn_slowpath_fmt) from [<c04fd408>] (l3_interrupt_handler+0x25c/0x36c)
[ 305.423753] r3:ec1c8ac0 r2:c0bc958c
[ 305.427336] r4:80080003
[ 305.429878] [<c04fd1ac>] (l3_interrupt_handler) from [<c027fcf4>] (__handle_irq_event_percpu+0xb4/0x138)
[ 305.439395] r10:c104dd6e r9:ec1cb200 r8:00000017 r7:ed0cdc8c r6:00000000 r5:ec1cb200
[ 305.447253] r4:ec1c8fc0
[ 305.449793] [<c027fc40>] (__handle_irq_event_percpu) from [<c027fd9c>] (handle_irq_event_percpu+0x24/0x60)
[ 305.459483] r10:00000000 r9:ed0cc000 r8:ec006000 r7:00000000 r6:c1008bf4 r5:ec1cb200
[ 305.467341] r4:ec1cb200
[ 305.469882] [<c027fd78>] (handle_irq_event_percpu) from [<c027fe18>] (handle_irq_event+0x40/0x64)
[ 305.478786] r5:ec1cb260 r4:ec1cb200
[ 305.482374] [<c027fdd8>] (handle_irq_event) from [<c02834c8>] (handle_fasteoi_irq+0xc0/0x190)
[ 305.490930] r7:00000000 r6:c1008bf4 r5:ec1cb260 r4:ec1cb200
[ 305.496610] [<c0283408>] (handle_fasteoi_irq) from [<c027ef30>] (generic_handle_irq+0x2c/0x3c)
[ 305.505254] r7:00000000 r6:00000000 r5:00000017 r4:c0e5cde0
[ 305.510933] [<c027ef04>] (generic_handle_irq) from [<c027f4a4>] (__handle_domain_irq+0x64/0xbc)
[ 305.519666] [<c027f440>] (__handle_domain_irq) from [<c02014a0>] (gic_handle_irq+0x40/0x7c)
[ 305.528047] r9:ed0cc000 r8:fa213000 r7:fa212000 r6:ed0cdd48 r5:fa21200c r4:c1003424
[ 305.535820] [<c0201460>] (gic_handle_irq) from [<c020c0f8>] (__irq_svc+0x58/0x8c)
[ 305.543330] Exception stack(0xed0cdd48 to 0xed0cdd90)
[ 305.548399] dd40: ec256e88 600c0013 00000001 0000002d 00000000 00000004
[ 305.556607] dd60: ec256e88 600c0013 0000c350 00000000 00000000 ed0cdda4 ed0cdda8 ed0cdd98
[ 305.564815] dd80: c062f8cc c08d27ec 200c0013 ffffffff
[ 305.569883] r9:ed0cc000 r8:0000c350 r7:ed0cdd7c r6:ffffffff r5:200c0013 r4:c08d27ec
[ 305.577661] [<c08d27c4>] (_raw_spin_unlock_irqrestore) from [<c062f8cc>] (__pm_runtime_idle+0x74/0x88)
[ 305.587006] [<c062f858>] (__pm_runtime_idle) from [<c0229f20>] (omap_dm_timer_disable+0x1c/0x20)
[ 305.595824] r7:ecd6d0a0 r6:0000c350 r5:ecd07b90 r4:ecd07b90
[ 305.601509] [<c0229f04>] (omap_dm_timer_disable) from [<bf020044>] (pwm_omap_dmtimer_start+0x44/0x58 [pwm_omap_dmtimer])
[ 305.612425] [<bf020000>] (pwm_omap_dmtimer_start [pwm_omap_dmtimer]) from [<bf02010c>] (pwm_omap_dmtimer_enable+0x24/0x34 [pwm_omap_dmtimer])
[ 305.625167] r5:ecd07b90 r4:ecd07bb8
[ 305.628758] [<bf0200e8>] (pwm_omap_dmtimer_enable [pwm_omap_dmtimer]) from [<c0514390>] (pwm_apply_state+0x180/0x1bc)
[ 305.639408] r5:ecd6d080 r4:ed0cde38
[ 305.642995] [<c0514210>] (pwm_apply_state) from [<c0514a60>] (enable_store+0x84/0xbc)
[ 305.650854] r9:00000000 r8:00000000 r7:00000002 r6:ecd6d080 r5:ecd671a4 r4:00000000
[ 305.658629] [<c05149dc>] (enable_store) from [<c061ff38>] (dev_attr_store+0x20/0x2c)
[ 305.666399] r7:ed092c80 r6:ed0cdf78 r5:00000002 r4:c05149dc
[ 305.672080] [<c061ff18>] (dev_attr_store) from [<c0397b1c>] (sysfs_kf_write+0x48/0x4c)
[ 305.680025] r5:00000002 r4:c061ff18
[ 305.683611] [<c0397ad4>] (sysfs_kf_write) from [<c03972c8>] (kernfs_fop_write+0xdc/0x1dc)
[ 305.691818] r5:00000002 r4:ecf46280
[ 305.695405] [<c03971ec>] (kernfs_fop_write) from [<c032ee90>] (__vfs_write+0x34/0x120)
[ 305.703351] r10:00000000 r9:00000002 r8:00000000 r7:00000002 r6:ed0cdf78 r5:c03971ec
[ 305.711209] r4:ecaa8e40
[ 305.713750] [<c032ee5c>] (__vfs_write) from [<c032fcdc>] (vfs_write+0xac/0x170)
[ 305.721087] r9:00000002 r8:00000000 r7:ed0cdf78 r6:000d8108 r5:ecaa8e40 r4:00000002
[ 305.728860] [<c032fc30>] (vfs_write) from [<c0330adc>] (SyS_write+0x44/0x98)
[ 305.735933] r9:00000002 r8:000d8108 r7:00000000 r6:00000000 r5:ecaa8e40 r4:ecaa8e40
[ 305.743707] [<c0330a98>] (SyS_write) from [<c0207be0>] (ret_fast_syscall+0x0/0x34)
[ 305.751304] r9:ed0cc000 r8:c0207d84 r7:00000004 r6:b6ef6d58 r5:000d8108 r4:00000002
[ 305.759075] ---[ end trace 82bf4a1b5681e2fe ]---
Will you guys please help me to solve this error.
Thanks,
Simit.