Part Number: AM6548
Tool/software: TI-RTOS
Hi TI Experts,
Please let me confirm the following question.
[Question.1-1]
Can AM65x set the write-back for cache?
[Question.1-2]
Can AM65x support the sharing data between Cortex-A53 and BUS Master IPs like PCIe, EDMA, Ethernet and so on with enabling the cache and write-back mode via SDRAM or on-chip RAM?
[Question1-3]
Can AM65x stay in the cache coherency with above situations??
[Question1-4]
If AM65x support the above case, can the BUS master IPs read the correct data on cache in following case?
1. Write the data to sharing memory region by Cortex-A53
2. This value is on cache (Not reflect on actually memory yet)
3. Access the same memory region by PCIe.
-> At this time, can PCIe read the write back data on cache?
[Question.2-1]
Can AM65x support the sharing data between Cortex-R5 and BUS Master IPs like PCIe, EDMA, Ethernet and so on with enabling the cache and write-back mode via SDRAM or on-chip RAM?
[Question2-2]
Can AM65x stay in the cache coherency with above situations??
[Question2-3]
If AM65x support the above case, can the Bus Master or other cores read the correct data on cache in following case?
1. Write the data to sharing memory region by Cortex-R5
2. This value is on cache (Not reflect on actually memory yet)
3. Access the same memory region by PCIe.
-> At this time, can PCIe read the write back data on cache?
If you have any qeustions, please let me know.
Best regards.
Kaka