This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C5505: java.lang.StackOverflowError in CCStudio.

Part Number: TMS320C5505


Tool/software: Code Composer Studio

Hi TIers,

I am running test programs from BSL (board Support libraries) for TMS320C5505 eZDSP USB stick and I keep getting the below Internal Stack overflow Error when I try to build the project. (Nothing extra other than building the project is running while trying to build the project).

Environment: Win 10+ DSP BIOSv5.42.2.10 + CCSv8

Code Compiler: Project describes/is configured to use C5500 (TI v4.3.2) but is using TIv4.4.1 as this is the only C5500 compiler version installed on the PC.

Any help would be appreciated to resolve this. Please suggest. Thank you. in advance for your time and patience.