This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3352: Dual Ethernet, PHY issue on MAC2



Hi,

I apologize if you have seen this thread already, I tried to split and I am not able to see the thread.

To  address the TI PHY you are seeing we will need some additional information.

Earlier you mentioned that the PHY connection was working. To align with where we need to see the results of a checklist we for on Ethernet triage on the second PHY.

Please follow this checklist and attach the requested information:

Link to Ethernet Checklist

Best Regards,

Schuyler

  • Trying to verify customer saw this thread as being split from original thread.
    e2e.ti.com/.../764624
  • my log and DTS file as follows 

    [ 2.713201] libphy: Fixed MDIO Bus: probed
    [ 2.790327] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000
    [ 2.798031] davinci_mdio 4a101000.mdio: detected phy mask ffffefe0
    [ 2.821942] libphy: 4a101000.mdio: probed
    [ 2.826006] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver unknown
    [ 2.834206] davinci_mdio 4a101000.mdio: phy[1]: device 4a101000.mdio:01, driver unknown
    [ 2.842379] davinci_mdio 4a101000.mdio: phy[2]: device 4a101000.mdio:02, driver unknown
    [ 2.850466] davinci_mdio 4a101000.mdio: phy[3]: device 4a101000.mdio:03, driver unknown
    [ 2.858506] davinci_mdio 4a101000.mdio: phy[4]: device 4a101000.mdio:04, driver unknown
    [ 2.866583] davinci_mdio 4a101000.mdio: phy[12]: device 4a101000.mdio:0c, driver TI DP83867

    [ 2.875940] cpsw 4a100000.ethernet: Detected MACID = fc:69:47:49:ca:26
    [ 2.882686] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4
    [ 2.889074] cpsw 4a100000.ethernet: ALE Table size 1024
    [ 2.894389] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies)
    [ 2.902457] cpsw 4a100000.ethernet: cpsw: Detected MACID = fc:69:47:49:ca:28

    [ 4.953790] net eth0: initializing cpsw version 1.12 (0)

    [ 4.981970] Generic PHY 4a101000.mdio:00: attached PHY driver [Generic PHY] (mii_bus:phy_addr=4a101000.mdio:00, irq=POLL)
    [ 5.005926] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
    [ 9.121595] cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
    [ 9.129795] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
    [ 17.608187] net eth0: initializing cpsw version 1.12 (0)
    [ 17.617262] Generic PHY 4a101000.mdio:00: attached PHY driver [Generic PHY] (mii_bus:phy_addr=4a101000.mdio:00, irq=POLL)
    [ 17.636016] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
    [ 18.641646] cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
    [ 18.649849] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
    [ 29.224252] net eth0: initializing cpsw version 1.12 (0)
    [ 29.233282] Generic PHY 4a101000.mdio:00: attached PHY driver [Generic PHY] (mii_bus:phy_addr=4a101000.mdio:00, irq=POLL)
    [ 29.252134] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
    [ 30.321640] cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
    [ 30.329842] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
    [ 39.853342] net eth0: initializing cpsw version 1.12 (0)
    [ 39.862475] Generic PHY 4a101000.mdio:00: attached PHY driver [Generic PHY] (mii_bus:phy_addr=4a101000.mdio:00, irq=POLL)
    [ 39.881255] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
    [ 40.881639] cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
    [ 40.889839] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
    [ 49.153087] net eth1: initializing cpsw version 1.12 (0)
    [ 49.181165] net eth1: phy "4a101000.mdio:0c" not found on slave 1, err -19
    [ 49.192790] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
    [ 58.485569] random: dropbear: uninitialized urandom read (32 bytes read)

    Please press Enter to activate this console.

    root@AM335X:/#
    root@AM335X:/#
    root@AM335X:/# ifconfig -a
    eth0 Link encap:Ethernet HWaddr FC:69:47:49:CA:26
    inet6 addr: fe80::fe69:47ff:fe49:ca26/64 Scope:Link
    UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
    RX packets:0 errors:0 dropped:0 overruns:0 frame:0
    TX packets:43 errors:0 dropped:0 overruns:0 carrier:0
    collisions:0 txqueuelen:1000
    RX bytes:0 (0.0 B) TX bytes:6154 (6.0 KiB)
    Interrupt:51

    eth1 Link encap:Ethernet HWaddr FC:69:47:49:CA:28
    UP BROADCAST MULTICAST MTU:1500 Metric:1
    RX packets:0 errors:0 dropped:0 overruns:0 frame:0
    TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
    collisions:0 txqueuelen:1000
    RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

    lo Link encap:Local Loopback
    inet addr:127.0.0.1 Mask:255.0.0.0
    inet6 addr: ::1/128 Scope:Host
    UP LOOPBACK RUNNING MTU:65536 Metric:1
    RX packets:0 errors:0 dropped:0 overruns:0 frame:0
    TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
    collisions:0 txqueuelen:1000
    RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

    sit0 Link encap:IPv6-in-IPv4
    NOARP MTU:1480 Metric:1
    RX packets:0 errors:0 dropped:0 overruns:0 frame:0
    TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
    collisions:0 txqueuelen:1000
    RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

    ethtool eth0
    Settings for eth0:
    Supported ports: [ TP AUI BNC MII FIBRE ]
    Supported link modes: 10baseT/Half 10baseT/Full
    100baseT/Half 100baseT/Full
    Supported pause frame use: Symmetric Receive-only
    Supports auto-negotiation: Yes
    Supported FEC modes: Not reported
    Advertised link modes: 10baseT/Half 10baseT/Full
    100baseT/Half 100baseT/Full
    Advertised pause frame use: No
    Advertised auto-negotiation: Yes
    Advertised FEC modes: Not reported
    Link partner advertised link modes: 10baseT/Half 10baseT/Full
    100baseT/Half 100baseT/Full
    Link partner advertised pause frame use: Symmetric
    Link partner advertised auto-negotiation: Yes
    Link partner advertised FEC modes: Not reported
    Speed: 100Mb/s
    Duplex: Full
    Port: MII
    PHYAD: 0
    Transceiver: internal
    Auto-negotiation: on
    Supports Wake-on: d
    Wake-on: d
    Current message level: 0x00000000 (0)

    Link detected: yes

    ethtool eth1
    Settings for eth1:
    Supports Wake-on: d
    Wake-on: d
    Current message level: 0x00000000 (0)

    Link detected: no


    /dts-v1/;

    #include "am33xx.dtsi"
    #include <dt-bindings/interrupt-controller/irq.h>
    #include <dt-bindings/net/ti-dp83867.h>

    / {
    model = "TI AM335x EVM";
    compatible = "ti,am335x-evm", "ti,am33xx";

    memory@80000000 {
    device_type = "memory";
    reg = <0x80000000 0x10000000>; /* 256 MB */
    };

    chosen {
    stdout-path = &uart0;
    };

    leds {
    compatible = "gpio-leds";

    led0 {
    label = "onboard:green:usr1";
    gpios = <&gpio3 20 GPIO_ACTIVE_HIGH>;
    /*default-state = "on";*/
    linux,default-trigger = "heartbeat";
    };
    };

    vbat: fixedregulator0 {
    compatible = "regulator-fixed";
    };

    v3v3c_reg: fixedregulator1 {
    compatible = "regulator-fixed";
    };

    vdd5_reg: fixedregulator2 {
    compatible = "regulator-fixed";
    };

    aliases {
    ethernet0 = &cpsw_emac0;
    ethernet1 = &cpsw_emac1;
    };
    };

    &am33xx_pinmux {
    pinctrl-names = "default";

    spi0_pins: pinmux_spi0_pins {
    pinctrl-single,pins = <
    AM33XX_IOPAD(0x950, PIN_INPUT_PULLUP | MUX_MODE0) /* spi0_sclk.spi0_sclk */
    AM33XX_IOPAD(0x95C, PIN_INPUT_PULLUP | MUX_MODE0) /* spi0_cs0.spi0_cs0 */
    AM33XX_IOPAD(0x960, PIN_INPUT_PULLUP | MUX_MODE0) /* spi0_cs0.spi0_cs0 */
    AM33XX_IOPAD(0x954, PIN_INPUT_PULLUP | MUX_MODE0) /* spi0_d0.spi0_d0 */
    AM33XX_IOPAD(0x958, PIN_INPUT_PULLUP | MUX_MODE0) /* spi0_d1.spi0_d1 */
    >;
    };

    spi1_pins: pinmux_spi1_pins {
    pinctrl-single,pins = <
    AM33XX_IOPAD(0x990, PIN_INPUT_PULLUP | MUX_MODE3) /* mcasp0_aclkx.spi1_clk */
    AM33XX_IOPAD(0x994, PIN_INPUT_PULLUP | MUX_MODE3) /* MOSI - mcasp0_fsx.spi1_d0 */
    AM33XX_IOPAD(0x998, PIN_INPUT_PULLUP | MUX_MODE3) /* MISO - mcasp0_axr0.spi1_d1 */
    AM33XX_IOPAD(0x99c, PIN_INPUT_PULLUP | MUX_MODE3) /* mcasp0_ahclkr.spi1_cs0 */
    AM33XX_IOPAD(0x964, PIN_INPUT_PULLUP | MUX_MODE2) /* ecap0_in_pwm0_out.SPI1_CS1 */
    >;
    };

    i2c0_pins: pinmux_i2c0_pins {
    pinctrl-single,pins = <
    AM33XX_IOPAD(0x988, PIN_INPUT_PULLUP | MUX_MODE0) /* i2c0_sda.i2c0_sda */
    AM33XX_IOPAD(0x98c, PIN_INPUT_PULLUP | MUX_MODE0) /* i2c0_scl.i2c0_scl */
    >;
    };

    i2c1_pins: pinmux_i2c1_pins {
    pinctrl-single,pins = <
    AM33XX_IOPAD(0x96c, PIN_INPUT_PULLUP | MUX_MODE3) /* uart0_rtsn.i2c1_scl */
    AM33XX_IOPAD(0x968, PIN_INPUT_PULLUP | MUX_MODE3) /* uart0_ctsn.i2c1_sda */
    >;
    };

    i2c2_pins: pinmux_i2c2_pins {
    pinctrl-single,pins = <
    AM33XX_IOPAD(0x978, PIN_INPUT_PULLUP | MUX_MODE3) /* uart1_ctsn.i2c2_sda */
    AM33XX_IOPAD(0x97c, PIN_INPUT_PULLUP | MUX_MODE3) /* uart1_rtsn.i2c2_scl */
    >;
    };

    uart0_pins: pinmux_uart0_pins {
    pinctrl-single,pins = <
    AM33XX_IOPAD(0x970, PIN_INPUT_PULLUP | MUX_MODE0) /* uart0_rxd.uart0_rxd */
    AM33XX_IOPAD(0x974, PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* uart0_txd.uart0_txd */
    >;
    };

    uart1_pins: pinmux_uart1_pins {
    pinctrl-single,pins = <
    AM33XX_IOPAD(0x980 , PIN_INPUT_PULLUP | MUX_MODE0) /* uart1_rxd.uart1_rxd */
    AM33XX_IOPAD(0x984 , PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* uart1_txd.uart1_txd */
    >;
    };

    uart2_pins: pinmux_uart2_pins {
    pinctrl-single,pins = <
    AM33XX_IOPAD(0x90C , PIN_INPUT_PULLUP | MUX_MODE6) /* MII1_CRS => UART2_RXD => FPGA_TX_PROC_RX_UART2 */
    AM33XX_IOPAD(0x910 , PIN_OUTPUT_PULLDOWN | MUX_MODE6) /* MII1_RXERR => UART2_RXD => FPGA_TX_PROC_RX_UART2 */
    >;
    };
    uart4_pins: pinmux_uart4_pins {
    pinctrl-single,pins = <
    AM33XX_IOPAD( 0x870, PIN_INPUT_PULLUP | MUX_MODE6) /* GPMC_WAIT_0 => UART4_RXD => FPGA_TX_PROC_RX_UART4 */
    AM33XX_IOPAD( 0x874, PIN_OUTPUT_PULLDOWN | MUX_MODE6) /* GPMC_WPn => UART4_TXD => FPGA_RX_PROC_TX_UART4 */
    >;
    };
    uart5_pins: pinmux_uart5_pins {
    pinctrl-single,pins = <
    AM33XX_IOPAD(0x908 , PIN_INPUT_PULLUP | MUX_MODE3) /* MII1_COL => UART5_RXD => FPGA_TX_PROC_RX_UART5 */
    AM33XX_IOPAD(0x944 , PIN_OUTPUT_PULLDOWN | MUX_MODE3) /* RMII1_REFCLK => UART5_TXD => FPGA_RX_PROC_TX_UART5 */
    >;
    };

    led_pins: pinmux_led_pins {
    pinctrl-single,pins = <
    AM33XX_IOPAD(0x9a8, PIN_INPUT_PULLDOWN | MUX_MODE7) /* mcasp0_axr1.mcasp0_axr1 */
    >;
    };

    mmc1_pins: pinmux_mmc1_pins {
    pinctrl-single,pins = <
    AM33XX_IOPAD(0x8fc, PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_dat0.mmc0_dat0 */
    AM33XX_IOPAD(0x8f8, PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_dat1.mmc0_dat1 */
    AM33XX_IOPAD(0x8f4, PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_dat2.mmc0_dat2 */
    AM33XX_IOPAD(0x8f0, PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_dat3.mmc0_dat3 */
    AM33XX_IOPAD(0x904, PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_cmd.mmc0_cmd */
    AM33XX_IOPAD(0x900, PIN_INPUT_PULLUP | MUX_MODE0) /* mmc0_clk.mmc0_clk */
    >;
    };

    ethernet0_pins: pinmux_ethernet0 {
    pinctrl-single,pins = <
    /* Slave 1 */
    AM33XX_IOPAD(0x92c, PIN_INPUT | MUX_MODE0) /* mii1_txclk.rmii1_tclk */
    AM33XX_IOPAD(0x928, PIN_OUTPUT | MUX_MODE0) /* mii1_txd0.rgmii1_td0 */
    AM33XX_IOPAD(0x924, PIN_OUTPUT | MUX_MODE0) /* mii1_txd1.rgmii1_td1 */
    AM33XX_IOPAD(0x920, PIN_OUTPUT | MUX_MODE0) /* mii1_txd0.rgmii1_td2 */
    AM33XX_IOPAD(0x91c, PIN_OUTPUT | MUX_MODE0) /* mii1_txd1.rgmii1_td3 */
    AM33XX_IOPAD(0x914, PIN_OUTPUT | MUX_MODE0) /* mii1_txen.rgmii1_tctl */

    AM33XX_IOPAD(0x930, PIN_INPUT | MUX_MODE0) /* mii1_rxclk.rmii1_rclk */
    AM33XX_IOPAD(0x940, PIN_INPUT | MUX_MODE0) /* mii1_rxd0.rgmii1_rd0 */
    AM33XX_IOPAD(0x93c, PIN_INPUT | MUX_MODE0) /* mii1_rxd1.rgmii1_rd1 */
    AM33XX_IOPAD(0x938, PIN_INPUT | MUX_MODE0) /* mii1_rxd0.rgmii1_rd2 */
    AM33XX_IOPAD(0x934, PIN_INPUT | MUX_MODE0) /* mii1_rxd1.rgmii1_rd3 */
    AM33XX_IOPAD(0x918, PIN_INPUT | MUX_MODE0) /* mii1_rxdv.rgmii1_rctl */
    >;
    };

    ethernet1_pins: pinmux_ethernet1 {
    pinctrl-single,pins = <
    /* Slave 2 */
    AM33XX_IOPAD(0x858, PIN_OUTPUT | MUX_MODE2) /* gpmc_a6.rgmii2_tclk */
    AM33XX_IOPAD(0x840, PIN_OUTPUT | MUX_MODE2) /* gpmc_a0.rgmii2_tctl */
    AM33XX_IOPAD(0x854, PIN_OUTPUT | MUX_MODE2) /* gpmc_a5.rgmii2_td0 */
    AM33XX_IOPAD(0x850, PIN_OUTPUT | MUX_MODE2) /* gpmc_a4.rgmii2_td1 */
    AM33XX_IOPAD(0x84c, PIN_OUTPUT | MUX_MODE2) /* gpmc_a3.rgmii2_td2 */
    AM33XX_IOPAD(0x848, PIN_OUTPUT | MUX_MODE2) /* gpmc_a2.rgmii2_td3 */
    AM33XX_IOPAD(0x85c, PIN_INPUT | MUX_MODE2) /* gpmc_a7.rgmii2_rclk */
    AM33XX_IOPAD(0x844, PIN_INPUT | MUX_MODE2) /* gpmc_a1.rgmii2_rtcl */
    AM33XX_IOPAD(0x86c, PIN_INPUT | MUX_MODE2) /* gpmc_a11.rgmii2_rd0 */
    AM33XX_IOPAD(0x868, PIN_INPUT | MUX_MODE2) /* gpmc_a10.rgmii2_rd1 */
    AM33XX_IOPAD(0x864, PIN_INPUT | MUX_MODE2) /* gpmc_a9.rgmii2_rd2 */
    AM33XX_IOPAD(0x860, PIN_INPUT | MUX_MODE2) /* gpmc_a8.rgmii2_rd3 */
    >;
    };

    usb1_drvvbus: usb1_drvvbus {
    pinctrl-single,pins = <
    AM33XX_IOPAD(0xa34, PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* usb1_drvvbus.usb1_drvvbus */
    >;
    };

    mdio_pins: pinmyx_mdio {
    pinctrl-single,pins = <
    /* MDIO */
    AM33XX_IOPAD(0x948, PIN_INPUT_PULLUP | SLEWCTRL_FAST | MUX_MODE0) /* mdio_data.mdio_data */
    AM33XX_IOPAD(0x94c, PIN_OUTPUT_PULLUP | MUX_MODE0) /* mdio_clk.mdio_clk */
    >;
    };

    misc_gpio_pins: pinmux_misc_gpio_pins {
    pinctrl-single,pins = <
    //?AM33XX_IOPAD(0x9a0, PIN_OUTPUT_PULLUP | MUX_MODE7) /* mcasp0_aclkr.gpio3_18 */
    //?AM33XX_IOPAD(0x9a4, PIN_INPUT_PULLDOWN | MUX_MODE7) /* mcasp0_fsr.gpio3_19 */
    //?AM33XX_IOPAD(0x9ac, PIN_INPUT_PULLDOWN | MUX_MODE7) /* mcasp0_ahcklx.gpio3_21 */

    AM33XX_IOPAD(0x8d0, PIN_OUTPUT | MUX_MODE7) /* lcd_data12.gpio0_8 - PROC_I2C_CTRL_V1V8_S */
    AM33XX_IOPAD(0x8d4, PIN_OUTPUT | MUX_MODE7) /* lcd_data13.gpio0_9 - PROC_I2C_CTRL_V1V0 */
    AM33XX_IOPAD(0x8d8, PIN_OUTPUT | MUX_MODE7) /* lcd_data14.gpio0_10 - PROC_I2C_CTRL_V0P95 */

    AM33XX_IOPAD(0x820, PIN_OUTPUT | MUX_MODE7) /* gpmc_ad8.gpi0_22 */
    AM33XX_IOPAD(0x824, PIN_OUTPUT | MUX_MODE7) /* gpmc_ad9.gpio0_23 */
    AM33XX_IOPAD(0x828, PIN_OUTPUT | MUX_MODE7) /* gpmc_ad10.gpio0_26 */
    AM33XX_IOPAD(0x82c, PIN_OUTPUT | MUX_MODE7) /* gpmc_ad11.gpio0_27 */

    AM33XX_IOPAD(0x800, PIN_OUTPUT | MUX_MODE7) /* gpmc_ad0.gpio1_0 */
    AM33XX_IOPAD(0x804, PIN_OUTPUT | MUX_MODE7) /* gpmc_ad1.gpio1_1 */
    AM33XX_IOPAD(0x808, PIN_OUTPUT | MUX_MODE7) /* gpmc_ad2.gpio1_2 */
    AM33XX_IOPAD(0x80c, PIN_OUTPUT | MUX_MODE7) /* gpmc_ad3.gpio1_3 */
    AM33XX_IOPAD(0x810, PIN_OUTPUT | MUX_MODE7) /* gpmc_ad4.gpio1_4 */
    AM33XX_IOPAD(0x814, PIN_OUTPUT | MUX_MODE7) /* gpmc_ad5.gpio1_5 */
    AM33XX_IOPAD(0x818, PIN_OUTPUT | MUX_MODE7) /* gpmc_ad6.gpio1_6 */
    AM33XX_IOPAD(0x81c, PIN_OUTPUT | MUX_MODE7) /* gpmc_ad7.gpio1_7 */
    AM33XX_IOPAD(0x830, PIN_OUTPUT | MUX_MODE7) /* gpmc_ad12.gpio1_12 */
    AM33XX_IOPAD(0x834, PIN_OUTPUT | MUX_MODE7) /* gpmc_ad13.gpio1_13 */
    AM33XX_IOPAD(0x838, PIN_OUTPUT | MUX_MODE7) /* gpmc_ad14.gpio1_14 */
    AM33XX_IOPAD(0x83c, PIN_OUTPUT | MUX_MODE7) /* gpmc_ad15.gpio1_15 */
    AM33XX_IOPAD(0x878, PIN_OUTPUT | MUX_MODE7) /* gpmc_ben1.gpio1_28 */
    AM33XX_IOPAD(0x87c, PIN_OUTPUT | MUX_MODE7) /* gpmc_csn0.gpio1_29 */
    AM33XX_IOPAD(0x880, PIN_OUTPUT | MUX_MODE7) /* gpmc_csn1.gpio1_30 */
    AM33XX_IOPAD(0x884, PIN_OUTPUT | MUX_MODE7) /* gpmc_csn2.gpio1_31 */

    AM33XX_IOPAD(0x888, PIN_OUTPUT | MUX_MODE7) /* gpmc_csn3.gpio2_0 */
    AM33XX_IOPAD(0x88c, PIN_OUTPUT | MUX_MODE7) /* gpmc_clk.gpio2_1 */
    AM33XX_IOPAD(0x890, PIN_OUTPUT | MUX_MODE7) /* gpmc_advn_ale.gpio2_2 */
    AM33XX_IOPAD(0x894, PIN_OUTPUT | MUX_MODE7) /* gpmc_oen_ren.gpio2_3 */
    AM33XX_IOPAD(0x898, PIN_OUTPUT | MUX_MODE7) /* gpmc_wen.gpio2_4 */
    AM33XX_IOPAD(0x89c, PIN_OUTPUT | MUX_MODE7) /* gpmc_ben0_cle.gpio2_5 */
    AM33XX_IOPAD(0x8a0, PIN_OUTPUT | MUX_MODE7) /* lcd_data0.gpio2_6 */
    AM33XX_IOPAD(0x8a8, PIN_OUTPUT | MUX_MODE7) /* lcd_data2.gpio2_8 */
    AM33XX_IOPAD(0x8b4, PIN_OUTPUT | MUX_MODE7) /* lcd_data5.gpio2_11 */
    AM33XX_IOPAD(0x8c8, PIN_OUTPUT | MUX_MODE7) /* lcd_data10.gpio2_16 */
    AM33XX_IOPAD(0x8cc, PIN_OUTPUT | MUX_MODE7) /* lcd_data11.gpio2_17 */
    AM33XX_IOPAD(0x8e0, PIN_OUTPUT | MUX_MODE7) /* lcd_vsync.gpio2_22 */
    AM33XX_IOPAD(0x8e4, PIN_OUTPUT | MUX_MODE7) /* lcd_hsync.gpio2_23 */
    AM33XX_IOPAD(0x8e8, PIN_OUTPUT | MUX_MODE7) /* lcd_pclk.gpio2_24 */
    AM33XX_IOPAD(0x8ec, PIN_OUTPUT | MUX_MODE7) /* lcd_ac_bias_en.gpio2_25 */

    AM33XX_IOPAD(0x9a8, PIN_INPUT_PULLDOWN | MUX_MODE7) /* mcasp0_axr1.gpio3_20 - green LED*/


    >;
    };
    };

    /*-----------------------------------------------------------------------------*/

    &spi0 {
    status = "okay";
    pinctrl-names = "default";
    pinctrl-0 = <&spi0_pins>;

    /*spi0_0: spi0_0@0 {
    #address-cells = <1>;
    #size-cells = <0>;
    compatible = "linux,spidev";
    reg = <0>;
    spi-max-frequency = <16000000>;
    spi-cpha;
    spi-cpol;
    spi-cs-low;
    };*/

    /* from u-boot.
    * Default to using SPI for environment, etc.
    * 0x000000 - 0x020000 : SPL (128KiB)
    * 0x020000 - 0x0A0000 : U-Boot (512KiB)
    * 0x0A0000 - 0x0BFFFF : First copy of U-Boot Environment (128KiB)
    * 0x0C0000 - 0x0DFFFF : Second copy of U-Boot Environment (128KiB)
    * 0x0E0000 - 0x442000 : Linux Kernel
    * 0x442000 - 0x800000 : Userland
    */

    nor_flash: n25q128a11@0 {
    #address-cells = <1>;
    #size-cells = <1>;
    compatible = "Micron,n25q128a11";
    spi-max-frequency = <16000000>;
    m25p,fast-read;
    reg = <0>;
    partition@0 {
    label = "u-boot-spl";
    reg = <0x0 0x20000>;
    read-only;
    };
    partition@1 {
    label = "u-boot";
    reg = <0x20000 0x80000>;
    read-only;
    };
    partition@2 {
    label = "nvram0";
    reg = <0xa0000 0x20000>;
    read-only;
    };
    partition@3 {
    label = "nvram1";
    reg = <0xc0000 0x20000>;
    read-only;
    };
    };

    spi0_1: spi0_1@1 {
    #address-cells = <1>;
    #size-cells = <0>;
    compatible = "spidev";
    reg = <1>;
    spi-max-frequency = <16000000>;
    };
    };

    &spi1 {
    status = "okay";
    pinctrl-names = "default";
    pinctrl-0 = <&spi1_pins>;
    ti,pindir-d0-out-d1-in = <1>;
    spi1_0: spi1_0@0 {
    #address-cells = <1>;
    #size-cells = <0>;
    compatible = "spidev";
    reg = <0>;
    spi-max-frequency = <16000000>;
    };

    spi1_1: spi1_1@1 {
    #address-cells = <1>;
    #size-cells = <0>;
    compatible = "spidev";
    reg = <1>;
    spi-max-frequency = <16000000>;
    };
    };

    &misc_gpio_pins {
    pinctrl-names = "default";
    pinctrl-0 = <&misc_gpio_pins>;
    lcd-reset = <&gpio1 9 GPIO_ACTIVE_LOW>;
    lcd-on = <&gpio1 9 GPIO_ACTIVE_HIGH>;
    fpga_to_proc_intr = <&gpio3 21 GPIO_ACTIVE_HIGH>;
    gpio_expander_reset = <&gpio3 18 GPIO_ACTIVE_HIGH>;
    gpio_expander_interrupt = <&gpio3 19 GPIO_ACTIVE_HIGH>;
    status = "okay";
    };

    &uart0 {
    pinctrl-names = "default";
    pinctrl-0 = <&uart0_pins>;
    pinctrl-1 = <&led_pins>;
    led-on = <&gpio3 20 GPIO_ACTIVE_HIGH>;
    led-off = <&gpio3 20 GPIO_ACTIVE_LOW>;
    status = "okay";
    };

    &uart1 {
    pinctrl-names = "default";
    pinctrl-0 = <&uart1_pins>;
    status = "okay";
    };

    &uart2 {
    pinctrl-names = "default";
    pinctrl-0 = <&uart2_pins>;
    status = "okay";
    };

    &uart4 {
    pinctrl-names = "default";
    pinctrl-0 = <&uart4_pins>;
    status = "okay";
    };

    &uart5 {
    pinctrl-names = "default";
    pinctrl-0 = <&uart5_pins>;
    status = "okay";
    };


    &i2c0 {
    pinctrl-names = "default";
    pinctrl-0 = <&i2c0_pins>;
    status = "okay";
    clock-frequency = <100000>;
    };

    &i2c1 {
    pinctrl-names = "default";
    pinctrl-0 = <&i2c1_pins>;
    status = "okay";
    clock-frequency = <100000>;
    };

    &i2c2 {
    pinctrl-names = "default";
    pinctrl-0 = <&i2c2_pins>;
    status = "okay";
    clock-frequency = <100000>;
    };

    &mac {
    slaves = <2>;
    pinctrl-names = "default";
    pinctrl-0 = <&ethernet0_pins &ethernet1_pins>;
    status = "okay";
    dual_emac=<1>;
    };

    &phy_sel {
    rmii-clock-ext = <1>;
    };

    &davinci_mdio {
    pinctrl-names = "default";
    pinctrl-0 = <&mdio_pins>;
    status = "okay";
    };

    &cpsw_emac0 {
    phy_id = <&davinci_mdio>, <0>;
    phy-mode = "mii";
    dual_emac_res_vlan = <1>;
    status = "okay";
    };

    &cpsw_emac1 {
    phy_id = <&davinci_mdio>, <0xc>;
    phy-mode = "rgmii-txid";
    dual_emac_res_vlan = <2>;
    status = "okay";
    };

    &mmc1 {
    status = "okay";
    bus-width = <4>;
    pinctrl-names = "default";
    pinctrl-0 = <&mmc1_pins>;
    max-frequency = <26000000>;
    ti,non-removable;
    vmmc-supply = <&v3v3c_reg>;
    };

    /* Power */
    &vbat {
    regulator-name = "vbat";
    regulator-min-microvolt = <5000000>;
    regulator-max-microvolt = <5000000>;
    };

    &v3v3c_reg {
    regulator-name = "v3v3c_reg";
    regulator-min-microvolt = <3300000>;
    regulator-max-microvolt = <3300000>;
    vin-supply = <&vbat>;
    };

    &vdd5_reg {
    regulator-name = "vdd5_reg";
    regulator-min-microvolt = <5000000>;
    regulator-max-microvolt = <5000000>;
    vin-supply = <&vbat>;
    };

    &rtc {
    clocks = <&clk_32768_ck>, <&clkdiv32k_ick>;
    clock-names = "ext-clk", "int-clk";
    };

    &wkup_m3_ipc {
    ti,scale-data-fw = "am335x-evm-scale-data.bin";
    };

    &pruss_soc_bus {
    status = "okay";

    pruss: pruss@0 {
    status = "okay";
    };
    };

    &sgx {
    status = "okay";
    };

    &tscadc {
    status = "okay";
    };

    &sham {
    status = "okay";
    };

    &aes {
    status = "okay";
    };

    &elm {
    status = "okay";
    };

    &epwmss0 {
    status = "okay";
    };


    &mcasp1 {
    status = "okay";
    };

    &usb {
    status = "okay";
    };

    &usb_ctrl_mod {
    status = "okay";
    };

    &usb0_phy {
    status = "okay";
    };

    &usb1_phy {
    status = "okay";
    };

    &usb0 {
    status = "okay";
    };

    &usb1 {
    pinctrl-names = "default";
    pinctrl-0 = <&usb1_drvvbus>;

    status = "okay";
    dr_mode = "host";
    };

    &gpmc {
    status = "okay";
    };

  • Hi,
    First I need to say that we may have to start another thread due to I split the thread wrong.

    In the meantime the ethtool results are showing that there is no link which matches what these lines are saying in the boot output.

    ethtool eth1
    .....
    Link detected: no

    [ 49.181165] net eth1: phy "4a101000.mdio:0c" not found on slave 1, err -19

    Currently it looks like the PHY is not being detected as part of the MDIO polling process . I would recommend looking at the resistor strapping to make sure the ID portion is configured as intended. I am assuming that the PHY is not showing up as a different address in the Boot Log? Additionally the PHY may not be coming out of reset properly.

    Best Regards,
    Schuyler
  • Hi,
    I have not heard back from you in a while so I going to assume that you were able to move past your issue. I am going to close the thread for now and mark as resolved. If this is not the case you can still respond to this thread or create a new one based on this thread.
    Best Regards,
    Schuyler