Part Number: 66AK2H12
Tool/software: Linux
Hi,
I am trying to build Linux using Yocto following the guide at http://processors.wiki.ti.com/index.php/Processor_SDK_Building_The_SDK
I am getting what I have pasted below. Also, what is not visible in that console output is that after running bitbake, there exists a directory named ${OEBASE} in the directory where I run bitbake. I am quite sure that's a sign of variable expansion not working somewhere, but I am not sure if what bitbake is complaining about is the same problem.
Any ideas what to do?
/yocto/tisdk/build$ MACHINE=k2hk-evm bitbake -p -P arago-core-tisdk-image
NOTE: Your conf/bblayers.conf has been automatically updated.
NOTE: Your conf/bblayers.conf has been automatically updated.
WARNING: Can't get the filesystem id of: ${OEBASE}/build/arago-tmp-external-linaro-toolchain
WARNING: /yocto/tisdk/sources/meta-ti/recipes-ti/devtools/ti-cgt6x_8.2.2.bb: ti-cgt6x-8.2.2 ONLY supports hardfp mode for now | ETA: 0:00:57
WARNING: /yocto/tisdk/sources/meta-ti/recipes-kernel/linux/linux-ti-staging_4.9.bb: Exception during build_dependencies for PKG_kernel-base | ETA: 0:00:55
WARNING: /yocto/tisdk/sources/meta-ti/recipes-kernel/linux/linux-ti-staging_4.9.bb: Error during finalise of /yocto/tisdk/sources/meta-ti/recipes-kernel/linux/linux-ti-staging_4.9.bb
ERROR: ExpansionError during parsing /yocto/tisdk/sources/meta-ti/recipes-kernel/linux/linux-ti-staging_4.9.bb
Traceback (most recent call last):
bb.data_smart.ExpansionError: Failure expanding variable PKG_kernel-base, expression was kernel-${@legitimize_package_name('${@get_kernelversion_headers('${OEBASE}/build/arago-tmp-external-linaro-toolchain/work/arago-linux-gnueabi/linux-ti-staging/4.9.59+gitAUTOINC+a75d8e9305-a.arago5.tisdk16/build')}')} which triggered exception SyntaxError: invalid syntax (PKG_kernel-base, line 1)
WARNING: /yocto/tisdk/sources/meta-ti/recipes-kernel/linux/linux-ti-staging-systest_4.9.bb: Exception during build_dependencies for PKG_kernel-base
WARNING: /yocto/tisdk/sources/meta-ti/recipes-kernel/linux/linux-ti-staging-systest_4.9.bb: Error during finalise of /yocto/tisdk/sources/meta-ti/recipes-kernel/linux/linux-ti-staging-systest_4.9.bb
WARNING: /yocto/tisdk/sources/meta-ti/recipes-graphics/libgles/ti-sgx-ddk-um_1.14.3699939.bb: ti-sgx-ddk-um-1.14.3699939 ONLY supports hardfp mode for now
WARNING: /yocto/tisdk/sources/meta-ti/recipes-kernel/linux/linux-ti-staging-rt_4.9.bb: Exception during build_dependencies for PKG_kernel-base
WARNING: /yocto/tisdk/sources/meta-ti/recipes-kernel/linux/linux-ti-staging-rt_4.9.bb: Error during finalise of /yocto/tisdk/sources/meta-ti/recipes-kernel/linux/linux-ti-staging-rt_4.9.bb
Processed parsing statistics saved to profile-parse.log.processed
Summary: There were 9 WARNING messages shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.
Raw profiling information saved to profile.log and processed statistics to profile.log.processed
This is what I did to get the SDK:
/yocto$ git clone git://arago-project.org/git/projects/oe-layersetup.git tisdk
/yocto/tisdk$ ./oe-layertool-setup.sh -f configs/processor-sdk/processor-sdk-04.02.00.09-config.txt