Part Number: AM3359
Tool/software: Linux
Hello all,
We are using a custom board based on am3359 icev2.We have an SPI flash connected to spi1.We enabled all the drivers and modified u-boot dts file accordingly.But our spi flash is not being detected by sf probe.But it is able to detect the default spi flash which comes with evm connected to spi0.I have attached the dts file.SPI flash part number :MT25QL256ABA1EW9-0SIT
Boot log:
U-Boot SPL 2018.01-00444-g96cdbefd5c-dirty (Jan 31 2019 - 16:06:34)
Trying to boot from NAND
U-Boot 2018.01-00444-g96cdbefd5c-dirty (Feb 11 2019 - 13:00:46 +0530)
CPU : AM335X-GP rev 2.1
Model: TI AM335x EVM
DRAM: 512 MiB
NAND: 256 MiB
MMC: OMAP SD/MMC: 0
Net: Could not get PHY for cpsw: addr 0
cpsw, usb_ether
Hit any key to stop autoboot: 0
=> sf probe
SF: Detected w25q64cv with page size 256 Bytes, erase size 4 KiB, total 8 MiB
=> sf probe 1
SF: unrecognized JEDEC id bytes: ff, ff, ff
Failed to initialize SPI flash at 0:1
=> sf probe 1
SF: unrecognized JEDEC id bytes: ff, ff, ff
Failed to initialize SPI flash at 0:1
dts file:
/*
* Copyright (C) 2016 Texas Instruments Incorporated - http://www.ti.com/
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*/
/*
* AM335x ICE V2 board
* http://www.ti.com/tool/tmdsice3359
*/
/dts-v1/;
#include "am33xx.dtsi"
#include <dt-bindings/interrupt-controller/irq.h>
#include <dt-bindings/net/ti-dp83867.h>
/ {
model = "TI AM3359 ICE-V2";
compatible = "ti,am3359-icev2", "ti,am33xx";
memory@80000000 {
device_type = "memory";
reg = <0x80000000 0x10000000>; /* 256 MB */
};
chosen {
stdout-path = &uart0;
};
vbat: fixedregulator0 {
compatible = "regulator-fixed";
regulator-name = "vbat";
regulator-min-microvolt = <5000000>;
regulator-max-microvolt = <5000000>;
regulator-boot-on;
};
vtt_fixed: fixedregulator1 {
compatible = "regulator-fixed";
regulator-name = "vtt";
regulator-min-microvolt = <1500000>;
regulator-max-microvolt = <1500000>;
gpio = <&gpio0 18 GPIO_ACTIVE_HIGH>;
regulator-always-on;
regulator-boot-on;
enable-active-high;
};
leds-iio {
status = "disabled";
compatible = "gpio-leds";
led-out0 {
label = "out0";
gpios = <&tpic2810 0 GPIO_ACTIVE_HIGH>;
default-state = "off";
};
led-out1 {
label = "out1";
gpios = <&tpic2810 1 GPIO_ACTIVE_HIGH>;
default-state = "off";
};
led-out2 {
label = "out2";
gpios = <&tpic2810 2 GPIO_ACTIVE_HIGH>;
default-state = "off";
};
led-out3 {
label = "out3";
gpios = <&tpic2810 3 GPIO_ACTIVE_HIGH>;
default-state = "off";
};
led-out4 {
label = "out4";
gpios = <&tpic2810 4 GPIO_ACTIVE_HIGH>;
default-state = "off";
};
led-out5 {
label = "out5";
gpios = <&tpic2810 5 GPIO_ACTIVE_HIGH>;
default-state = "off";
};
led-out6 {
label = "out6";
gpios = <&tpic2810 6 GPIO_ACTIVE_HIGH>;
default-state = "off";
};
led-out7 {
label = "out7";
gpios = <&tpic2810 7 GPIO_ACTIVE_HIGH>;
default-state = "off";
};
};
/* Tricolor status LEDs */
leds1 {
compatible = "gpio-leds";
pinctrl-names = "default";
pinctrl-0 = <&user_leds>;
led0 {
label = "status0:red:cpu0";
gpios = <&gpio0 17 GPIO_ACTIVE_HIGH>;
default-state = "off";
linux,default-trigger = "cpu0";
};
led1 {
label = "status0:green:usr";
gpios = <&gpio0 16 GPIO_ACTIVE_HIGH>;
default-state = "off";
};
led2 {
label = "status0:yellow:usr";
gpios = <&gpio3 9 GPIO_ACTIVE_HIGH>;
default-state = "off";
};
led3 {
label = "status1:red:mmc0";
gpios = <&gpio1 30 GPIO_ACTIVE_HIGH>;
default-state = "off";
linux,default-trigger = "mmc0";
};
led4 {
label = "status1:green:usr";
gpios = <&gpio0 20 GPIO_ACTIVE_HIGH>;
default-state = "off";
};
led5 {
label = "status1:yellow:usr";
gpios = <&gpio0 19 GPIO_ACTIVE_HIGH>;
default-state = "off";
};
};
gpio-decoder {
compatible = "gpio-decoder";
gpios = <&pca9536 3 GPIO_ACTIVE_HIGH>,
<&pca9536 2 GPIO_ACTIVE_HIGH>,
<&pca9536 1 GPIO_ACTIVE_HIGH>,
<&pca9536 0 GPIO_ACTIVE_HIGH>;
linux,axis = <0>; /* ABS_X */
decoder-max-value = <9>;
};
/* Dual mac ethernet application node on icss */
/*pruss_eth {
compatible = "ti,am3359-prueth";
pruss = <&pruss>;
sram = <&ocmcram>;
interrupt-parent = <&pruss_intc>;
status = "disabled";
pinctrl-0 = <&pruss_eth_default>;
pinctrl-names = "default";
pruss_emac0: ethernet-mii0 {
phy-handle = <&pruss_eth0_phy>;
phy-mode = "mii";
interrupts = <20>, <22>;
interrupt-names = "rx", "tx";
/* Filled in by bootloader
local-mac-address = [00 00 00 00 00 00];
};
pruss_emac1: ethernet-mii1 {
phy-handle = <&pruss_eth1_phy>;
phy-mode = "mii";
interrupts = <21>, <23>;
interrupt-names = "rx", "tx";
/* Filled in by bootloader
local-mac-address = [00 00 00 00 00 00];
};
};*/
};
&am33xx_pinmux {
user_leds: user_leds {
pinctrl-single,pins = <
AM33XX_IOPAD(0x91c, PIN_OUTPUT | MUX_MODE7) /* (J18) gmii1_txd3.gpio0[16] */
AM33XX_IOPAD(0x920, PIN_OUTPUT | MUX_MODE7) /* (K15) gmii1_txd2.gpio0[17] */
AM33XX_IOPAD(0x9b0, PIN_OUTPUT | MUX_MODE7) /* (A15) xdma_event_intr0.gpio0[19] */
AM33XX_IOPAD(0x9b4, PIN_OUTPUT | MUX_MODE7) /* (D14) xdma_event_intr1.gpio0[20] */
AM33XX_IOPAD(0x880, PIN_OUTPUT | MUX_MODE7) /* (U9) gpmc_csn1.gpio1[30] */
AM33XX_IOPAD(0x92c, PIN_OUTPUT | MUX_MODE7) /* (K18) gmii1_txclk.gpio3[9] */
>;
};
mmc0_pins_default: mmc0_pins_default {
pinctrl-single,pins = <
AM33XX_IOPAD(0x8f0, PIN_INPUT_PULLUP | MUX_MODE0) /* (F17) mmc0_dat3.mmc0_dat3 */
AM33XX_IOPAD(0x8f4, PIN_INPUT_PULLUP | MUX_MODE0) /* (F18) mmc0_dat2.mmc0_dat2 */
AM33XX_IOPAD(0x8f8, PIN_INPUT_PULLUP | MUX_MODE0) /* (G15) mmc0_dat1.mmc0_dat1 */
AM33XX_IOPAD(0x8fc, PIN_INPUT_PULLUP | MUX_MODE0) /* (G16) mmc0_dat0.mmc0_dat0 */
AM33XX_IOPAD(0x900, PIN_INPUT_PULLUP | MUX_MODE0) /* (G17) mmc0_clk.mmc0_clk */
AM33XX_IOPAD(0x904, PIN_INPUT_PULLUP | MUX_MODE0) /* (G18) mmc0_cmd.mmc0_cmd */
>;
};
i2c0_pins_default: i2c0_pins_default {
pinctrl-single,pins = <
AM33XX_IOPAD(0x988, PIN_INPUT | MUX_MODE0) /* (C17) I2C0_SDA.I2C0_SDA */
AM33XX_IOPAD(0x98c, PIN_INPUT | MUX_MODE0) /* (C16) I2C0_SCL.I2C0_SCL */
>;
};
spi0_pins_default: spi0_pins_default {
pinctrl-single,pins = <
AM33XX_IOPAD(0x950, PIN_INPUT_PULLUP | MUX_MODE0) /* (A17) spi0_sclk.spi0_sclk */
AM33XX_IOPAD(0x954, PIN_INPUT_PULLUP | MUX_MODE0) /* (B17) spi0_d0.spi0_d0 */
AM33XX_IOPAD(0x958, PIN_INPUT_PULLUP | MUX_MODE0) /* (B16) spi0_d1.spi0_d1 */
AM33XX_IOPAD(0x95c, PIN_INPUT_PULLUP | MUX_MODE0) /* (A16) spi0_cs0.spi0_cs0 */
AM33XX_IOPAD(0x960, PIN_INPUT_PULLUP | MUX_MODE0) /* (C15) spi0_cs1.spi0_cs1 */
AM33XX_IOPAD(0x9a0, PIN_INPUT_PULLUP | MUX_MODE7) /* (B12) mcasp0_aclkr.gpio3[18] */
>;
};
spi1_pins_default: spi1_pins_default {
pinctrl-single,pins = <
AM33XX_IOPAD(0x990, PIN_INPUT_PULLUP | MUX_MODE3) /* (A13) mcasp0_aclkx.spi1_sclk */
AM33XX_IOPAD(0x994, PIN_INPUT_PULLUP | MUX_MODE3) /* (B13) mcasp0_fsx.spi1_d0 */
AM33XX_IOPAD(0x998, PIN_INPUT_PULLUP | MUX_MODE3) /* (D12) mcasp0_axr0.spi1_d1 */
AM33XX_IOPAD(0x99c, PIN_INPUT_PULLUP | MUX_MODE3) /* (C12) mcasp0_ahclkr.spi1_cs0 */
>;
};
uart3_pins_default: uart3_pins_default {
pinctrl-single,pins = <
AM33XX_IOPAD(0x934, PIN_INPUT_PULLUP | MUX_MODE1) /* (L17) gmii1_rxd3.uart3_rxd */
AM33XX_IOPAD(0x938, PIN_OUTPUT_PULLUP | MUX_MODE1) /* (L16) gmii1_rxd2.uart3_txd */
>;
};
uart4_pins_default: uart4_pins_default {
pinctrl-single,pins = <
AM33XX_IOPAD(0x870, PIN_INPUT_PULLUP | MUX_MODE6) /* (T17) gpmc_wait0.uart4_rxd */
AM33XX_IOPAD(0x874, PIN_OUTPUT_PULLUP | MUX_MODE6) /* (U17) gpmc_wpn.uart4_txd */
>;
};
cpsw_default: cpsw_default {
pinctrl-single,pins = <
/* Slave 1 */
AM33XX_IOPAD(0x914, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txen.rgmii1_tctl */
AM33XX_IOPAD(0x918, PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxdv.rgmii1_rctl */
AM33XX_IOPAD(0x91c, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd3.rgmii1_td3 */
AM33XX_IOPAD(0x920, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd2.rgmii1_td2 */
AM33XX_IOPAD(0x924, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd1.rgmii1_td1 */
AM33XX_IOPAD(0x928, PIN_OUTPUT_PULLDOWN | MUX_MODE2)/* mii1_txd0.rgmii1_td0 */
AM33XX_IOPAD(0x92c, PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txclk.rgmii1_tclk */
AM33XX_IOPAD(0x930, PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxclk.rgmii1_rclk */
AM33XX_IOPAD(0x934, PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd3.rgmii1_rd3 */
AM33XX_IOPAD(0x938, PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd2.rgmii1_rd2 */
AM33XX_IOPAD(0x93c, PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd1.rgmii1_rd1 */
AM33XX_IOPAD(0x940, PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd0.rgmii1_rd0 */
AM33XX_IOPAD(0xA34, PIN_OUTPUT_PULLUP | MUX_MODE7) /* (F15) USB1_DRVVBUS.gpio3[13] */
>;
};
cpsw_sleep: cpsw_sleep {
pinctrl-single,pins = <
AM33XX_IOPAD(0x914, (PIN_INPUT_PULLDOWN | MUX_MODE7) ) /* (J16) gmii1_txen.rgmii1_tctl */
AM33XX_IOPAD(0x918, (PIN_INPUT_PULLDOWN | MUX_MODE7) ) /* (J17) gmii1_rxdv.rgmii1_rctl */
AM33XX_IOPAD(0x92c, (PIN_INPUT_PULLDOWN | MUX_MODE7) ) /* (K18) gmii1_txclk.rgmii1_tclk */
AM33XX_IOPAD(0x930, (PIN_INPUT_PULLDOWN | MUX_MODE7)) /* (L18) gmii1_rxclk.rgmii1_rclk */
AM33XX_IOPAD(0x928, (PIN_INPUT_PULLDOWN | MUX_MODE7) ) /* (K17) gmii1_txd0.rgmii1_td0 */
AM33XX_IOPAD(0x924, (PIN_INPUT_PULLDOWN | MUX_MODE7) ) /* (K16) gmii1_txd1.rgmii1_td1 */
AM33XX_IOPAD(0x920, (PIN_INPUT_PULLDOWN | MUX_MODE7) ) /* (K15) gmii1_txd2.rgmii1_td2 */
AM33XX_IOPAD(0x91c, (PIN_INPUT_PULLDOWN | MUX_MODE7) ) /* (J18) gmii1_txd3.rgmii1_td3 */
AM33XX_IOPAD(0x940, (PIN_INPUT_PULLDOWN | MUX_MODE7) ) /* (M16) gmii1_rxd0.rgmii1_rd0 */
AM33XX_IOPAD(0x93c, (PIN_INPUT_PULLDOWN | MUX_MODE7) ) /* (L15) gmii1_rxd1.rgmii1_rd1 */
AM33XX_IOPAD(0x938, (PIN_INPUT_PULLDOWN | MUX_MODE7) ) /* (L16) gmii1_rxd2.rgmii1_rd2 */
AM33XX_IOPAD(0x934, (PIN_INPUT_PULLDOWN | MUX_MODE7) ) /* (L17) gmii1_rxd3.rgmii1_rd3 */
AM33XX_IOPAD(0xA34, PIN_OUTPUT_PULLDOWN | MUX_MODE7)
>;
};
davinci_mdio_default: davinci_mdio_default {
pinctrl-single,pins = <
/* MDIO */
AM33XX_IOPAD(0x948, (PIN_INPUT_PULLUP | SLEWCTRL_FAST | MUX_MODE0)) /* mdio_data.mdio_data */
AM33XX_IOPAD(0x94c, (PIN_OUTPUT_PULLUP | MUX_MODE0)) /* mdio_clk.mdio_clk */
>;
};
davinci_mdio_sleep: davinci_mdio_sleep {
pinctrl-single,pins = <
/* MDIO reset value */
AM33XX_IOPAD(0x948, (PIN_INPUT_PULLDOWN | MUX_MODE7))
AM33XX_IOPAD(0x94c, (PIN_INPUT_PULLDOWN | MUX_MODE7))
>;
};
};
&i2c0 {
pinctrl-names = "default";
pinctrl-0 = <&i2c0_pins_default>;
status = "okay";
clock-frequency = <400000>;
tps: power-controller@2d {
reg = <0x2d>;
};
tpic2810: gpio@60 {
compatible = "ti,tpic2810";
reg = <0x60>;
gpio-controller;
#gpio-cells = <2>;
};
pca9536: gpio@41 {
compatible = "ti,pca9536";
reg = <0x41>;
gpio-controller;
#gpio-cells = <2>;
};
};
&spi0 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&spi0_pins_default>;
sn65hvs882@1 {
compatible = "pisosr-gpio";
gpio-controller;
#gpio-cells = <2>;
load-gpios = <&gpio3 18 GPIO_ACTIVE_LOW>;
reg = <1>;
spi-max-frequency = <1000000>;
spi-cpol;
};
spi_nor: flash@0 {
#address-cells = <1>;
#size-cells = <1>;
compatible = "winbond,w25q64", "jedec,spi-nor";
spi-max-frequency = <80000000>;
m25p,fast-read;
reg = <0>;
partition@0 {
label = "u-boot-spl";
reg = <0x0 0x80000>;
read-only;
};
partition@1 {
label = "u-boot";
reg = <0x80000 0x100000>;
read-only;
};
partition@2 {
label = "u-boot-env";
reg = <0x180000 0x20000>;
read-only;
};
partition@3 {
label = "misc";
reg = <0x1A0000 0x660000>;
};
};
};
&spi1 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&spi0_pins_default>;
spi_nor1: flash@0 {
#address-cells = <1>;
#size-cells = <1>;
compatible ="jedec,spi-nor";
spi-max-frequency = <80000000>;
m25p,fast-read;
reg = <0>;
partition@0 {
label = "u-boot-spl";
reg = <0x0 0x80000>;
read-only;
};
partition@1 {
label = "u-boot";
reg = <0x80000 0x100000>;
read-only;
};
partition@2 {
label = "u-boot-env";
reg = <0x180000 0x20000>;
read-only;
};
partition@3 {
label = "misc";
reg = <0x1A0000 0x660000>;
};
};
};
&tscadc {
status = "okay";
adc {
ti,adc-channels = <1 2 3 4 5 6 7>;
};
};
#include "tps65910.dtsi"
&tps {
vcc1-supply = <&vbat>;
vcc2-supply = <&vbat>;
vcc3-supply = <&vbat>;
vcc4-supply = <&vbat>;
vcc5-supply = <&vbat>;
vcc6-supply = <&vbat>;
vcc7-supply = <&vbat>;
vccio-supply = <&vbat>;
regulators {
vrtc_reg: regulator@0 {
regulator-always-on;
};
vio_reg: regulator@1 {
regulator-always-on;
};
vdd1_reg: regulator@2 {
regulator-name = "vdd_mpu";
regulator-min-microvolt = <912500>;
regulator-max-microvolt = <1326000>;
regulator-boot-on;
regulator-always-on;
};
vdd2_reg: regulator@3 {
regulator-name = "vdd_core";
regulator-min-microvolt = <912500>;
regulator-max-microvolt = <1144000>;
regulator-boot-on;
regulator-always-on;
};
vdd3_reg: regulator@4 {
regulator-always-on;
};
vdig1_reg: regulator@5 {
regulator-always-on;
};
vdig2_reg: regulator@6 {
regulator-always-on;
};
vpll_reg: regulator@7 {
regulator-always-on;
};
vdac_reg: regulator@8 {
regulator-always-on;
};
vaux1_reg: regulator@9 {
regulator-always-on;
};
vaux2_reg: regulator@10 {
regulator-always-on;
};
vaux33_reg: regulator@11 {
regulator-always-on;
};
vmmc_reg: regulator@12 {
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
};
};
};
&mmc1 {
status = "okay";
vmmc-supply = <&vmmc_reg>;
bus-width = <4>;
pinctrl-names = "default";
pinctrl-0 = <&mmc0_pins_default>;
};
&gpio0 {
/* Do not idle the GPIO used for holding the VTT regulator */
ti,no-reset-on-init;
ti,no-idle-on-init;
p7 {
gpio-hog;
gpios = <7 GPIO_ACTIVE_HIGH>;
output-high;
line-name = "FET_SWITCH_CTRL";
};
};
&uart3 {
pinctrl-names = "default";
pinctrl-0 = <&uart3_pins_default>;
status = "okay";
};
&uart4 {
pinctrl-names = "default";
pinctrl-0 = <&uart4_pins_default>;
status = "okay";
};
&gpio3 {
p4 {
gpio-hog;
gpios = <4 GPIO_ACTIVE_HIGH>;
output-high;
line-name = "PR1_MII_CTRL";
};
p10 {
gpio-hog;
gpios = <10 GPIO_ACTIVE_HIGH>;
/* ETH1 mux: Low for MII-PRU, high for RMII-CPSW */
output-high;
line-name = "MUX_MII_CTL1";
};
};
&mac {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&cpsw_default>;
pinctrl-1 = <&cpsw_sleep>;
dual_emac = <1>;
mode-gpios = <&gpio3 13 GPIO_ACTIVE_LOW>;
status = "okay";
};
&davinci_mdio {
pinctrl-names = "default", "sleep";
compatible = "ti, cpsw-mdio","ti,davinci_mdio";
pinctrl-0 = <&davinci_mdio_default>;
pinctrl-1 = <&davinci_mdio_sleep>;
status = "okay";
ti,rx-internal-delay = <DP83867_RGMIIDCTL_1_75_NS>;
ti,tx-internal-delay = <DP83867_RGMIIDCTL_1_75_NS>;
ti,fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>;
ti,min-output-impedance;
ti,dp83867-rxctrl-strap-quirk;
};
&cpsw_emac0 {
phy_id = <&davinci_mdio>, <0x0>;
phy-mode = "rgmii-id";
status = "okay";
};
&cpsw_emac1 {
phy_id = <&davinci_mdio>, <0x0>;
phy-mode = "rgmii-id";
status = "okay";
};
&i2c1{
compatible = "ti,omap4-i2c";
#address-cells = <1>;
#size-cells = <0>;
ti,hwmods = "i2c2";
reg = <0x4802a000 0x1000>;
interrupts = <71>;
status = "okay";
ad7414@48 {
compatible = "analog,ad7414";
reg = <0x48>;
status = "okay";
};
};
&gpmc {
status = "okay";
pinctrl-names = "default";
/*pinctrl-0 = <&gpmc_pins>;*/
ranges = <0 0 0x08000000 0x10000000>; /* CS0: NAND */
nand@0,0 {
reg = <0 0 0>; /* CS0, offset 0 */
ti,nand-ecc-opt = "bch8";
ti,elm-id = <&elm>;
nand-bus-width = <8>;
gpmc,device-width = <1>;
gpmc,sync-clk-ps = <0>;
gpmc,cs-on-ns = <0>;
gpmc,cs-rd-off-ns = <44>;
gpmc,cs-wr-off-ns = <44>;
gpmc,adv-on-ns = <6>;
gpmc,adv-rd-off-ns = <34>;
gpmc,adv-wr-off-ns = <44>;
gpmc,we-on-ns = <0>;
gpmc,we-off-ns = <40>;
gpmc,oe-on-ns = <0>;
gpmc,oe-off-ns = <54>;
gpmc,access-ns = <64>;
gpmc,rd-cycle-ns = <82>;
gpmc,wr-cycle-ns = <82>;
gpmc,wait-on-read = "true";
gpmc,wait-on-write = "true";
gpmc,bus-turnaround-ns = <0>;
gpmc,cycle2cycle-delay-ns = <0>;
gpmc,clk-activation-ns = <0>;
gpmc,wait-monitoring-ns = <0>;
gpmc,wr-access-ns = <40>;
gpmc,wr-data-mux-bus-ns = <0>;
/* MTD partition table */
/* All SPL-* partitions are sized to minimal length
* which can be independently programmable. For
* NAND flash this is equal to size of erase-block */
#address-cells = <1>;
#size-cells = <1>;
partition@0 {
label = "NAND.SPL";
reg = <0x00000000 0x000020000>;
};
partition@1 {
label = "NAND.SPL.backup1";
reg = <0x00020000 0x00020000>;
};
partition@2 {
label = "NAND.SPL.backup2";
reg = <0x00040000 0x00020000>;
};
partition@3 {
label = "NAND.SPL.backup3";
reg = <0x00060000 0x00020000>;
};
partition@4 {
label = "NAND.u-boot-spl-os";
reg = <0x00080000 0x00040000>;
};
partition@5 {
label = "NAND.u-boot";
reg = <0x000C0000 0x00100000>;
};
partition@6 {
label = "NAND.u-boot-env";
reg = <0x001C0000 0x00020000>;
};
partition@7 {
label = "NAND.kernel-dtb";
reg = <0x001E0000 0x00020000>;
};
partition@8 {
label = "NAND.kernel";
reg = <0x00200000 0x00800000>;
};
partition@9 {
label = "NAND.file-system";
reg = <0x00A00000 0x0F600000>;
};
};
fpga{
reg = <1 0 0x01000000>; /*CSn1*/
bank-width = <2>; /* GPMC_CONFIG1_DEVICESIZE(1) */
/*gpmc,burst-write;*/
/*gpmc,burst-read;*/
/*gpmc,burst-wrap;*/
gpmc,sync-read; /* GPMC_CONFIG1_READTYPE_ASYNC */
gpmc,sync-write; /* GPMC_CONFIG1_WRITETYPE_ASYNC */
gpmc,clk-activation-ns = <0>; /* GPMC_CONFIG1_CLKACTIVATIONTIME(2) */
gpmc,burst-length = <16>; /* GPMC_CONFIG1_PAGE_LEN(2) */
gpmc,mux-add-data = <2>; /* GPMC_CONFIG1_MUXTYPE(2) */
gpmc,sync-clk-ps = <20000>; /* CONFIG2 */
gpmc,cs-on-ns = <0>;
gpmc,cs-rd-off-ns = <100>;
gpmc,cs-wr-off-ns = <40>;
gpmc,adv-on-ns = <0>; /* CONFIG3 */
gpmc,adv-rd-off-ns = <20>;
gpmc,adv-wr-off-ns = <20>;
gpmc,we-on-ns = <20>; /* CONFIG4 */
gpmc,we-off-ns = <40>;
gpmc,oe-on-ns = <20>;
gpmc,oe-off-ns = <100>;
gpmc,page-burst-access-ns = <20>; /* CONFIG 5 */
gpmc,access-ns = <80>;
gpmc,rd-cycle-ns = <120>;
gpmc,wr-cycle-ns = <60>;
gpmc,wr-access-ns = <40>; /* CONFIG 6 */
gpmc,wr-data-mux-bus-ns = <20>;
/*gpmc,bus-turnaround-ns = <40>;*/ /* CONFIG6:3:0 = 4 */
gpmc,cycle2cycle-samecsen; /* CONFIG6:7 = 1 */
gpmc,cycle2cycle-delay-ns = <20>; /* CONFIG6:11:8 = 4 */
/* not using dma engine yet, but we can get the channel number here */
dmas = <&edma 1>;
dma-names = "cscdma";
};
};
Will the pinmuxing in dts file be enough?Or should I also do the pinmuxing in /board/ti/am335x/mux.c?
Regards,
Murugan S