Part Number: AM5728
Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI-RTOS
I have a complex algorithm which can run on a15_0 and I want to test it on a15. Then there is a problem. When I run the code, there is a instruction fetch exception happened. And the log is following:
[C66xx_DSP1] A28=0x0 A29=0x2
A30=0x804cd868 A31=0xf
B0=0x804cd868 B1=0xf
B2=0x6ef6ff5d B3=0x80af7e11
B4=0x80af0d78 B5=0x80ac27b0
B6=0x80afd600 B7=0x1c
B8=0x80ab0010 B9=0x1
B10=0x80aa39e4 B11=0x80af0d80
B12=0x80af0cd8 B13=0x2
B14=0x5001c B15=0x0
B16=0x80af7e7b B17=0x80acfa24
B18=0x80000000 B19=0xa
B20=0xffff0000 B21=0x80af0d10
B22=0x0 B23=0x80af0d10
B24=0xffffffff B25=0xffffffff
B26=0xfffffff7 B27=0x0
B28=0x66666666 B29=0x30666666
B30=0x804e2a50 B31=0x3
NTSR=0x0
ITSR=0x25
IRP=0x80acb09c
SSR=0xa
AMR=0x80af0d54
RILC=0x80aa8280
ILC=0xa
Exception at 0x40004c8
EFR=0x2 NRP=0x40004c8
Internal exception: IERR=0x1
Instruction fetch exception
ti.sysbios.family.c64p.Exception: line 256: E_exceptionMax: pc = 0x0000002d, sp = 0x00000001.
xdc.runtime.Error.raise: terminating execution
Can yo give me some advice to solve it?