Part Number: AM5718
Other Parts Discussed in Thread: TMDXIDK5718
Tool/software: Linux
Hi,
I'm trying to use RS485 (UART) in the following environment.
OS:Ubuntu 16.04.4 LTS
SDK:PROCESSOR-SDK-LINUX-RT-AM57X 05_02_00_10
EVM: TMDXIDK5718
Question1
Does RS485 (UART2) correspond to "/dev/ttyS1" on Linux?
Question2
I am using TMDXIDK57X-LCD.
Therefore am571x-idk-lcd-osd101t2587.dts is used,
Is RS-485 (UART2) recognized in this device tree?
And I am checking about Pinmux of RS485.
[sdk_install_dir]/board-support/u-boot-2018.01+gitAUTOINC+313dcd69c2^g313dcd69c2/board/ti/am57xx/mux_data.h
Question3
I look at TMDXIDK 5718 Schematic (Page. 29).
I think that the following description is incorrect.
Is this a mistake of OUTPUT?
Line 990: {MCASP5_ACLKX, (M12 | PIN_INPUT | MANUAL_MODE)}, /* mcasp5_aclkx.pr2_pru1_gpi1 */
Regards,
Rei