Part Number: TMS320C6678
Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI-RTOS
Hi,
I was roughly measuring the execution time of some function on my C6678 on one core and I am getting some time difference measuring in two ways. To do so, I included the following in my .cfg file:
var BIOS = xdc.useModule('ti.sysbios.BIOS');
var Clock = xdc.useModule('ti.sysbios.knl.Clock');
var Hwi = xdc.useModule('ti.sysbios.hal.Hwi');
In my C-file I included:
#include <ti/sysbios/knl/Clock.h>
#include <pthread.h>
#include <time.h>
#include <sys/time.h>
The function is embedded in a task which is called after BIOS_start. I am measuring the time in the following two ways:
clock_gettime(CLOCK_MONOTONIC, &tic);
t1 = TSCL;
// long function call
t2 = TSCL;
clock_gettime(CLOCK_MONOTONIC, &toc);
elapsed_time = calc_time(&tic, &toc);
elapsed_tscl_time = ((double)t2-(double)t1)/(1000000000.0); // running at 1GHz
where I pasted the function calc_time() below.
that I should use constant Clock_tickPeriod to calculate the elapsed time. On that website, it says that Clock_tickPeriod is defined in MICROseconds.
In some post in this forum, I read that TSCL returns the number of elapsed cycles. I therefore have to use the processor frequency of 1GHz in order to extract the elapsed time.
The output of my code is the following:
TSCL elapsed time = 0.89283968 seconds
clock_gettime elapsed time: 0.000893 seconds
The results from TSCL and clock_gettime seem to be different by a factor of 1000. I measured 10 functions runs and compared it with my watch (~8 seconds), and the TSCL measurement seems to be correct. From that, I follow that either Clock_tickPeriod is defined in MILLIseconds or that the function calc_time() below does something wrong. Can someone confirm my observation? Thank you very much.
calc_time:
float calc_time(struct timespec *tic, struct timespec *toc)
{
struct timespec temp;
if ((toc->tv_nsec - tic->tv_nsec) < 0) {
temp.tv_sec = toc->tv_sec - tic->tv_sec - 1;
temp.tv_nsec = 1e9 + toc->tv_nsec - tic->tv_nsec;
} else {
temp.tv_sec = toc->tv_sec - tic->tv_sec;
temp.tv_nsec = toc->tv_nsec - tic->tv_nsec;
}
// Clock_tickPeriod in microseconds
return ((float)temp.tv_sec + (float)temp.tv_nsec / 1e9)*((float)Clock_tickPeriod)*1.0e-6;
}