Part Number: AM3352
Other Parts Discussed in Thread: DP83640
Hi,
AM335x TRM section 14.3.2.2 describes IEEE 1588v2 Clock Synchronization Support. The necessary conditions for the CPTS to capture a time stamp for an IPV4 (Annex D) message appear to include the requirement that the destination IP address is 224.0.1.129 (or .130 or .131 or .132). If this is truly the case, then the system has the following limitations:
(a) Only multicast messages can be time-stamped. Unicast messages are not supported.
(b) Peer-to-peer synchronization is not possible as, by the IEEE 1588v2 spec, peer delay multicast messages use the IP address 224.0.0.107
These are pretty severe limitations. Could some one please confirm that my interpretation is correct?
And if correct, is there a workaround?
Thanks,
GerryL