Hi,
I have a custom board with 66AK2H14.
I use CCSV9 + GEL file to setup DDR3 configuration registers.
On the board DDR3B is not connected to a DDR3 chip. DDR3A is used.
DDR3_REMAP_EN=0
I cannot figure out if access to 0x80000000 when running DDR test from the GEL file is correctly directed to DDR3A.
In my case, what would be the correct configuration sequence (XMC and MSMC) to be sure that read/write to 0x80000000 is directed to DDR3A chip ?
Thank you.