This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/BEAGLEBN: UART4 not showing in Beaglebone Black

Part Number: BEAGLEBN

Tool/software: Linux

I have added the following configurations in my am335x-boneblack.dts file to enable uart4.

&am33xx_pinmux {
	uart4_pins_default: uart4_pins_default {
		pinctrl-single,pins = <
			AM33XX_IOPAD(0x870, PIN_INPUT_PULLUP | MUX_MODE6)       /* (P9_11) uart4_rxd */
			AM33XX_IOPAD(0x874, PIN_OUTPUT_PULLDOWN | MUX_MODE6)       /* (P9_13) uart4_txd */		
		>;
	};
};
&uart4 {
	pinctrl-names = "default";
	pinctrl-0 = <&uart4_pins_default>;
	status = "okay";
};

After creating a dtb file with these configurations. I could change the disabled status to okay as shown below:

serial@481a8000 {
compatible = "ti,am3352-uart", "ti,omap3-uart";
ti,hwmods = "uart5";   // in TI uart starts from 1, so uart4=uart5
clock-frequency = <0x2dc6c00>;
reg = <0x481a8000 0x2000>;
interrupts = <0x2d>;
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <0x2c>;
};

I then copied the compiled dtb file into beaglebone's boot folder, performed a sync operation and rebooted it and checked for the device with the command:

>>dmesg | grep ttyO

Only the UART0 is showing and there are no signs of UART4. What could have possibly gone wrong?