Part Number: TMDSICE3359
Tool/software: TI C/C++ Compiler
Hello,
I've the TMDSICE3359 and I want to implement HSR protocol on it.
To do that, I've download :
- PRU ICSS SW for HSR/PRP v01.00.04.02
- Processor SDK TI RTOS v4.03.00.05
- CCS 7.4.0.00015
I have also target my board and import the HSR project (that I've find in the PRU ICSS SW for HSR/PRP).
Now, when I build this project, there is 13 Errors.
After searching the error, I find an inconsistency in this project.
As you can see in the following PDF, in the fonction void runRxTxTest(ICSSEMAC_Handle emachandle) that we find in the hsr_prp_menu.c, the ethPrioQueue is used as an array.
Utilisation ethPrioQueue en tableau.pdf
But, it is define as an Uint8 in the of typedefstruct that we find in the icss_emacDrv.h, as you can see in the PDF. So I don't understant. And this inconsistency bring me an error like that "subscripted value is neither array nor pointer nor vector". Could you help me please to resolve this.