Part Number: AM5728
Tool/software: Code Composer Studio
Hello,
I’m trying to build an SPI Master application for IPU1/AM5728 based upon RTOS Template Application Workshop described here: http://software-dl.ti.com/processor-sdk-rtos/esd/docs/latest/rtos/index_examples_demos.html
The Beagleboard x15 is running TI Linux RT SDK. I compiled the example Project using CCS 9.0 and copied the .out file to /lib/firmware/rtos_template/ rtos_template_app_am572x_m4.xem4. After that I linked the app to start it using remoteproc:
ln -sf /lib/firmware/rtos_template/rtos_template_app_am572x_m4.xem4 dra7-ipu1-fw.xem4 root@am57xx-evm:/lib/firmware# ls -l dra7-ipu1-fw.xem4 lrwxrwxrwx 1 root root 60 Jun 11 19:39 dra7-ipu1-fw.xem4 -> /lib/firmware/rtos_template/rtos_template_app_am572x_m4.xem4
Then I stop the core:
echo 58820000.ipu > /sys/bus/platform/drivers/omap-rproc/unbind
dmesg:
[ 3996.732892] remoteproc remoteproc0: releasing 58820000.ipu
And start the application:
echo 58820000.ipu > /sys/bus/platform/drivers/omap-rproc/bind
And then dmesg shows that resource table error:
[ 4019.802885] omap-rproc 58820000.ipu: assigned reserved memory node ipu1-memory@9d000000 [ 4019.812784] remoteproc remoteproc0: 58820000.ipu is available [ 4019.831368] remoteproc remoteproc0: powering up 58820000.ipu [ 4019.837077] remoteproc remoteproc0: Booting fw image dra7-ipu1-fw.xem4, size 2957080 [ 4019.844966] omap-iommu 58882000.mmu: 58882000.mmu: version 2.1 [ 4019.850846] remoteproc remoteproc0: Failed to find resource table
How can I fix that problem?
At the moment I don’t have a JTAG debugger so I'm not able to start the application from CCS, but an XDS110 is on it's way.
Thanks a lot!