Hi,
I am considering a gateway for industrial communication. I want to realize this in one chip.
Is there a device that can realize the following functions with Sitara in one chip?
1. EtherNet/IP Master + EtherNet/IP Slave + EtherCAT Master + EtherCAT Slave
2. EtherNet/IP Master + EtherCAT Master
3. EtherNet/IP Slave + EtherCAT Slave
4. Standard TCP/IP + EtherNet/IP Master + EtherNet/IP Slave
5. Standard TCP/IP + EtherCAT Master + EtherCAT Slave
Can each combination mentioned above be realized with AM57xx?
Also, is there a possibility that can be realized with AM335x or AM437x?
Best Regards,
H.U