Part Number: 66AK2H14
Hello, I found an example of a cycle delay for and ARM core and the trouble is when I read the cycle count register is returns zero. Here is my code:
#include <ti/csl/csl_tmr.h>
static unsigned int ReadTime32(void)
{
unsigned int timeVal;
__asm__ __volatile__ ("MRC p15,0,%0,c9,c13,0\t\n" : "=r"(timeVal));
return timeVal;
}
void CycleDelay(unsigned int iCount)
{
if(iCount <=0)
{
return;
}
unsigned int start = ReadTime32();
while((ReadTime32() - start) < iCount);
}
#define CSL_GPIO_CFG_REGS 0x0260BF00
#define CSL_GPIO_DIR (*(unsigned int*)(CSL_GPIO_CFG_REGS + 0x010))
#define GPIO_SET_DATA (*(unsigned int*)(CSL_GPIO_CFG_REGS + 0x018))
#define GPIO_CLEAR_DATA (*(unsigned int*)(CSL_GPIO_CFG_REGS + 0x01C))
int main(void)
{
int i;
CSL_GPIO_DIR = 0xFFFE;
while(1)
{
GPIO_SET_DATA = 0x1;
CycleDelay(1000);
GPIO_CLEAR_DATA = 0x1;
for (i=0;i<100;i++);
}
return 0;
}
Here is my design:
The example I found did not list the main() so maybe there is some other things I need to do to get things working.
Thank you very much,
Joe