Tool/software: Code Composer Studio
Hello, when I compile my simple, Baremetal, SPI example code I receive the following warning:
warning #10247-D: creating output section ".csl_vect" without a SECTIONS specification
How can get rid of this warning?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hello, when I compile my simple, Baremetal, SPI example code I receive the following warning:
warning #10247-D: creating output section ".csl_vect" without a SECTIONS specification
How can get rid of this warning?
To resolve the warning the 66AK2Gxx_C66.cmd linker command file used by the project needs to modified to explicitly place the ".csl_vect" section in a memory region. Since all other sections are placed in the L2_SRAM_0 region, suggest add the following to the SECTIONS:joe306 said:warning #10247-D: creating output section ".csl_vect" without a SECTIONS specificationHow can get rid of this warning?
.csl_vect > L2_SRAM_0
Chester,
Hello, thank you for solving my problem.
Would I put that under the /* COFF sections */ or under the /* EABI sections */
Thanks,
Joe
It doesn't matter, since they are only comments.joe306 said:Would I put that under the /* COFF sections */ or under the /* EABI sections */
The ".csl_vect" section is actually defined in the PDK packages/ti/csl/src/intc/_csl_intcIsrDispatch.asm source file which is independent of the COFF or EABI output format, so placing ".csl_vect" with the section prior to the /* COFF sections */ comment make more logical sense.