This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6548: am6548 SDk release 5.03.0.07 devmem2 source

Part Number: AM6548


Hi 

I like to get the source for the devmem2 please. I found the following at the below site

https://www.lorixone.io/yocto/licenses/2.1.2/devmem2/devmem2.c

I compiled it using the SDK compiler.

i did the below command

devmem2  $((0x686000 + 0x0010)) w 0x0

got the below error

Error at line 81, file devmem2.c (22) [Invalid argument]

but if i do the same with the devmem2 that comes with the SDK it works fine i get the below

root@am65xx-evm:~# devmem2 $((0x686000 + 0x0010)) w 0x0
/dev/mem opened.
Memory mapped at address 0xffff94090000.
Read at address 0x00686010 (0xffff94096010): 0x68EF3491
Write at address 0x00686010 (0xffff94096010): 0x00000000, readback 0x00000000

Any ideas would be great.

It sounds like it does not calculate the correct address from the MMU

Thanks

  • Hello Mohsen,

    This is the source code of devmem2.

    /*
     * devmem2.c: Simple program to read/write from/to any location in memory.
     *
     *  Copyright (C) 2000, Jan-Derk Bakker (J.D.Bakker@its.tudelft.nl)
     *
     *
     * This software has been developed for the LART computing board
     * (http://www.lart.tudelft.nl/). The development has been sponsored by
     * the Mobile MultiMedia Communications (http://www.mmc.tudelft.nl/)
     * and Ubiquitous Communications (http://www.ubicom.tudelft.nl/)
     * projects.
     *
     * The author can be reached at:
     *
     *  Jan-Derk Bakker
     *  Information and Communication Theory Group
     *  Faculty of Information Technology and Systems
     *  Delft University of Technology
     *  P.O. Box 5031
     *  2600 GA Delft
     *  The Netherlands
     *
     *
     * This program is free software; you can redistribute it and/or modify
     * it under the terms of the GNU General Public License as published by
     * the Free Software Foundation; either version 2 of the License, or
     * (at your option) any later version.
     *
     * This program is distributed in the hope that it will be useful,
     * but WITHOUT ANY WARRANTY; without even the implied warranty of
     * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
     * GNU General Public License for more details.
     * 
     * You should have received a copy of the GNU General Public License
     * along with this program; if not, write to the Free Software
     * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA  02111-1307  USA
     *
     */
    
    #include <stdio.h>
    #include <stdlib.h>
    #include <unistd.h>
    #include <string.h>
    #include <errno.h>
    #include <signal.h>
    #include <fcntl.h>
    #include <ctype.h>
    #include <termios.h>
    #include <sys/types.h>
    #include <sys/mman.h>
      
    #define FATAL do { fprintf(stderr, "Error at line %d, file %s (%d) [%s]\n", \
      __LINE__, __FILE__, errno, strerror(errno)); exit(1); } while(0)
     
    #define MAP_SIZE 4096UL
    #define MAP_MASK (MAP_SIZE - 1)
    
    int main(int argc, char **argv) {
        int fd;
        void *map_base, *virt_addr; 
    	unsigned long read_result, writeval;
    	off_t target;
    	int access_type = 'w';
    	
    	if(argc < 2) {
    		fprintf(stderr, "\nUsage:\t%s { address } [ type [ data ] ]\n"
    			"\taddress : memory address to act upon\n"
    			"\ttype    : access operation type : [b]yte, [h]alfword, [w]ord\n"
    			"\tdata    : data to be written\n\n",
    			argv[0]);
    		exit(1);
    	}
    	target = strtoul(argv[1], 0, 0);
    
    	if(argc > 2)
    		access_type = tolower(argv[2][0]);
    
    
        if((fd = open("/dev/mem", O_RDWR | O_SYNC)) == -1) FATAL;
        printf("/dev/mem opened.\n"); 
        fflush(stdout);
        
        /* Map one page */
        map_base = mmap(0, MAP_SIZE, PROT_READ | PROT_WRITE, MAP_SHARED, fd, target & ~MAP_MASK);
        if(map_base == (void *) -1) FATAL;
        printf("Memory mapped at address %p.\n", map_base); 
        fflush(stdout);
        
        virt_addr = map_base + (target & MAP_MASK);
        switch(access_type) {
    		case 'b':
    			read_result = *((unsigned char *) virt_addr);
    			break;
    		case 'h':
    			read_result = *((unsigned short *) virt_addr);
    			break;
    		case 'w':
    			read_result = *((unsigned long *) virt_addr);
    			break;
    		default:
    			fprintf(stderr, "Illegal data type '%c'.\n", access_type);
    			exit(2);
    	}
        printf("Value at address 0x%X (%p): 0x%X\n", target, virt_addr, read_result); 
        fflush(stdout);
    
    	if(argc > 3) {
    		writeval = strtoul(argv[3], 0, 0);
    		switch(access_type) {
    			case 'b':
    				*((unsigned char *) virt_addr) = writeval;
    				read_result = *((unsigned char *) virt_addr);
    				break;
    			case 'h':
    				*((unsigned short *) virt_addr) = writeval;
    				read_result = *((unsigned short *) virt_addr);
    				break;
    			case 'w':
    				*((unsigned long *) virt_addr) = writeval;
    				read_result = *((unsigned long *) virt_addr);
    				break;
    		}
    		printf("Written 0x%X; readback 0x%X\n", writeval, read_result); 
    		fflush(stdout);
    	}
    	
    	if(munmap(map_base, MAP_SIZE) == -1) FATAL;
        close(fd);
        return 0;
    }
    
    


    You need to apply these three patches on it.
    https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/791/devmem2_2D00_fixups_2D00_2.patch
    https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/791/0001_2D00_devmem.c_2D00_ensure_2D00_word_2D00_is_2D00_32_2D00_bit_2D00_and_2D00_add_2D00_support_2D00_for_2D00_6.patch
    https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/791/0001_2D00_devmem2_2D00_support_2D00_different_2D00_page_2D00_sizes_2D00_at_2D00_run_2D00_time.patch

    Best regards,
    Kemal

  • Hello Mohsen,

    Were you able to find the sources now?

    Best regards,
    Kemal

  • Hi Kemal

    how did you find this out? i did a search but could not find the third patch? I will give it a try tomorrow and let you know if that resolves my issue or not..

    Thanks

  • I figured this out from the OE build system. These patches gets applied there while building. The third patch gets applied by <tisdk>/sources/meta-arago/meta-arago-extras/recipes-support/devmem2/devmem2.bbappend file, maybe this confused you.