This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA3XEVM: Why does Fast boot usecase not allow ipu1_1 to be added?

Part Number: TDA3XEVM

Regarding to IPU1_1, I’m seeing the following statement in the user guide.

In the first note, you can add cores as needed.

But "fast_boot_iss_capture_isp_simcop_pd_display"   IPU1_1 is not allowed when testing options 3 and 4.

What is the cause of this?

Does "FAST_BOOT_INCLUDE=yes" affect the use of IPU1_1?

I need to use my own fastboot usecase by modify "fast_boot_iss_capture_isp_simcop_pd_display" and I need IPU1_0, IPU1_1, DSP1.