Part Number: AM5729
Other Parts Discussed in Thread: AM3358
I am on the BeagleBone AI (AM5729) and I added this to the dtb:
&mcspi3 {
#address-cells = <1>;
#size-cells = <0>;
status = "okay";
cs-gpios = <0>, <&gpio7 11 0>;
channel@0 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "spidev";
reg = <0>;
spi-max-frequency = <24000000>;
};
channel@1 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "spidev";
reg = <1>;
spi-max-frequency = <24000000>;
};
};
When I try to use the McSPI, the SCLK and MOSI lines work just fine, however I cannot receive any data on the input. I tried both connecting the MISO and MOSI lines together and connecting the MISO line to 3.3V, with no luck.
Here's my code:
#include <stdio.h>
#include <unistd.h>
#include <sys/types.h>
#include <sys/stat.h>
#include <fcntl.h>
#include <sys/ioctl.h>
#include <linux/spi/spidev.h>
int main(){
static struct spi_ioc_transfer transfer_spidev;
int fd = 0;
char* spi_dev_path = "/dev/spidev2.0";
unsigned long spi_bus_speed = 1000000;
unsigned char spi_chip_select = 0;
unsigned short spi_delay_us = 0;
unsigned char spi_bits_no = 8;
unsigned char spi_mode = SPI_MODE_3;
/* Open the spidev device */
if((fd = open(spi_dev_path, O_RDWR))<0)
{
perror("SPI: Failed to open spidev1.0 |");
return -1;
}
/* Set the SPI mode for RD and WR operations */
if(ioctl(fd, SPI_IOC_WR_MODE, &spi_mode)==-1) {
perror("SPI: Failed to set SPIMODE |");
return -1;
}
if(ioctl(fd, SPI_IOC_RD_MODE, &spi_mode)==-1) {
perror("SPI: Failed to set SPIMODE |");
return -1;
}
/* Set the No. of bits per transaction */
if(ioctl(fd, SPI_IOC_WR_BITS_PER_WORD, &spi_bits_no)==-1) {
perror("SPI: Failed to set No. of bits per word |");
return -1;
}
if(ioctl(fd, SPI_IOC_RD_BITS_PER_WORD, &spi_bits_no)==-1) {
perror("SPI: Failed to set No. of bits per word |");
return -1;
}
/* Set the SPI bus speed in Hz */
if(ioctl(fd, SPI_IOC_WR_MAX_SPEED_HZ, &spi_bus_speed)==-1) {
perror("SPI: Failed to set SPI bus frequency |");
return -1;
}
if(ioctl(fd, SPI_IOC_RD_MAX_SPEED_HZ, &spi_bus_speed)==-1) {
perror("SPI: Failed to set SPI bus frequency |");
return -1;
}
/* Initialize the spi_ioc_transfer structure that will be passed to the
* KERNEL to define/configure each SPI Transactions*/
transfer_spidev.tx_buf = 0;
transfer_spidev.rx_buf = 0;
transfer_spidev.pad = 0;
transfer_spidev.tx_nbits = 0;
transfer_spidev.rx_nbits = 0;
transfer_spidev.speed_hz = spi_bus_speed;
transfer_spidev.delay_usecs = spi_delay_us;
transfer_spidev.bits_per_word = spi_bits_no;
transfer_spidev.cs_change = spi_chip_select;
int transmissionLength = 4;
unsigned char tx_spi[transmissionLength];
unsigned char rx_spi[transmissionLength];
tx_spi[0] = 0xff;
tx_spi[1] = 0x22;
tx_spi[2] = 0xff;
tx_spi[3] = 0x0;
for(int n = 0; n < transmissionLength; ++n)
rx_spi[n] = 0xA0; // initialize to known value
while(1) {
/* Points to the Tx and Rx buffer */
transfer_spidev.tx_buf = (unsigned long)tx_spi;
transfer_spidev.rx_buf = (unsigned long)rx_spi;
/* Override No. of bytes per transaction */
transfer_spidev.len = transmissionLength;
/* Perform a SPI Transaction */
if (ioctl(fd, SPI_IOC_MESSAGE(1), &transfer_spidev)<0)
{
perror("SPI: SPI_IOC_MESSAGE Failed |");
return -1;
}
printf("rx_buf [%u]: ", transfer_spidev.len);
for(int n = 0; n < transfer_spidev.len; ++n)
printf("0x%02x ", rx_spi[n]);
printf("\n");
usleep(100000);
}
close(fd);
return 0;
}
Regardless of whether I connect the MISO line to 3.3V or to MOSI, or leave it unconnected, I alway get as an output:
rx_buf [4]: 0x0 0x0 0x00 0x00
Notes:
- on the am5729 I get the same results (i.e.: no input) with kernel 4.14 and 4.19
- this code works just fine on the am3358 (PocketBeagle).