This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/K2GICE: GPIO Port/Pin configurations

Part Number: K2GICE


Tool/software: Code Composer Studio

Hi

Im learning my way thought the GPIO led blink example.

I got the software running, but im having difficulties modifying in to blink different LED. Id amuse that changing LED0 these port and pin values at GPIO_board.h would be the solution

#if defined (iceK2G)
#define GPIO_LED0_PIN_NUM (11U) /* by default PADCONFIG139 set to GPIO0_108 */
#define GPIO_LED0_PORT_NUM (0U) /* GPIO port 0 */
#define GPIO_LED1_PIN_NUM (12U) /* by default PADCONFIG186 set to GPIO1_11 */
#define GPIO_LED1_PORT_NUM (1U) /* GPIO port 1 */

Problem is that i can not find these values for different gpio ports from technical reference guide or documentation.