Part Number: AM5708
This is related to topic: https://e2e.ti.com/support/processors/f/791/t/639301
We have migrated from the 4.4 TI linux kernel to the newer 4.19.79+ kernel which is supported in the latest SDK release for AM57xx SoC.
Using the new U-Blox driver for a 4.20+ kernel on our platform, we see that the driver doesn't boot. According to U-Blox support this could be caused by SDHCI driver handling interrupts & clock:
"The problem is most likely related to SDIO IRQs from the module being lost, because the host switches off the SDIO clock between transfers, instead of keeping it running or switching to 1-bit mode as required by the spec. We've seen this issue on other TI AM57xx platforms as well with newer kernel versions that use sdhci driver instead of the older hsmmc."
Is there some way we could keep the sdio clock alive between transfers?
We are executing the following prior to loading the module:
echo on > /sys/class/mmc_host/mmc2/device/power/control echo on > /sys/class/mmc_host/mmc2/power/control echo 1 > /sys/devices/platform/44000000.ocp/480ad000.mmc/mmc_host/mmc2/rescan
But it isn't sufficient..
Below the full boot-log:
Thanks in advance,
Stef Boerrigter
Boot Log (Dmesg Output)
root@target:~# dmesg
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.19.73-00043-g58cd7d7-dirty (BEI\boerrs@aln-lx911922) (gcc version 7.3.0 (GCC)) #254 PREEMPT Mon Dec 2 13:35:42 CET 2019
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: div instructions available: patching division code
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] OF: fdt: Machine model: TI AM5708
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] Reserved memory: created CMA memory pool at 0x95800000, size 56 MiB
[ 0.000000] OF: reserved mem: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
[ 0.000000] OMAP4: Map 0x9fe00000 to (ptrval) for dram barrier
[ 0.000000] On node 0 totalpages: 119552
[ 0.000000] Normal zone: 1148 pages used for memmap
[ 0.000000] Normal zone: 0 pages reserved
[ 0.000000] Normal zone: 119552 pages, LIFO batch:31
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] DRA722 ES2.1
[ 0.000000] random: get_random_bytes called from start_kernel+0xa0/0x49c with crng_init=0
[ 0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
[ 0.000000] pcpu-alloc: [0] 0
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 118404
[ 0.000000] Kernel command line: console=ttyO1,115200n8 rootwait noinitrd loglevel=7 HDMI-A-1:1280x800@60 vt.global_cursor_default=0 rw nfsroot=192.168.0.254:/srv/target/nfsroot root=/dev/nfs ip=192.168.0.1:192.168.0.254:192.168.0.254:255.255.255.0::eth0:off::
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 390408K/478208K available (10240K kernel code, 791K rwdata, 3080K rodata, 1024K init, 7454K bss, 30456K reserved, 57344K cma-reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xe0000000 - 0xff800000 ( 504 MB)
lowmem : 0xc0000000 - 0xdfe00000 ( 510 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.text : 0x(ptrval) - 0x(ptrval) (11232 kB)
.init : 0x(ptrval) - 0x(ptrval) (1024 kB)
.data : 0x(ptrval) - 0x(ptrval) ( 792 kB)
.bss : 0x(ptrval) - 0x(ptrval) (7455 kB)
[ 0.000000] Running RCU self tests
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU lockdep checking is enabled.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] OMAP clockevent source: timer1 at 32786 Hz
[ 0.000000] arch_timer: cp15 timer(s) running at 6.14MHz (virt).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[ 0.000005] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[ 0.000023] Switching to timer-based delay loop, resolution 162ns
[ 0.000280] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000295] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.001187] Console: colour dummy device 80x30
[ 0.001221] Lock dependency validator: Copyright (c) 2006 Red Hat, Inc., Ingo Molnar
[ 0.001235] ... MAX_LOCKDEP_SUBCLASSES: 8
[ 0.001250] ... MAX_LOCK_DEPTH: 48
[ 0.001264] ... MAX_LOCKDEP_KEYS: 8191
[ 0.001277] ... CLASSHASH_SIZE: 4096
[ 0.001291] ... MAX_LOCKDEP_ENTRIES: 32768
[ 0.001304] ... MAX_LOCKDEP_CHAINS: 65536
[ 0.001317] ... CHAINHASH_SIZE: 32768
[ 0.001331] memory used by lock dependency info: 4655 kB
[ 0.001344] per task-struct memory footprint: 1536 bytes
[ 0.001392] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[ 0.001418] pid_max: default: 32768 minimum: 301
[ 0.001641] Security Framework initialized
[ 0.001728] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.001748] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.003833] CPU: Testing write buffer coherency: ok
[ 0.003945] CPU0: Spectre v2: using ICIALLU workaround
[ 0.006421] Setting up static identity map for 0x80100000 - 0x80100060
[ 0.006783] rcu: Hierarchical SRCU implementation.
[ 0.009952] devtmpfs: initialized
[ 0.059014] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.060337] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.060381] futex hash table entries: 256 (order: 1, 11264 bytes)
[ 0.062258] pinctrl core: initialized pinctrl subsystem
[ 0.065351] NET: Registered protocol family 16
[ 0.065971] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.067743] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.369518] audit: initializing netlink subsys (disabled)
[ 0.371328] cpuidle: using governor ladder
[ 0.371476] cpuidle: using governor menu
[ 0.380867] audit: type=2000 audit(0.360:1): state=initialized audit_enabled=0 res=1
[ 0.392134] gpio gpiochip0: (gpio-0-31): added GPIO chardev (254:0)
[ 0.392417] gpiochip_setup_dev: registered GPIOs 0 to 31 on device: gpiochip0 (gpio-0-31)
[ 0.392474] OMAP GPIO hardware version 0.1
[ 0.393789] gpio gpiochip1: (gpio-32-63): added GPIO chardev (254:1)
[ 0.393941] gpiochip_setup_dev: registered GPIOs 32 to 63 on device: gpiochip1 (gpio-32-63)
[ 0.395142] gpio gpiochip2: (gpio-64-95): added GPIO chardev (254:2)
[ 0.395287] gpiochip_setup_dev: registered GPIOs 64 to 95 on device: gpiochip2 (gpio-64-95)
[ 0.396484] gpio gpiochip3: (gpio-96-127): added GPIO chardev (254:3)
[ 0.396637] gpiochip_setup_dev: registered GPIOs 96 to 127 on device: gpiochip3 (gpio-96-127)
[ 0.397860] gpio gpiochip4: (gpio-128-159): added GPIO chardev (254:4)
[ 0.398006] gpiochip_setup_dev: registered GPIOs 128 to 159 on device: gpiochip4 (gpio-128-159)
[ 0.399216] gpio gpiochip5: (gpio-160-191): added GPIO chardev (254:5)
[ 0.399367] gpiochip_setup_dev: registered GPIOs 160 to 191 on device: gpiochip5 (gpio-160-191)
[ 0.400523] gpio gpiochip6: (gpio-192-223): added GPIO chardev (254:6)
[ 0.400675] gpiochip_setup_dev: registered GPIOs 192 to 223 on device: gpiochip6 (gpio-192-223)
[ 0.401956] gpio gpiochip7: (gpio-224-255): added GPIO chardev (254:7)
[ 0.402103] gpiochip_setup_dev: registered GPIOs 224 to 255 on device: gpiochip7 (gpio-224-255)
[ 0.435976] No ATAGs?
[ 0.436014] hw-breakpoint: Failed to enable monitor mode on CPU 0.
[ 0.437949] OMAP DMA hardware revision 0.0
[ 0.465211] edma 43300000.edma: memcpy is disabled
[ 0.473880] edma 43300000.edma: TI EDMA DMA engine driver
[ 0.491232] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
[ 0.492181] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator-vsys5v0[0]'
[ 0.492689] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator-vdd_3v3[0]'
[ 0.493179] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator-vdd_1v8[0]'
[ 0.496149] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[ 0.496518] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[ 0.497013] omap-iommu 58882000.mmu: 58882000.mmu registered
[ 0.497516] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 0.498216] iommu: Adding device 55020000.ipu to group 2
[ 0.499761] SCSI subsystem initialized
[ 0.500274] usbcore: registered new interface driver usbfs
[ 0.500411] usbcore: registered new interface driver hub
[ 0.500572] usbcore: registered new device driver usb
[ 0.503217] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[ 0.504273] omap_i2c 48072000.i2c: bus 1 rev0.12 at 100 kHz
[ 0.505104] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz
[ 0.506399] omap_i2c 4807a000.i2c: bus 3 rev0.12 at 400 kHz
[ 0.506815] pps_core: LinuxPPS API ver. 1 registered
[ 0.506832] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.506875] PTP clock support registered
[ 0.507851] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[ 0.508684] Advanced Linux Sound Architecture Driver Initialized.
[ 0.511588] clocksource: Switched to clocksource arch_sys_counter
[ 0.691131] missing cooling_device property
[ 0.691155] failed to build thermal zone board_thermal: -2
[ 0.691463] NET: Registered protocol family 2
[ 0.692949] tcp_listen_portaddr_hash hash table entries: 256 (order: 1, 10240 bytes)
[ 0.693024] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.693101] TCP bind hash table entries: 4096 (order: 5, 147456 bytes)
[ 0.693847] TCP: Hash tables configured (established 4096 bind 4096)
[ 0.694082] UDP hash table entries: 256 (order: 2, 20480 bytes)
[ 0.694206] UDP-Lite hash table entries: 256 (order: 2, 20480 bytes)
[ 0.694527] NET: Registered protocol family 1
[ 0.695747] RPC: Registered named UNIX socket transport module.
[ 0.695800] RPC: Registered udp transport module.
[ 0.695816] RPC: Registered tcp transport module.
[ 0.695831] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.697784] Unpacking initramfs...
[ 1.247625] Freeing initrd memory: 1648K
[ 1.248805] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[ 1.251846] Initialise system trusted keyrings
[ 1.252276] workingset: timestamp_bits=14 max_order=17 bucket_order=3
[ 1.253243] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 1.254690] NFS: Registering the id_resolver key type
[ 1.254779] Key type id_resolver registered
[ 1.254830] Key type id_legacy registered
[ 1.265618] Key type asymmetric registered
[ 1.265703] Asymmetric key parser 'x509' registered
[ 1.265809] io scheduler noop registered
[ 1.265828] io scheduler deadline registered
[ 1.265908] io scheduler cfq registered (default)
[ 1.265926] io scheduler mq-deadline registered
[ 1.265943] io scheduler kyber registered
[ 1.272425] of_get_named_gpiod_flags: parsed 'device-enable' property of node '/tca9617bdgk@0[0]' - status (0)
[ 1.272635] of_get_named_gpiod_flags: parsed 'device-enable' property of node '/tca9617bdgk@1[0]' - status (0)
[ 1.278908] pinctrl-single 4a003400.pinmux: 282 pins, size 1128
[ 1.279355] pinctrl-single 4a002e8c.pinmux: initialized with no interrupts
[ 1.279374] pinctrl-single 4a002e8c.pinmux: 1 pins, size 4
[ 1.287626] pwm-backlight backlight: GPIO lookup for consumer backlight-power-enable
[ 1.287639] pwm-backlight backlight: using device tree for GPIO lookup
[ 1.287685] of_get_named_gpiod_flags: parsed 'backlight-power-enable-gpios' property of node '/backlight[0]' - status (0)
[ 1.287708] gpio gpiochip4: Persistence not supported for GPIO 18
[ 1.287727] pwm-backlight backlight: GPIO lookup for consumer enable
[ 1.287737] pwm-backlight backlight: using device tree for GPIO lookup
[ 1.287779] of_get_named_gpiod_flags: parsed 'enable-gpios' property of node '/backlight[0]' - status (0)
[ 1.287844] gpio gpiochip0: Persistence not supported for GPIO 23
[ 1.288234] pwm-backlight backlight: Linked as a consumer to regulator.2
[ 1.290127] usbcore: registered new interface driver udlfb
[ 1.290231] usbcore: registered new interface driver smscufx
[ 1.305222] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 1.308982] omap_uart 4806a000.serial: no wakeirq for uart0
[ 1.309044] of_get_named_gpiod_flags: parsed 'rts-gpio' property of node '/ocp/serial@4806a000[0]' - status (0)
[ 1.309138] serial_omap_probe_rs485: RSP RX Timeout set to 244 us
[ 1.309157] serial_omap_probe_rs485: Driver vs Serial line discipline sync active
[ 1.309494] 4806a000.serial: ttyO0 at MMIO 0x4806a000 (irq = 43, base_baud = 3000000) is a OMAP UART0
[ 1.310261] omap_uart 4806c000.serial: no wakeirq for uart1
[ 1.310305] of_get_named_gpiod_flags: can't parse 'rts-gpio' property of node '/ocp/serial@4806c000[0]'
[ 1.310400] 4806c000.serial: ttyO1 at MMIO 0x4806c000 (irq = 44, base_baud = 3000000) is a OMAP UART1
[ 2.192730] console [ttyO1] enabled
[ 2.197592] usbcore: registered new interface driver udl
[ 2.204058] omapdss_dss 58000000.dss: Linked as a consumer to regulator.2
[ 2.211252] omapdss_dss 58000000.dss: GPIO lookup for consumer lcd-power-enable
[ 2.211264] omapdss_dss 58000000.dss: using device tree for GPIO lookup
[ 2.211310] of_get_named_gpiod_flags: parsed 'lcd-power-enable-gpios' property of node '/ocp/dss@58000000[0]' - status (0)
[ 2.211331] gpio gpiochip4: Persistence not supported for GPIO 19
[ 2.211903] omapdss_dss 58000000.dss: Dropping the link to regulator.2
[ 2.222480] dmm 4e000000.dmm: workaround for errata i878 in use
[ 2.230716] dmm 4e000000.dmm: initialized all PAT entries
[ 2.245976] panel-simple display: Linked as a consumer to regulator.2
[ 2.252989] panel-simple display: GPIO lookup for consumer enable
[ 2.253001] panel-simple display: using device tree for GPIO lookup
[ 2.253049] of_get_named_gpiod_flags: parsed 'enable-gpios' property of node '/display[0]' - status (0)
[ 2.253071] gpio gpiochip6: Persistence not supported for GPIO 24
[ 2.270526] loop: module loaded
[ 2.274463] of_get_named_gpiod_flags: parsed 'revision-gpios' property of node '/board-revision[0]' - status (0)
[ 2.274522] of_get_named_gpiod_flags: parsed 'revision-gpios' property of node '/board-revision[1]' - status (0)
[ 2.274579] of_get_named_gpiod_flags: parsed 'revision-gpios' property of node '/board-revision[2]' - status (0)
[ 2.274638] of_get_named_gpiod_flags: parsed 'revision-gpios' property of node '/board-revision[3]' - status (0)
[ 2.274762] of_get_named_gpiod_flags: parsed 'revision-gpios' property of node '/board-revision[4]' - status (0)
[ 2.302440] BUCK0: supplied by vdd_3v3
[ 2.308500] BUCK1: supplied by vdd_3v3
[ 2.314310] LDO0: supplied by vdd_5v0
[ 2.319252] LDO1: supplied by vdd_5v0
[ 2.325433] BUCK0: supplied by vdd_5v0
[ 2.331001] BUCK1: supplied by vdd_5v0
[ 2.336627] LDO0: supplied by vdd_3v3
[ 2.341893] LDO1: supplied by vdd_3v3
[ 2.352078] mdio_bus fixed-0: GPIO lookup for consumer reset
[ 2.352091] mdio_bus fixed-0: using lookup tables for GPIO lookup
[ 2.352152] mdio_bus fixed-0: No GPIO consumer reset found
[ 2.352325] libphy: Fixed MDIO Bus: probed
[ 2.361294] mdio_bus 48485000.mdio: GPIO lookup for consumer reset
[ 2.361307] mdio_bus 48485000.mdio: using device tree for GPIO lookup
[ 2.361336] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp/ethernet@48484000/mdio@48485000[0]'
[ 2.361363] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp/ethernet@48484000/mdio@48485000[0]'
[ 2.361376] mdio_bus 48485000.mdio: using lookup tables for GPIO lookup
[ 2.361389] mdio_bus 48485000.mdio: No GPIO consumer reset found
[ 2.411644] davinci_mdio 48485000.mdio: davinci mdio revision 1.6, bus freq 1000000
[ 2.419669] libphy: 48485000.mdio: probed
[ 2.433507] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp/ethernet@48484000/mdio@48485000/ethernet-phy@1[0]'
[ 2.434039] davinci_mdio 48485000.mdio: phy[1]: device 48485000.mdio:01, driver TI DP83822
[ 2.443969] cpsw 48484000.ethernet: Read MACID from Registers = 74:e1:82:90:56:20
[ 2.452251] cpsw 48484000.ethernet: initialized cpsw ale version 1.4
[ 2.458901] cpsw 48484000.ethernet: ALE Table size 1024
[ 2.464524] cpsw 48484000.ethernet: cpts: overflow check period 500 (jiffies)
[ 2.474174] usbcore: registered new interface driver rtl8xxxu
[ 2.490615] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 2.497491] ehci-platform: EHCI generic platform driver
[ 2.503572] ehci-omap: OMAP-EHCI Host Controller driver
[ 2.509534] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 2.516069] ohci-platform: OHCI generic platform driver
[ 2.523749] xhci-hcd xhci-hcd.4.auto: xHCI Host Controller
[ 2.529611] xhci-hcd xhci-hcd.4.auto: new USB bus registered, assigned bus number 1
[ 2.538005] xhci-hcd xhci-hcd.4.auto: hcc params 0x0220f04c hci version 0x100 quirks 0x0000000002010010
[ 2.547910] xhci-hcd xhci-hcd.4.auto: irq 169, io mem 0x48890000
[ 2.555572] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19
[ 2.564337] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 2.571921] usb usb1: Product: xHCI Host Controller
[ 2.577023] usb usb1: Manufacturer: Linux 4.19.73-00043-g58cd7d7-dirty xhci-hcd
[ 2.584705] usb usb1: SerialNumber: xhci-hcd.4.auto
[ 2.591815] hub 1-0:1.0: USB hub found
[ 2.595961] hub 1-0:1.0: 1 port detected
[ 2.601554] xhci-hcd xhci-hcd.4.auto: xHCI Host Controller
[ 2.607419] xhci-hcd xhci-hcd.4.auto: new USB bus registered, assigned bus number 2
[ 2.615527] xhci-hcd xhci-hcd.4.auto: Host supports USB 3.0 SuperSpeed
[ 2.622567] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 2.631373] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 4.19
[ 2.640049] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 2.647637] usb usb2: Product: xHCI Host Controller
[ 2.652776] usb usb2: Manufacturer: Linux 4.19.73-00043-g58cd7d7-dirty xhci-hcd
[ 2.660429] usb usb2: SerialNumber: xhci-hcd.4.auto
[ 2.666628] hub 2-0:1.0: USB hub found
[ 2.670627] hub 2-0:1.0: 1 port detected
[ 2.675944] xhci-hcd xhci-hcd.5.auto: xHCI Host Controller
[ 2.681828] xhci-hcd xhci-hcd.5.auto: new USB bus registered, assigned bus number 3
[ 2.690126] xhci-hcd xhci-hcd.5.auto: hcc params 0x0220f04c hci version 0x100 quirks 0x0000000002010010
[ 2.700096] xhci-hcd xhci-hcd.5.auto: irq 170, io mem 0x488d0000
[ 2.708346] usb usb3: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19
[ 2.717034] usb usb3: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 2.724618] usb usb3: Product: xHCI Host Controller
[ 2.729720] usb usb3: Manufacturer: Linux 4.19.73-00043-g58cd7d7-dirty xhci-hcd
[ 2.737397] usb usb3: SerialNumber: xhci-hcd.5.auto
[ 2.743526] hub 3-0:1.0: USB hub found
[ 2.747522] hub 3-0:1.0: 1 port detected
[ 2.752482] xhci-hcd xhci-hcd.5.auto: xHCI Host Controller
[ 2.758247] xhci-hcd xhci-hcd.5.auto: new USB bus registered, assigned bus number 4
[ 2.766362] xhci-hcd xhci-hcd.5.auto: Host supports USB 3.0 SuperSpeed
[ 2.773447] usb usb4: We don't know the algorithms for LPM for this host, disabling LPM.
[ 2.782645] usb usb4: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 4.19
[ 2.791297] usb usb4: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 2.798887] usb usb4: Product: xHCI Host Controller
[ 2.804023] usb usb4: Manufacturer: Linux 4.19.73-00043-g58cd7d7-dirty xhci-hcd
[ 2.811696] usb usb4: SerialNumber: xhci-hcd.5.auto
[ 2.817784] hub 4-0:1.0: USB hub found
[ 2.821860] hub 4-0:1.0: 1 port detected
[ 2.826888] usbcore: registered new interface driver cdc_acm
[ 2.832905] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[ 2.841415] usbcore: registered new interface driver usb-storage
[ 2.848465] mousedev: PS/2 mouse device common for all mice
[ 2.855796] atmel_mxt_ts 1-004a: GPIO lookup for consumer reset
[ 2.855808] atmel_mxt_ts 1-004a: using device tree for GPIO lookup
[ 2.855838] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp/i2c@48072000/touch@4a[0]'
[ 2.855866] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp/i2c@48072000/touch@4a[0]'
[ 2.855878] atmel_mxt_ts 1-004a: using lookup tables for GPIO lookup
[ 2.855891] atmel_mxt_ts 1-004a: No GPIO consumer reset found
[ 2.881793] atmel_mxt_ts 1-004a: __mxt_read_reg: i2c transfer failed (-121)
[ 2.889252] atmel_mxt_ts 1-004a: mxt_bootloader_read: i2c recv failed (-121)
[ 2.896659] atmel_mxt_ts 1-004a: Trying alternate bootloader address
[ 2.903503] atmel_mxt_ts 1-004a: mxt_bootloader_read: i2c recv failed (-121)
[ 2.911249] atmel_mxt_ts: probe of 1-004a failed with error -121
[ 2.917886] usbcore: registered new interface driver usbtouchscreen
[ 2.953442] rtc-pcf85063 3-0051: rtc core: registered rtc-pcf85063 as rtc0
[ 2.960793] i2c /dev entries driver
[ 2.974948] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 2.985537] cpu cpu0: Linked as a consumer to regulator.9
[ 2.991357] cpu cpu0: Linked as a consumer to regulator.5
[ 3.002884] sdhci: Secure Digital Host Controller Interface driver
[ 3.009349] sdhci: Copyright(c) Pierre Ossman
[ 3.015277] sdhci-pltfm: SDHCI platform and OF driver helper
[ 3.022092] sdhci-omap 4809c000.mmc: GPIO lookup for consumer cd
[ 3.022104] sdhci-omap 4809c000.mmc: using device tree for GPIO lookup
[ 3.022153] of_get_named_gpiod_flags: parsed 'cd-gpios' property of node '/ocp/mmc@4809c000[0]' - status (0)
[ 3.022176] gpio gpiochip5: Persistence not supported for GPIO 27
[ 3.022195] omap_gpio 4805d000.gpio: Could not set line 27 debounce to 200000 microseconds (-22)
[ 3.031391] sdhci-omap 4809c000.mmc: Got CD GPIO
[ 3.036320] sdhci-omap 4809c000.mmc: GPIO lookup for consumer wp
[ 3.036331] sdhci-omap 4809c000.mmc: using device tree for GPIO lookup
[ 3.036360] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@4809c000[0]'
[ 3.036387] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@4809c000[0]'
[ 3.036400] sdhci-omap 4809c000.mmc: using lookup tables for GPIO lookup
[ 3.036412] sdhci-omap 4809c000.mmc: No GPIO consumer wp found
[ 3.036732] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.4
[ 3.044059] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.2
[ 3.051210] sdhci-omap 4809c000.mmc: Dropping the link to regulator.2
[ 3.058281] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.2
[ 3.066494] mmc_add_host: mmc0
[ 3.070100] mmc_add_host: mmc0
[ 3.099784] mmc0: SDHCI controller on 4809c000.mmc [4809c000.mmc] using ADMA
[ 3.110338] sdhci-omap 480b4000.mmc: GPIO lookup for consumer cd
[ 3.110361] sdhci-omap 480b4000.mmc: using device tree for GPIO lookup
[ 3.110420] of_get_named_gpiod_flags: can't parse 'cd-gpios' property of node '/ocp/mmc@480b4000[0]'
[ 3.110596] of_get_named_gpiod_flags: can't parse 'cd-gpio' property of node '/ocp/mmc@480b4000[0]'
[ 3.110623] sdhci-omap 480b4000.mmc: using lookup tables for GPIO lookup
[ 3.110649] sdhci-omap 480b4000.mmc: No GPIO consumer cd found
[ 3.110682] sdhci-omap 480b4000.mmc: GPIO lookup for consumer wp
[ 3.110703] sdhci-omap 480b4000.mmc: using device tree for GPIO lookup
[ 3.110755] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@480b4000[0]'
[ 3.110806] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@480b4000[0]'
[ 3.110831] sdhci-omap 480b4000.mmc: using lookup tables for GPIO lookup
[ 3.110854] sdhci-omap 480b4000.mmc: No GPIO consumer wp found
[ 3.113315] sdhci-omap 480b4000.mmc: Linked as a consumer to regulator.3
[ 3.120642] sdhci-omap 480b4000.mmc: Dropping the link to regulator.3
[ 3.127981] sdhci-omap 480b4000.mmc: Linked as a consumer to regulator.3
[ 3.137335] mmc_add_host: mmc1
[ 3.140936] mmc_add_host: mmc1
[ 3.169782] mmc1: SDHCI controller on 480b4000.mmc [480b4000.mmc] using ADMA
[ 3.178559] sdhci-omap 480ad000.mmc: GPIO lookup for consumer cd
[ 3.178574] sdhci-omap 480ad000.mmc: using device tree for GPIO lookup
[ 3.178615] of_get_named_gpiod_flags: can't parse 'cd-gpios' property of node '/ocp/mmc@480ad000[0]'
[ 3.178650] of_get_named_gpiod_flags: can't parse 'cd-gpio' property of node '/ocp/mmc@480ad000[0]'
[ 3.178668] sdhci-omap 480ad000.mmc: using lookup tables for GPIO lookup
[ 3.178684] sdhci-omap 480ad000.mmc: No GPIO consumer cd found
[ 3.178705] sdhci-omap 480ad000.mmc: GPIO lookup for consumer wp
[ 3.178719] sdhci-omap 480ad000.mmc: using device tree for GPIO lookup
[ 3.178846] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@480ad000[0]'
[ 3.178881] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@480ad000[0]'
[ 3.178898] sdhci-omap 480ad000.mmc: using lookup tables for GPIO lookup
[ 3.178914] sdhci-omap 480ad000.mmc: No GPIO consumer wp found
[ 3.179544] sdhci-omap 480ad000.mmc: Linked as a consumer to regulator.2
[ 3.187220] sdhci-omap 480ad000.mmc: Dropping the link to regulator.2
[ 3.194524] sdhci-omap 480ad000.mmc: Linked as a consumer to regulator.2
[ 3.204337] mmc_add_host: mmc2
[ 3.207793] random: fast init done
[ 3.212143] mmc_add_host: mmc2
[ 3.215412] mmc0: host does not support reading read-only switch, assuming write-enable
[ 3.227544] mmc0: new high speed SDHC card at address aaaa
[ 3.236488] mmcblk0: mmc0:aaaa SA08G 7.40 GiB
[ 3.245874] mmcblk0: p1 p2
[ 3.248961] mmc2: SDHCI controller on 480ad000.mmc [480ad000.mmc] using PIO
[ 3.261204] ledtrig-cpu: registered to indicate activity on CPUs
[ 3.274819] ti-iodelay 4844a000.padconf: Set reg 0x194 Delay(a: 285 g: 0), Elements(C=0 F=8)0x29008
[ 3.286393] optee: probing for conduit method from DT.
[ 3.291878] ti-iodelay 4844a000.padconf: Set reg 0x1ac Delay(a: 189 g: 0), Elements(C=0 F=5)0x29005
[ 3.301342] ti-iodelay 4844a000.padconf: Set reg 0x1b8 Delay(a: 0 g: 120), Elements(C=0 F=2)0x29002
[ 3.311228] optee: revision 3.2 (0dd915f1)
[ 3.312041] optee: initialized driver
[ 3.325495] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp/i2c@4807a000/tlv320aic3104@18[0]'
[ 3.325523] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp/i2c@4807a000/tlv320aic3104@18[0]'
[ 3.325887] tlv320aic3x-codec 3-0018: Linked as a consumer to regulator.2
[ 3.333154] ti-iodelay 4844a000.padconf: Set reg 0x1c4 Delay(a: 0 g: 70), Elements(C=0 F=1)0x29001
[ 3.342924] tlv320aic3x-codec 3-0018: Linked as a consumer to regulator.3
[ 3.350165] ti-iodelay 4844a000.padconf: Set reg 0x1d0 Delay(a: 730 g: 360), Elements(C=1 F=12)0x2902c
[ 3.366645] oprofile: using timer interrupt.
[ 3.371203] ti-iodelay 4844a000.padconf: Set reg 0x1dc Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.381353] Initializing XFRM netlink socket
[ 3.385995] NET: Registered protocol family 17
[ 3.390685] NET: Registered protocol family 15
[ 3.395468] ti-iodelay 4844a000.padconf: Set reg 0x1e8 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.405192] Key type dns_resolver registered
[ 3.409898] ti-iodelay 4844a000.padconf: Set reg 0x1f4 Delay(a: 70 g: 0), Elements(C=0 F=2)0x29002
[ 3.419517] ThumbEE CPU extension supported.
[ 3.424117] Registering SWP/SWPB emulation handler
[ 3.429201] ti-iodelay 4844a000.padconf: Set reg 0x200 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.438561] omap_voltage_late_init: Voltage driver support not added
[ 3.445439] Power Management for TI OMAP4+ devices.
[ 3.450729] ti-iodelay 4844a000.padconf: Set reg 0x368 Delay(a: 0 g: 120), Elements(C=0 F=2)0x29002
[ 3.462383] Loading compiled-in X.509 certificates
[ 3.467607] ti-iodelay 4844a000.padconf: Set reg 0x190 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.484526] ti-iodelay 4844a000.padconf: Set reg 0x1a8 Delay(a: 231 g: 0), Elements(C=0 F=6)0x29006
[ 3.500812] ti-iodelay 4844a000.padconf: Set reg 0x1b4 Delay(a: 39 g: 0), Elements(C=0 F=1)0x29001
[ 3.510822] Key type encrypted registered
[ 3.515925] ima: No TPM chip found, activating TPM-bypass!
[ 3.522134] ima: Allocated hash algorithm: sha1
[ 3.526960] ti-iodelay 4844a000.padconf: Set reg 0x1c0 Delay(a: 91 g: 0), Elements(C=0 F=2)0x29002
[ 3.536811] evm: Initialising EVM extended attributes:
[ 3.542359] evm: security.ima
[ 3.545539] ti-iodelay 4844a000.padconf: Set reg 0x1d8 Delay(a: 176 g: 0), Elements(C=0 F=5)0x29005
[ 3.555388] evm: security.capability
[ 3.559382] evm: HMAC attrs: 0x1
[ 3.563130] ti-iodelay 4844a000.padconf: Set reg 0x1e4 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.583232] ti-iodelay 4844a000.padconf: Set reg 0x1f0 Delay(a: 101 g: 0), Elements(C=0 F=2)0x29002
[ 3.601647] ti-iodelay 4844a000.padconf: Set reg 0x1fc Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.610947] ti-iodelay 4844a000.padconf: Set reg 0x364 Delay(a: 360 g: 0), Elements(C=0 F=10)0x2900a
[ 3.659583] mmc1: new HS200 MMC card at address 0001
[ 3.674020] mmcblk1: mmc1:0001 004G60 3.67 GiB
[ 3.680001] mmcblk1boot0: mmc1:0001 004G60 partition 1 2.00 MiB
[ 3.702924] mmcblk1boot1: mmc1:0001 004G60 partition 2 2.00 MiB
[ 3.710440] mmcblk1gp0: mmc1:0001 004G60 partition 4 4.00 MiB
[ 3.732894] mmcblk1gp1: mmc1:0001 004G60 partition 5 4.00 MiB
[ 3.746612] mmcblk1rpmb: mmc1:0001 004G60 partition 3 512 KiB, chardev (242:0)
[ 3.756547] omapdss_dss 58000000.dss: Linked as a consumer to regulator.2
[ 3.763865] mmcblk1: p1 p2
[ 3.769970] omapdss_dss 58000000.dss: GPIO lookup for consumer lcd-power-enable
[ 3.769989] omapdss_dss 58000000.dss: using device tree for GPIO lookup
[ 3.770423] of_get_named_gpiod_flags: parsed 'lcd-power-enable-gpios' property of node '/ocp/dss@58000000[0]' - status (0)
[ 3.770469] gpio gpiochip4: Persistence not supported for GPIO 19
[ 3.772150] DSS: OMAP DSS rev 6.1
[ 3.778431] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops)
[ 3.824181] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 3.831311] [drm] No driver support for vblank timestamp query.
[ 3.896641] [drm] Enabling DMM ywrap scrolling
[ 3.920759] Console: switching to colour frame buffer device 160x50
[ 4.199476] omapdrm omapdrm.0: fb0: omapdrm frame buffer device
[ 4.212501] [drm] Initialized omapdrm 1.0.0 20110917 for omapdrm.0 on minor 0
[ 4.224306] of_get_named_gpiod_flags: parsed 'amplifier-sd-gpio' property of node '/sound@0[0]' - status (0)
[ 4.225017] of_get_named_gpiod_flags: can't parse 'simple-audio-card,hp-det-gpio' property of node '/sound@0[0]'
[ 4.225074] of_get_named_gpiod_flags: can't parse 'simple-audio-card,mic-det-gpio' property of node '/sound@0[0]'
[ 4.227337] asoc-simple-card sound@0: tlv320aic3x-hifi <-> 48468000.mcasp mapping ok
[ 4.247080] of_get_named_gpiod_flags: parsed 'gpios' property of node '/on-off-key/on-off-key[0]' - status (0)
[ 4.247108] gpio gpiochip4: Persistence not supported for GPIO 1
[ 4.247596] input: on-off-key as /devices/platform/on-off-key/input/input0
[ 4.258745] rtc-pcf85063 3-0051: setting system clock to 2019-09-15 09:00:41 UTC (1568538041)
[ 4.271209] net eth0: initializing cpsw version 1.15 (0)
[ 4.301412] TI DP83822 48485000.mdio:01: attached PHY driver [TI DP83822] (mii_bus:phy_addr=48485000.mdio:01, irq=POLL)
[ 4.491677] Waiting up to 2 more seconds for network.
[ 4.671733] Waiting up to 2 more seconds for network.
[ 4.851676] Waiting up to 1 more seconds for network.
[ 5.031676] Waiting up to 1 more seconds for network.
[ 5.211677] Waiting up to 1 more seconds for network.
[ 5.391739] Waiting up to 1 more seconds for network.
[ 5.571677] Waiting up to 1 more seconds for network.
[ 5.751672] Waiting up to 1 more seconds for network.
[ 5.931670] Waiting up to 0 more seconds for network.
[ 6.111679] Waiting up to 0 more seconds for network.
[ 6.291783] Waiting up to 0 more seconds for network.
[ 6.351678] IP-Config: Complete:
[ 6.355119] device=eth0, hwaddr=74:e1:82:90:56:20, ipaddr=192.168.0.1, mask=255.255.255.0, gw=192.168.0.254
[ 6.366278] host=192.168.0.1, domain=, nis-domain=(none)
[ 6.373091] bootserver=192.168.0.254, rootserver=192.168.0.254, rootpath=
[ 6.382941] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 6.393220] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 6.400960] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 6.411519] ALSA device list:
[ 6.414857] cfg80211: failed to load regulatory.db
[ 6.420208] #0: Target-Audio
[ 6.425638] Freeing unused kernel memory: 1024K
[ 6.430635] Run /init as init process
[ 6.436672] cpsw 48484000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 7.254527] systemd[1]: systemd 234 running in system mode. (-PAM -AUDIT -SELINUX -IMA -APPARMOR -SMACK +SYSVINIT -UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL -XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN default-hierarchy=hybrid)
[ 7.278760] systemd[1]: Detected architecture arm.
[ 7.316553] systemd[1]: Set hostname to <target>.
[ 7.946087] random: systemd: uninitialized urandom read (16 bytes read)
[ 7.953509] systemd[1]: Listening on Network Service Netlink Socket.
[ 7.993385] random: systemd: uninitialized urandom read (16 bytes read)
[ 8.000707] systemd[1]: Listening on udev Kernel Socket.
[ 8.031798] random: systemd: uninitialized urandom read (16 bytes read)
[ 8.040008] systemd[1]: Listening on Journal Socket (/dev/log).
[ 8.072125] systemd[1]: Reached target Paths.
[ 8.114048] systemd[1]: Created slice System Slice.
[ 8.148894] systemd[1]: Mounting Kernel Debug File System...
[ 8.198046] systemd[1]: Mounting POSIX Message Queue File System...
[ 8.830325] random: crng init done
[ 8.833947] random: 7 urandom warning(s) missed due to ratelimiting
[ 9.651515] systemd-journald[128]: Received request to flush runtime journal from PID 1
[ 12.973530] power_module: loading out-of-tree module taints kernel.
[ 13.045099] of_get_named_gpiod_flags: parsed 'wlan-enable-gpio' property of node '/power-module[0]' - status (0)
[ 13.045164] of_get_named_gpiod_flags: parsed 'power-good-gpio' property of node '/power-module[0]' - status (0)
[ 13.045388] of_get_named_gpiod_flags: parsed 'bsp-support-gpios' property of node '/power-module[0]' - status (0)
[ 13.045576] of_get_named_gpiod_flags: parsed 'bsp-support-gpios' property of node '/power-module[1]' - status (0)
[ 13.156208] mmc2: new high speed SDIO card at address 0001
[ 14.112968] EXT4-fs (mmcblk1gp0): mounted filesystem with ordered data mode. Opts: (null)
[ 14.150970] EXT4-fs (mmcblk1gp1): mounted filesystem with ordered data mode. Opts: (null)
[ 24.371626] mlan: module license 'Marvell Proprietary' taints kernel.
[ 24.378496] Disabling lock debugging due to kernel taint
[ 24.454788] wlan: Loading MWLAN driver
[ 24.465491] vendor=0x02DF device=0x9139 class=0 function=1
[ 24.473168] rx_work=0 cpu_num=1
[ 24.483761] Request firmware: mrvl/sd8801_uapsta.bin
[ 25.284818] Wlan: FW download over, firmwarelen=256188 downloaded 256188
[ 25.495062] WLAN FW is active
[ 25.498220] QUEUE_CMD: cmd=0xa9 is queued
[ 25.504999] QUEUE_CMD: cmd=0x3 is queued
[ 25.509124] DNLD_CMD (1568538062.750397): 0xa9, act 0x0, len 8, seqno 0x1
[ 25.518762] DNLD_CMD:
[ 25.518773] a9 00 08 00 01 00 00 00
[ 30.561669] Driver version = SD8801-0.0.0.p0-C4X14C635-GPL-(FP68)
[ 30.568216] main_state = 1
[ 30.571081] ioctl_pending = 0
[ 30.579071] tx_pending = 0
[ 30.585657] rx_pending = 0
[ 30.588496] lock_count = 28
[ 30.591470] malloc_count = 26
[ 30.598227] mbufalloc_count = 0
[ 30.601519] hs_skip_count = 0
[ 30.607315] hs_force_count = 0
[ 30.610539] Wakeup device...
[ 30.616178] woal_request_fw failed - mrvl/sd8801_uapsta.bin
[ 30.623345] Firmware Init Failed